Configuring an Ethernet motion system

Configuring a motion system is a process with many different configuration options. Basic Ethernet motion system setup requires these steps in the Logix Designer application:
Step
Process
Reason
1.
Add an Ethernet motion module
Identifies the motion module being used to the Logix controller
2.
Create an axis for a motion drive
An axis is used to define forward and backward motion in one direction.
3.
Create a motion group
Consolidates the axes into a control set to provide coordinated motion.
4.
Configure the axis properties
Defines the individual properties for the axis, including motor feedback, axis configuration, and scaling.
For the purposes of this quick start, assume this configuration:
  • An Ethernet motion module, either Kinetix or PowerFlex
  • Motor feedback
  • Position loop axis configuration
  • A new controller project with an Ethernet communications module configured
Add an Ethernet motion module
  1. Right-click the Ethernet network (node) and choose
    New Module
    .
  2. In
    Select Module Type
    , under
    Module Type Category Filters
    , select the appropriate checkbox to filter the selections and select the motion module from the list.
  3. Click Create. The
    New Module
    dialog box appears.
    • In
      Name
      , type a name for the module.
    • (optional) In
      Description
      , type a description.
  4. In
    Ethernet Address
    specify an IP address.
  5. Under
    Module Definition
    , click
    Change
    . The
    Module Definition
    dialog box appears.
  6. In
    Electronic Keying
    select
    Compatible Module
    .
    IMPORTANT:
    The electronic keying feature automatically compares the expected module, as shown in the configuration tree, to the physical module before communication begins.
    When you are using motion modules, set the electronic keying to either
    Exact Match
    or
    Compatible Module
    .
    Never use
    Disable Keying
    with motion modules.
  7. In
    Connection
    , select
    Motion
    .
  8. (optional) In
    Power Structure
    , select the appropriate power structure from the list (Example: 2094-BC01-MP5-M) and then select
    Verify Power Rating on Connection
    .
    TIP: Power structure identifiers are not required for all modules. If needed, these numbers are found on the hardware, in the device documentation, and on the bill of materials. Many modules have power structures defined by default.
  9. Click
    OK
    to apply the changes.
Create an axis for a motion drive
  1. Double-click the drive in the
    Controller Organizer
    to open the
    Module Properties
    dialog box.
  2. Click the
    Associated Axes
    tab.
  3. Click
    New Axis
    . The
    New Tag
    dialog box appears.
    • In
      Name
      , type a tag name.
    • (optional) In
      Description
      , type a description.
  4. In
    Type
    , select
    Base
    .
  5. In
    Data Type
    select
    AXIS_CIP_DRIVE
    .
  6. Click
    Create
    .
Create a Motion Group
  1. In the
    Controller Organizer
    , right-click
    Motion Groups
    and select
    New Motion Group
    .
  2. The
    New Tag
    dialog box appears.
    • In
      Name
      , type a tag name.
    • (optional) In
      Description
      , type a description.
  3. In
    Type
    , select
    Base
    .
  4. In
    External Access
    , select
    Read/Write
    .
  5. Click
    Create
    . The new motion group appears in the
    Controller Organizer
    under the
    Motion Groups
    folder.
  6. Right-click the new motion group and choose
    Properties
    . The
    Motion Group Properties
    dialog box appears.
  7. Click the
    Axis Assignment
    tab and move the axes (created earlier) from
    Unassigned
    to
    Assigned
    .
  8. Click the
    Attribute
    tab in the
    Motion Group Properties
    dialog box, set the
    Base Update Period
    to 5 ms. For the Kinetix 6500 drive, the minimum Base Update Rate is 1 ms.
  9. Click
    OK
    .
Configure the Axis Properties
  1. In the
    Controller Organizer
    , double-click the axis.
  2. Configure
    General
    properties
    • In
      Axis Configuration
      , select
      Position Loop
      .
    • In
      Feedback Configuration
      ,
      select
      Motor Feedback
      .
    • In
      Application Type
      , select
      Basic
    • In
      Loop Response
      , select
      Medium
      .
  3. Configure
    Motor
    properties
    • Select the
      Motor
      page.
    • Specify a motor with the
      Data Source
      selected as
      Catalog Number.
      All of the motor settings are completed automatically to match the settings specified for that catalog number.
  4. Motor Feedback
    properties are configured by default.
  5. Configure
    Scaling
    properties
    • Select the
      Scaling
      page.
    • In
      Load Type
      , select
      Direct Coupled Rotary
      .
    • In
      Scaling
      for
      Units
      , select
      Position Units
      .
    • Then in
      Scaling
      enter 1.0
      Position Units per
      1.0
      Motor Rev
      .
    • In
      Travel
      , for
      Mode
      select
      Unlimited
      .
  6. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal