The module could not be found
There was a problem communicating with the module. Check if:
- an incorrect slot was configured for the module
- the module created in the software does not exist on the network at the address specified in the software, or communication to the module was lost
- the module has a major fault
- a bridge module has been configured for an incorrect slot, it has faulted, or communication to it was lost
- FactoryTalk Linxis not running
Provide Feedback