FLEX I/O Calibration: Produce High Reference Signals

To produce high reference signals for gain calibration:
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
Select
Next
to perform gain calibration.
You may also select:
  • Retry
    if an error occurs and you need to repeat a step in the calibration process.
    TIP: This button is only enabled when an error occurs.
  • Stop
    to cancel calibration and exit the calibration.
  • Help
    for assistance with this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal