Attach High Reference Signals - Input - FLEX I/O Calibration
To attach high reference signals for gain calibration:
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
- Set the precision voltage/current source to the correct value.
- SelectNextto perform gain calibration.
The module reads the signal and calibrates.
You may also select:
- Retryif an error occurs and you need to repeat a step in the calibration process.TIP: This button is only enabled when an error occurs.
- Stopto cancel calibration and exit the calibration.
- Helpfor assistance with this tab.
Provide Feedback