Use Coordinated System Time to Timestamp I/O

Use Coordinated System Time (CST) to timestamp inputs and scheduled outputs.
  1. Choose a communications format for each input and output module that allows timestamping.
    TIP: If you need additional information about choosing a communications format, please refer to the
    ControlLogix Digital I/O Modules (1756-Series) User Manual
    .
  2. Ensure that a controller is in the same rack as both I/O modules.
  3. Disable the Change of State for all input points on the input module except for the point being timestamped.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal