Module Properties Dialog Box - Module Info Tab Overview
The Module Info Tab displays module and status information about the module. It also allows you to reset a module to its power-up state. The information on this tab is not displayed if you are:
- Offline, or
- Currently creating a module
Use this tab to determine the identity of the module.
TIP:
The data on this tab comes directly from the module. If you selected a
Listen-Only communication format when you created the module, this tab is not
available.
Parameters
Identification
Displays the module:
- Vendor
- Product Type
- Product Code
- Revision
- Serial Number
- Product Name
The name displayed in the Product Name field is read from the module. This name displays the series of the module. If the module is a 1756-L1 module, this field displays the catalog number of the memory expansion board (this selection applies to any controller catalog number even if additional memory cards are added.
Major/Minor Fault Status
If you are configuring a: | This field displays one of these: |
digital module |
|
analog module |
|
any other module |
|
Internal State Status
Displays the module’s current operational state.
- Self-test
- Flash update
- Communication fault
- Unconnected
- Flash configuration bad
- Major Fault (please refer to "Major/Minor Fault Status" above)
- Run mode
- Program mode
- (16#xxxx) unknown
If you selected the wrong module from the module selection tab, this field displays a hexadecimal value. A textual description of this state is only given when the module identity you provide is a match with the actual module.
Configured
Displays a yes or no value indicating whether the module has been configured by an owner controller connected to it. Once a module has been configured, it stays configured until the module is reset or power is cycled, even if the owner drops connection to the module. This information applies to I/O modules only and does not apply to adapters, scanners, bridges, or other communications modules.
Owned
Displays a yes or no value indicating whether an owner controller is currently connected to the module. This information applies to I/O modules only and does not apply to adapters, scanners, bridges, or other communications modules.
Module Identity
Displays: | If the physical module: |
Match | agrees with what is specified on the General Tab In order for the Match condition to exist, all of the following must agree:
|
Mismatch | does not agree with what is specified on the General Tab |
This field does not take into account the Electronic Keying or Minor Revision selections for the module that were specified on the General Tab.
TIP:
The Generic modules, such as the 1756-MODULE, always show a Mismatch because
the configured Generic Key does not match any target device.
Reset Module
Selct this button to return a module to its power-up state by emulating the cycling of power.
ATTENTION:
Resetting a module causes all connections to or through the module to
be closed, and this may result in loss of control.
TIP:
These modules return an error if a reset is attempted:
- 1756-L1 ControlLogix5550 Programmable Controller
- 1336T AC Vector Drive
- 1395 Digital DC Drive
TIP:
A controller cannot be reset.
Refresh
Select this button to refresh the tab with new data from the module.
TIP:
Only 1756 I/O, 1756-M02AE, 1756-L1, and 1756-L1Mx modules have the following
fields.
Coordinated System Time (CST)
Timer Hardware
Displays whether the timer’s hardware is OK or faulted.
Timer Sync’ed
Displays yes if the module’s timer is coordinated with the master; displays no if it is not.
Provide Feedback