Module Properties Dialog Box - Backplane Tab Overview

Use this tab to:
  • View diagnostic information about the module’s communications over the backplane and the chassis in which it is located
  • Clear fault
    fault
    A problem or error detected by the control system hardware or software. A fault is identified by an error code or an error bit.
Information on this tab is displayed only if you are online.
TIP: If you selected a Listen-Only communication format when you created the module, this tab is not available.
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
TIP: The data on this tab comes directly from the module.
Parameters
ControlBus Status
Displays the OK or one of these errors:
  • Receiver disabled
  • Multicast addresses disabled
  • RA/GA miscompare
Clear Fault
Select this button to clear the module’s backplane fault.
ControlBus Parameters
Multicast CRC Error Threshold
Displays the threshold for entering a fault state due to multicast CRC errors.
cyclic redundancy check (CRC)
A Cyclic Redundancy Check (CRC) is an error checking technique used by computers.
Transmit Retry Limit
Select a transmit retry limit. This limit is the number of times a frame is retried if a transmit error occurs. This field has a range of 0-63; we recommend you use a value between:
  • 8-12 for isolated analog modules
  • 3-10 for all other analog modules
When you reset a module, this field is reset to its factory default.
Receive Error Counters
Displays:
  • Number of bad CRC errors that occurred on received frames (messages)
  • Number of receiver bus time-outs
  • Number of multicast receive CRC errors
Transmit Error Counters
Displays:
  • Number of bad CRC errors that occurred on transmitted frames
  • Number of transmitter bus time-outs
1756 Specialty I/O Modules and Adapters, Communications, and Controllers
Chassis Information
Displays:
  • Revision number of the chassis
  • Size of the chassis
  • Serial number of the chassis
  • Module’s slot number
    TIP: This information remains blank in Module Match conditions for the 1756-HSC and 1756-PLS modules
Refresh
Select to refresh the tab. When you refresh the tab:
If you are using:
then:
digital, analog, or motion modules
counters are cleared
another module
the tab is refreshed but the counters are not cleared
OK
Select this button to accept your edits on any tab and close the dialog.
Cancel
Select this button to cancel your edits on any tab and close the dialog.
Apply
Select this button to apply your edits on any tab and continue editing.
If:
  • You are online in Program, Remote Program or Remote Run mode, and
  • This controller is the owner controller, and
    controller
    A device that controls machines or processes elements (for example, a programmable controller or relay panel).
  • You have changed the module’s configuration in the software
then when you select
Apply
or
OK
, the information is automatically sent to the controller. The controller tries to send the information to the module (if the module’s connection is not inhibited). If you don’t select
Apply
, your changes are not sent to the controller.
Help
Select this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal