Assign an ASCII character to a string data member
Use the assignment operator to assign an ASCII character to an element of the DATA member of a string tag. To assign a character, specify the value of the character or specify the tag name, DATA member, and element of the character. For example:
This is OK | This is not OK |
string1.DATA[0] := 65; | string1.DATA[0] := A; |
string1.DATA[0]:= string2.DATA[0]; | string1 := string2;
TIP:
This assigns all content of string2 to
string1 instead of just one character.
|
To add or insert a string of characters to a string tag, use either of these ASCII string instructions:
To | Use this instruction |
Add characters to the end of a string | CONCAT |
Insert characters into a string | INSERT |
Provide Feedback