Minimum Capture (MINC)
This information applies to the CompactLogix 5370, ControlLogix 5570, CompactGuardLogix
5370, GuardLogix 5570, CompactGuardLogix 5380, CompactLogix 5380, ControlLogix 5580,
GuardLogix 5580, and ControlLogix 5590 controllers.
The Minimum Capture (MINC) instruction retains the minimum value of the input over time and allows the user to re-establish a minimum as needed.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram.
Function Block

Structured Text
MINC(MINC_tag);
Operands
Function Block
Operand | Type | Format | Description |
MINC tag | MINIMUM_CAPTURE | structure | MINC structure |
MINIMUM_CAPTURE Structure
Input Parameter | Data Type | Description |
EnableIn | BOOL | Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set. |
In | REAL | The analog signal input to the instruction.
Valid = any float
Default = 0.0 |
Reset | BOOL | Request to reset control algorithm. The instruction sets Out = ResetValue as long as Reset is set.
Default is cleared. |
ResetValue | REAL | The reset value for the instruction. The instruction sets Out = ResetValue as long as Reset is set.
Valid = any float
Default = 0.0 |
Output Parameter | Data Type | Description |
EnableOut | BOOL | Enable output. |
Out | REAL | The calculated output of the algorithm. |
Structured Text
Operand | Type | Format | Description |
MINC tag | MINIMUM _CAPTURE | structure | MINC structure |
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
The MINC instruction executes this algorithm:
Condition | Action |
Reset is set | LastMinimum = ResetValue Out = ResetValue |
Reset is cleared | If In < LastMinimum then update LastMinimum.
Out = LastMinimum. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State | Action Taken |
Prescan | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is false | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is true | EnableIn and EnableOut bits are set to true. The instruction executes. |
Instruction first run | N/A |
Instruction first scan | Set request to initialize the Minimum value with the current input. |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
In Structured Text, EnableIn is always True during a normal scan. If the instruction is in
the control path activated by the logic, it executes.
Condition/State | Action Taken |
Prescan | See Prescan in the Function Block table. |
Normal Execution | See Tag.EnableIn is true in the Function Block table. |
Postscan | See Postscan in the Function Block table. |
Examples
If Reset is set, the instruction set Out=ResetValue. If Reset is cleared, the instruction set Out=In when In < LastMinimum. Otherwise, the instruction sets Out= LastMinimum.
Function Block

Structured Text
MINCTag.In := input_value;
MINCTag.Reset := reset_input;
MINCTag.ResetValue := reset_value;
MINC(MINCTag);
result := MINCTag.Out;
Provide Feedback