Selected Negate (SNEG)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers.The Selected Negate (SNEG) instruction uses a digital input to select between the input value and the negative of the input value.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram logic.
Function Block

Structured Text
SNEG(SNEG_tag);
Operands
Function Block
Operand | Type | Format | Description |
SNEG tag | SELECTABLE_NEGATE | Structure | SNEG structure |
SNEG Structure
Input Parameter | Data Type | Description |
EnableIn | BOOL | Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true. Structured Text:
No effect. The instruction executes. |
In | REAL | The analog signal input to the instruction.
Valid = any float
Default = 0.0 |
NegateEnable | BOOL | Negate enable. When NegateEnable is true, the instruction sets Out to the negative value of In.
Default is true. |
Output Parameter | Data Type | Description |
EnableOut | BOOL | Indicates if instruction is enabled. Cleared to false if Out overflows. |
Structured Text
Operand | Type | Format | Description |
SNEG tag | SELECTABLE_NEGATE | Structure | SNEG structure |
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
The SNEG instruction operates as follows:
Condition | Action |
NegateEnable is true | Out = - In |
NegateEnable is false | Out = In |
Affects Math Status Flags
No
Major/Minor faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State | Action Taken |
Prescan | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is false | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is true | EnableIn and EnableOut bits are set to true. The instruction executes. |
Instruction first run | N/A |
Instruction first scan | N/A |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
Condition/State | Action Taken |
Prescan | See Prescan in the Function Block table. |
Normal Execution | See Tag.EnableIn is true in the Function Block table. |
Postscan | See Postscan in the Function Block table. |
Example
The negate_enable input determines whether to negate In or not. The instruction sets Out = In if NegateEnable is false. The instruction sets Out = -In if NegateEnable is true.
Function Block

Structured Text
SNEG_01.In := analog_input1;
SNEG_01.NegateEnable := negate_enable;
SNEG(SNEG_01);
output_value := SNEG_01.Out;
Provide Feedback