Two Hand Run Station Enhanced (THRSe)
This instruction applies to the Compact GuardLogix 5370, GuardLogix 5570, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers.
Use this instruction to monitor the inputs of a Two-hand Run Station. Each run station button has two inputs; one normally-closed (N.C.) contact and one normally-open (N.O.) contact. To energize Output 1, the instruction must be enabled and connected with no faults present. Then both buttons must be pressed within 500 ms of one another.
IMPORTANT:
The right and left buttons of the Two-hand Run Station must be pressed
within 500 ms of one another to energize Output 1. To make sure this situation can be
properly detected, the safety task period cannot exceed 40 ms and the input device’s
requested packet interval (RPI) cannot exceed 20 ms.
Refer to the
GuardLogix
5580 and Compact GuardLogix
5380 Controller Systems Safety Reference, publication
1756-RM012, for information on the safety task period and the RPI.The Buttons Released (BR) output turns ON (1) whenever the Two-hand Run Station is connected and enabled, no faults are present, and both the right and left buttons are in the released (safe) state. In this case, all four contacts are in the safe state.
The Two-hand Run Station may be disconnected when not in use. To properly disconnect the Two-hand Run Station, the Disconnected input must be ON (1) and all button inputs must be OFF (0). When the Two-hand Run Station is disconnected, the (SB) Station Bypassed output turns ON (1).
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
WARNING:
If you change instruction parameters while in Run
mode, you must accept the pending edits and cycle the controller mode from Program to Run
for the changes to take effect.
IMPORTANT:
Unexpected operation, including controller assert or a
Major Non-Recoverable Fault, can occur if:
- Backing tag members are written to.
- Backing tags are shared by multiple instruction invocations.
- Backing tag members are passed as parameters to an instruction controlled by the same backing tag.
- The backing tag.EnableInmember is referenced anywhere in the program..EnableInis a parameter that represents rung state into an instruction and is only intended for internal use.For examples of these incorrect backing tag usages, seeBacking tag usages that can cause unexpected operation.
IMPORTANT:
Do not use the same tag for more than one instruction in the same
program. Do not write to any instruction output tag under any circumstances.
IMPORTANT:
Make sure that your safety input points are configured as Single, not
Equivalent or Complementary. These instructions provide all dual channel functionality
necessary for PLd (Cat. 3) or PLe (Cat. 4) safety functions.
The following table provides the parameter used to configure the instruction. This parameter cannot be changed at runtime.
Operand | Data Type | Description |
THRSe | THRS_ENHANCED | This parameter is a backing tag that maintains important execution information for each usage of this instruction. For examples of incorrect backing tag usages, see Backing tag usages that can cause unexpected operation. |
Discrepancy Time | DINT | The amount of time that the instruction lets the normally-open and normally-closed button contacts be inconsistent before generating a fault. The inconsistent state occurs when the normally-open contact and the normally-closed contact have the same logical value; that is, both are ON (1) or both are OFF (0). The valid range is 100 to 3000 ms. |
The following table provides the input parameters for the instruction.
Operand | Data Type | Description |
---|---|---|
Enable | BOOL | ON (1): The device is enabled. Output 1 is energized when both buttons are pressed within 500 ms of one another. OFF (0): The device is disabled. Output 1 stays de-energized. |
Disconnected | BOOL | This input indicates whether the run station is disconnected. When this input is ON (1) and all of the button inputs (Right Button Normally Open, Right Button Normally Closed, Left Button Normally Open, Left Button Normally Closed) are OFF (0), the Station Bypassed output turns ON (1). ON (1): The run station is disconnected. Output 1 cannot be energized. OFF (0): The run station is not disconnected. Output 1 may be energized. |
Right Button Normally Open 1 | BOOL | This is the normally-open contact for the right button. |
Right Button Normally Closed 1 | BOOL | This is the normally-closed contact for the right button. |
Left Button Normally Open 1 | BOOL | This is the normally-open contact for the left button. |
Left Button Normally Closed 1 | BOOL | This is the normally-closed contact for the left button. |
Input Status | BOOL | If the instruction inputs are from a safety I/O module, this value is the status from the I/O module or modules (Connection Status or Combined Status). If instruction inputs are derived from internal logic, it is the application programmer's responsibility to determine the conditions. ON (1): The inputs to this instruction are valid. OFF (0): The inputs to this instruction are invalid. |
Reset 2 | BOOL | This input clears instruction and circuit faults provided the fault condition is not present. OFF (0) -> ON (1): The Fault Present and Fault Code outputs are reset. |
1
If this input is from a Guard I/O
input module, make sure that the input is configured as single, not Equivalent or Complementary.2
Some safety standards require monitoring the transition of the reset
input. When the reset is used to reset a safety function, additional logic may be
required to verify a transition of the reset input from High-to-Low or
Low-to-High.The following table provides the output parameters for the instruction.
Operand | Data Type | Description |
Output 1 (O1) | BOOL | This output is energized when the run station is enabled and connected, and both buttons are pressed within 500 ms of one another. Output 1 is de-energized when one or more of the following occurs:
|
Buttons Released (BR) | BOOL | This output is ON (1) when both buttons are released, the run station is connected and enabled, and no faults are present. |
Station Bypassed (SB) | BOOL | This output is ON (1) when the run station has been properly disconnected and no faults are present. See the Disconnecting the Two-hand Run Station section. |
Fault Present (FP) | BOOL | ON (1): A fault is present in the instruction. OFF (0): The instruction is operating normally. |
Fault Code | DINT | This output indicates the type of fault that occurred. See the Fault Codes section below for the list of fault codes.This parameter is not safety-related. |
Diagnostic Code | DINT | This output indicates the diagnostic status of the instruction. See the Diagnostic Codes section below for a list of diagnostic codes.This parameter is not safety-related. |
IMPORTANT:
Do not write to any instruction output tag under any
circumstances.
Disconnecting the Two-hand Run Station
To energize the Station Bypassed output (disconnect the Two-hand Run Station), the Disconnected input must be ON (1), and all the button inputs must be OFF (0).
If a fault occurs while disconnecting the Two-hand Run Station, trigger a reset after the inputs are in the correct state.
Connecting the Two-hand Run Station
To de-energize the Station Bypassed output (connect the Two-hand Run Station), the Disconnected input must be OFF (0), and the button inputs must be in the release safe state.
If a fault occurs while connecting the Two-hand Run Station, trigger a reset after the inputs are in the correct state.
Operation
Normal Operation
As shown in the timing diagram, the Buttons Released output turns ON (1) whenever both buttons are released, the run station is connected and enabled, and no faults are present.
Before (A), the left and right buttons are both pressed, but Output 1 has not yet been energized because the Enable input is OFF (0). When the Enable input transitions from OFF (0) to ON (1) at (A), Output 1 is not energized because the buttons must be pressed while the Enable input is ON (1). At (B), the right button is pressed but the left button is still released, which turns OFF (0) the Buttons Released output. At (C), both buttons have been pressed within 500 ms of one another, which energizes Output 1 after a 50 ms delay. Output 1 is de-energized when the left button is released at (D). Output 1 is energized 50 ms after both buttons are pressed at (E). Lastly, at (F),Output 1 is de-energized because the Enable input turns OFF (0).

Button Held Down Diagnostic Operation
Output 1 cannot be energized when the right and left buttons are not pressed within 500 ms of one another.
At (A), the right button is pressed while the left button remains released. At (B), the buttons have been in an inconsistent state for 500 ms, which generates a diagnostic signal that requires both buttons be released before Output 1 can be energized again. At (C), the left button is pressed, but Output 1 is not energized because both buttons have not been released after the right button was held down longer than 500 ms. Both buttons are released, which clears the diagnostic signal at (D). Output 1 is energized after a 50 ms delay when both buttons are pressed within 500 ms of one another at (E).

Button Glitch Diagnostic Operation
When one button is released while the other button remains pressed, both buttons must be released to the safe state before Output 1 can be energized again.
At (A), Output 1 is de-energized because the right button is released.
At (B), the right button is pressed, but the left button remained released since (A), generating a diagnostic signal that requires both buttons to be released before Output 1 can be energized again. Both buttons are released at (C), which clears the diagnostic signal. At (D), Output 1 is energized after a 50 ms delay when both buttons are pressed within 500 ms of one another.

Button Discrepancy Fault (Channel-to-channel) Operation
A discrepancy fault occurs when the two channels of one button are in an inconsistent state for more than the configured Discrepancy Time (250 ms in this example).
At (A), the right button is pressed, but only the normally-open contact of the left button turns ON (1) while the normally-closed contact remains OFF (0). After the Left Button Normally Open and the Left Button Normally Closed inputs have been inconsistent for 250 ms, the fault occurs at (B). At (C), the fault is cleared by a Reset. Lastly, at (D), Output 1 is energized 50 ms after both buttons are pressed.

Run Station Disconnected (Station Bypassed) Operation
When the run station is properly disconnected, Output 1 cannot be energized. The Station Bypassed output is energized whenever the run station is properly disconnected.
At (A), Output 1 is energized 50 ms after both buttons are pressed. At (B), Output 1 is de-energized and a fault occurs when the Disconnected input turns ON (1). To clear the fault, both buttons must be released and a reset triggered at (C). The Station Bypassed output turns ON (1). At (D), the Station Bypassed output turns OFF (0) and a fault occurs when the Right Button Normally Open input turns ON (1) while the Disconnected input is ON (1). At (E), the fault is cleared and the Station Bypassed output is turned ON (1) when a reset is triggered with the Disconnected input ON (1) and all button inputs OFF (0). Lastly, at (F), the Enable input transitions from ON (1) to OFF (0) to ON (1), but has no effect on the Station Bypassed output, which remains ON (1).

False Rung State Behavior
When the instruction is executed on a false rung, all instruction outputs are de-energized.
Fault Codes and Corrective Actions
The fault codes are listed in hexadecimal format followed by decimal format.
Fault Code | Description | Corrective Action |
---|---|---|
00 | No fault. | None |
16#20 32 | The Input Status input transitioned from ON (1) to OFF (0) while the instruction was executing. |
|
16#7001 28673 | The right button contacts were in an inconsistent state for longer than the Discrepancy Time. At the time of the fault, the Right Button Normally Open was ON (1) and the Right Button Normally Closed was OFF (0). |
|
16#7002 28674 | The right button contacts were in an inconsistent state for longer than the Discrepancy Time. At the time of the fault, the Right Button Normally Closed was ON (1) and the Right Button Normally Open was OFF (0). | |
16#7003 28675 | The left button contacts were in an inconsistent state for longer than the Discrepancy Time. At the time of the fault, the Left Button Normally Open was ON (1) and the Left Button Normally Closed was OFF (0). |
|
16#7004 28676 | The left button contacts were in an inconsistent state for longer than the Discrepancy Time. At the time of the fault, the Left Button Normally Closed was ON (1) and the Left Button Normally Open was OFF (0). | |
16#7005 28677 | The Right Button Normally Open input transitioned from ON (1) to OFF (0) to ON (1) while the Right Button Normally Closed input remained ON (1). |
|
16#7006 28678 | The Right Button Normally Closed input transitioned from ON (1) to OFF (0) to ON (1) while the Right Button Normally Open input remained ON (1). | |
16#7007 28679 | The Left Button Normally Open input transitioned from ON (1) to OFF (0) to ON (1) while the Left Button Normally Closed input remained ON (1). |
|
16#7008 28680 | The Left Button Normally Closed input transitioned from ON (1) to OFF (0) to ON (1) while the Left Button Normally Open input remained ON (1). | |
16#7030 28720 | The Disconnected input was ON (1), but all of the button inputs were not OFF (0). |
|
16#7031 28721 | The button inputs were disconnected for longer than the Discrepancy time, but the Disconnected input was OFF (0). |
|
Diagnostic Codes and Corrective Actions
The diagnostic codes are listed in hexadecimal format followed by decimal format.
Diagnostic Code | Description | Corrective Action |
00 | No fault. | None |
16#20 32 | The Input Status was OFF (0) when the instruction started. | Check the I/O module connection |
16#7001 28673 | The device is not in the safe state for start-up. | Release both buttons to OFF (0). |
16#7002 28674 | The right button is held down. The left and right buttons have been in an inconsistent state for longer than 500 ms. | Release both buttons to OFF (0). |
16#7003 28675 | The left button is held down. The left and right buttons have been in an inconsistent state for longer than 500 ms. | Release both buttons to OFF (0). |
16#7004 28676 | The right button was released and then pressed while the left button remained pressed. | Release both buttons to OFF (0). |
16#7005 28677 | The left button was released and then pressed while the right button remained pressed. | Release both buttons to OFF (0). |
16#7060 28768 | The run station is not enabled. | Enable or disconnect the run station. |
16#7061 28769 | The run station is bypassed. | No action required. |
Affects Math Status Flags
No
Major / Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Condition/State | Action Taken |
---|---|
Prescan | Same as Rung-condition-in is false. |
Enable-in is false | The .O1, .BR, .SB and .FP are cleared to false. |
Enable-in is true | The instruction executes as described in the Normal Operation section. |
Postscan | Same as Rung-condition-in is false. |
Examples

Provide Feedback