Redundant Input (RIN)

This instruction applies to the Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers.
Use the Redundant Input (RIN) instruction to emulate the input functionality of a safety relay in a software programmable environment.
Available Languages
Ladder Diagram
L5K_RIN_LD_v31avail.png
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
IMPORTANT: Make sure that your safety input modules are configured as single, not Equivalent or Complementary. These instructions provide all dual channel functionality necessary for PLd (Cat. 3) or PLe (Cat. 4) safety functions.
IMPORTANT: Unexpected operation, including controller assert or a Major Non-Recoverable Fault, can occur if:
  • Backing tag members are written to.
  • Backing tags are shared by multiple instruction invocations.
  • Backing tag members are passed as parameters to an instruction controlled by the same backing tag.
  • The backing tag
    .EnableIn
    member is referenced anywhere in the program.
    .EnableIn
    is a parameter that represents rung state into an instruction and is only intended for internal use.
    For examples of these incorrect backing tag usages, seeBacking tag usages that can cause unexpected operation.
This table explains the instructions inputs.
Parameter
Data Type
Description
Safe, Active, and Initial Values
RIN
REDUNDANT_INPUT
This parameter is a backing tag. As such, it maintains important execution information for each usage of this instruction. Do not attempt to reuse this backing tag or write to any of its members anywhere else in your program.
-
Reset Type
Boolean
The reset type determines whether the instruction is using Manual or Automatic reset for Output 1.
Manual (1) or Automatic (0)
Channel A
1
Boolean
Channel A Input (Normally Open)
Safe = 0
Active = 1
Channel B
1
Boolean
Channel B Input (Normally Open)
Safe = 0
Active = 1
Circuit Reset
Boolean
Circuit Reset Input
Manual Reset - Sets Output 1 after Channel A and Channel B are in the Active state, and the Circuit Reset input transitions from zero to one.
Automatic Reset - Visible, but not used.
Initial = 0
Reset = 1
Fault Reset
Boolean
After fault conditions are corrected for the instruction, the fault outputs for the instruction are cleared when this input transitions from off to on.
Initial = 0
Reset = 1
1
If this input is from a Guard I/O input module, make sure that the input is configured as single, not Equivalent or Complementary.
This table explains the instructions outputs.
Parameter
Data Type
Description
Safe, Active, and Initial Values
Output 1
Boolean
Output 1 is set to the Active state when input conditions are met.
Safe = 0, Active = 1
Cycle Inputs
Boolean
Cycle Inputs prompts for action. Before Output 1 is turned on, Channel A and Channel B inputs must be cycled through their Safe States at the same time before the circuit can be reset.
This prompt is cleared when Channel A and Channel B transition to the Safe state.
Initial = 0
Prompt = 1
Circuit Reset Held On
Boolean
Manual Reset - The Circuit Reset Held On prompt is set when both input channels transition to the Active states, and the Circuit Reset input is already on.
The Circuit Reset Held On prompt is cleared when the Circuit Reset input is turned off.
Automatic Reset - Visible, but not used.
Initial = 0
Prompt = 1
Inputs Inconsistent
Boolean
This fault is set when Channel A and Channel B inputs are in inconsistent states (one Safe and one Active) for a period of time greater than the Inconsistent Time Period (listed below). This fault is cleared when Channel A and Channel B inputs return to consistent states (both Safe or both Active) and the Fault Reset input transitions from off to on.
Inconsistent Time Period: 500 ms
Initial = 0
Fault = 1
Fault Present
Boolean
This value is set whenever a fault is present in the instruction. Output 1 cannot enter the Active state when Fault Present is set. Fault Present is cleared when all faults are cleared and the Fault Reset input transitions from off to on.
Initial = 0
Fault = 1
IMPORTANT: Do not write to any instruction output tag under any circumstances.
Operation
Normal Operation
This instruction monitors the states of two input channels and turns on Output 1 when the following conditions are met:
  • When using Manual Reset: both inputs are in the Active state and the Circuit Reset input is transitioned from a zero to a one.
  • When using Automatic Reset: both inputs are in the Active state for 50 ms.
This instruction turns Output 1 off when either one or both of the input channels returns to the Safe state.
Both input channels for the Redundant Input (RIN) instruction are normally open. This means zeros on both channels represent the Safe state, and ones on both channels represent the Active state.
These normal operation state changes are shown in the following timing diagrams:
RIN Manual and Automatic Reset diagrams
Operation with Inconsistent Inputs
This instruction generates a fault if the input channels are in inconsistent states (i.e., one Safe and one Active) for more than the specified period of time. The inconsistent time period is 500 ms.
This fault condition is enunciated via the Inputs Inconsistent and the Fault Present outputs. Output 1 cannot enter the Active state while the Fault Present output is active. The fault indication is cleared when the offending condition is remedied and the Fault Reset input is transitioned from zero to one.
These state changes are shown in the following timing diagram:
RIN Operation with Inconsistent Inputs
Operation with Circuit Reset Held On - Manual Reset Only
This instruction also sets the Circuit Reset Held On output prompt if the Circuit Reset input is set (1) when the input channels transition to the Active state.
These state changes are shown in the following timing diagram.
RIN Operation w circuit reset held ON
Cycle Inputs Operation
If, while Output 1 is active, one of the input channels transitions from the Active state to the Safe state and back to the Active state before the other input channel transitions to the Safe state, the Cycle Inputs output prompt is set, and Output 1 cannot enter the Active state again until both input channels cycle through their Safe states.
These state changes are shown in the following timing diagram:
RIN Cycle Inputs Operation
False Rung State Behavior
When the instruction is executed on a false rung the behavior is exactly the same as true rung state except all outputs, including prompts and fault indicators, will be zero. When the rung state becomes true the outputs will be set as determined by the instruction logic.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Condition/State
Action Taken
Prescan
The .O1, .CI, .CRHO, .II, and .FP are cleared to false.
Rung-condition-in is false
The instruction executes as described in the False Rung State Behavior section.
Rung-condition-in is true
The instruction executes as described in the Normal Operation section.
Postscan
The instruction executes as described in the False Rung State Behavior section.
Example
RIN_LD_ex_v31
Manual Reset Wiring Example
The following wiring diagram is one example of how to wire a 2-channel switch having two normally open contacts to a 1791DS Safety I/O module to comply with ISO 13849-1 Category 4.
RIN Redundant Input with Manual Reset wiring
Manual Reset Programming Example
The following programming example shows how the Redundant Input instruction with Manual Reset can be applied to the previous wiring diagram.
RIN_Other_Pg361_v31
ISO 13849-1 Category 4 requires that inputs be independently pulse tested. The
Logix Designer
programming application is used to configure the following I/O module parameters for pulse testing.
Input Configuration
Input Point
Type
Point Mode
Test Source
0 (IN0)
Single
Safety Pulse Test
0 (T0)
1 (IN1)
Single
Safety Pulse Test
1 (T1)
2 (IN2)
Single
Safety
None
3 (IN3)
Single
Safety
None
Test Output
Test Output Point
Point Mode
0 (T0)
Pulse Test
1 (T1)
Pulse Test
2 (T2)
Power Supply
3 (T3)
Not Used
Automatic Reset Wiring
The following wiring diagram is one example of how to wire a 2-channel switch having normally open contacts to a 1791DS Safety I/O module to comply with ISO 13849-1 Category 4.
IMPORTANT: Various safety standards (EN 60204, ISO 13849-1) requires that when using the Automatic Circuit Reset feature, other measures must be implemented to make sure that an unexpected or unintended startup will not occur in the system or application.
RIN inputs diagram
Automatic Reset Programming Example
The following programming example shows how the Redundant Input instruction with Automatic Reset can be applied to the wiring diagram shown above.
RIN_Other_Pg362_v31
ISO 13849-1 Category 4 requires that inputs be independently pulse tested. The
Logix Designer
programming application is used to configure the following I/O module parameters for pulse testing.
Input Configuration
Input Point
Type
Point Mode
Test Source
0 (IN0)
Single
Safety Pulse Test
0 (T0)
1 (IN1)
Single
Safety Pulse Test
1 (T1)
2 (IN2)
Single
Safety
None
Test Output
Test Output Point
Point Mode
0 (T0)
Pulse Test
1 (T1)
Pulse Test
2 (T2)
Power Supply
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal