FSBM wiring and programming example

This section demonstrates how to wire the Guard I/O module and program the instruction in the safety control portion of an application.
This application example complies with ISO 13849-1, Category 4 operation.
TIP: The standard control portion of the application is not shown in the following diagram.
Wiring Diagram
The wiring diagram shows how to wire a light curtain and four muting sensors to a 1791DS-IB12 module to illustrate the use of the Four-Sensor Bidirectional Muting instruction. The application includes a hold-to-run switch and a momentary push button for reset.
FSBM wiring and programming example
Programming Example
The programming diagram shows the Four-Sensor Bidirectional Muting instruction used with a DCI Stop (light curtain) and DCI Start (hold-to-run switch) instruction.
FSBM wiring and programming example
Ladder Diagram
FSBM_Other_LD_v31
Module Definition
The following sections provide examples of how to use the programming software to set the Guard I/O module configuration operands.
When defining the module, setting the Input Status to Combined Status-Muting provides the smallest input packet possible and lets the muting lamp status be monitored. Choosing Test for Output Data lets safety logic control Test Output 3 to drive the Muting Lamp and Test Output 2 to drive the Clear Area Lamp.
FSBM_mod defin_v31
Rockwell Automation
suggests using Exact Match, as shown. However, setting Electronic Keying to Compatible Match is allowed.
The safety inputs that interface with the Light Curtain (Points 1 and 2) are not pulse-tested because the Light Curtain pulse-tests its own signals.
Module Input Configuration
FSBM_mod input config_v31
Configuring Test Output 3 for Muting Lamp causes the I/O module to monitor the lamp that is connected to this output.
FSBM_test output_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal