Always False (AFI)

This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers.
The AFI instruction sets the EnableOut to false.
Available Languages
Ladder Diagram
AFI_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
Operands
Ladder Diagram
None
Description
The AFI instruction sets its EnableOut to false.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults
Execution
All conditions below the thick solid line can only occur during Normal Scan mode.
Condition
Action
Prescan
N/A
Rung-condition-in is false
Clear EnableOut to false.
Rung-condition-in is true
Clear EnableOut to false.
Postscan
N/A
Examples
Ladder Diagram
Use the AFI instruction to temporarily disable a rung while you are debugging a program. AFI disables all the instructions on this rung.
AFI_LD_ex_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal