Internal Model Control (IMC)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers.The Internal Model Control (IMC) instruction controls a single process variable by
manipulating a single control-variable output. This function block performs an algorithm
where the actual error signal is compared against that of an internal first-order lag plus
deadtime model of the process. The IMC function block calculates the control variable output
(CV) in the Auto mode based on the PV - SP deviation, internal model, and tuning.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram.
Function Block

Structured Text
IMC(IMC_tag);
Operands
Function Block
Operands: | Type: | Format | Description: |
IMC tag | INTERNAL MODEL CONTROL | Structure | IMC Structure |
Structured Text
Operands: | Type: | Format | Description: |
IMC tag | INTERNAL MODEL CONTROL | Structure | IMC Structure |
See
Structured Text Syntax
for more information on the syntax of expressions within structured text.
IMPORTANT:
Whenever an APC block detects a change in Delta Time (DeltaT), a
ModelInit will be performed. For this reason the blocks should only be run in one of the
TimingModes in which DeltaT will be constant.
- TimingMode = 0 (Periodic) while executing these function blocks in a Periodic Task
- TimingMode = 1 (Oversample)
In either case, if the Periodic Task time is dynamically changed, or the
OversampleDT is dynamically changed, the block will perform a ModelInit.
The
following TimingMode setting are not recommended due to jitter in DeltaT:
- TimingMode = 0 (Periodic) while executing these function blocks in a Continuous or Event Task
- TimingMode = 2 (RealTimeSample)
Structure
Input Parameters | Data Type | Description | Valid and Default Values |
---|---|---|---|
EnableIn | BOOL | Enable Input. If False, the function block will not execute and outputs are not updated. | Default=TRUE |
PV | REAL | Scaled process variable input. This value is typically read from an analog input module. | Valid = any float Default = 0.0 |
PVFault | BOOL | PV bad health indicator. If PV is read from an analog input, then PVFault will normally be controlled by the analog input fault status. If PVFault is TRUE, it indicates an error on the input module, set bit in Status. | Default = FALSE FALSE = Good Health |
PVUEMax | REAL | Maximum scaled value for PV. The value of PV and SP that corresponds to 100% span of the Process Variable. If PVEUMax ≤ PVEUMin, set bit in Status. | Valid = PVEUMin < PVEUMax ≤ maximum positive float Default = 100.0 |
PVUEMin | REAL | Minimum scaled value for PV. The value of PV and SP that corresponds to 0% span of the Process Variable. If PVEUMax ≤ PVEUMin, set bit in Status. | Valid = maximum negative float ≤ PVEUMin < PVEUMax Default = 0.0 |
SPProg | REAL | SP Program value, scaled in PV units. SP is set to this value when in Program control. If value of SPProg or SPOper < SPLLimit or > SPHLimit, set bit in Status and limit value used for SP. | Valid = SPLLimit to SPHLimit Default = 0.0 |
SPOper | REAL | SP Operator value, scaled in PV units. SP set to this value when in Operator
control. If value of SPProg or SPOper < SPLLimit or > SPHLimit, set bit in Status and limit value used for SP. | Valid = SPLLimit to SPHLimit Default = 0.0 |
SPCascade | REAL | SP Cascade value, scaled in PV units. If CascadeRatio mode and UseRatio is FALSE, then SP is set to this value, typically this will be CVEU of a primary loop. If CascadeRatio mode and UseRatio is TRUE, then SP is set to this value times Ratio. If value of SPCascade < SPLLimit or > SPHLimit, set bit in Status and limit value used for SP. | Valid = SPLLimit to SPHLimit Default = 0.0 |
SPHLimit | REAL | SP high limit value, scaled in PV units. If SPHLimit < SPLLimit or SPHLimit > PVEUMax, set bit in Status. | Valid = SPLLimit to PVEUMax Default = 100.0 |
SPLLimit | REAL | SP low limit value, scaled in PV units. If SPLLimit < PVEUMin, or SPHLimit < SPLLimit, set bit in Status and limit SP by using the value of SPLLimit. | Valid = PVEUMin to SPHLimit Default = 0.0 |
UseRatio | BOOL | Allow Ratio control permissive. Set TRUE to enable ratio control when in CascadeRatio mode. | Default = FALSE |
RatioProg | REAL | Ratio Program multiplier, no units (for example, scalar). Ratio and RatioOper are set to this value when in Program control. If RatioProg or RatioOper < RatioLLimit or > RatioHLimit, set bit in Status and limit value used for Ratio. | Valid = RatioLLimit to RatioHLimit Default = 1.0 |
RatioOper | REAL | Ratio Operator multiplier, no units (for example, scalar). Ratio is set to this value when in Operator control. If RatioProg or RatioOper < RatioLLimit or > RatioHLimit, set bit in Status and limit value used for Ratio. | Valid = RatioLLimit to RatioHLimit Default = 1.0 |
RatioHLimit | REAL | Ratio high limit value, no units (for example, scalar). Limits the value of Ratio obtained from RatioProg or RatioOper. If RatioLLimit < 0, set bit in Status and limit to zero. If RatioHLimit < RatioLLimit, set bit in Status and limit Ratio by using the value of RatioLLimit. | Valid = RatioLLimit to maximum positive float Default = 1.0 |
RatioLLimit | REAL | Ratio low limit value, no units (for example, scalar). Limits the value of Ratio obtained from RatioProg or RatioOper. If RatioLLimit < 0, set bit in Status and limit to zero. If RatioHLimit < RatioLLimit, set bit in Status and limit Ratio by using the value of RatioLLimit. | Valid = 0.0 to RatioHLimit Default = 1.0 |
CVFault | BOOL | Control variable bad health indicator. If CVEU controls an analog output, then CVFault will normally come from the analog output's fault status. If CVFault is TRUE, it indicates an error on the output module, set bit in Status. | Default = FALSE FALSE = Good Health |
CVInitReq | BOOL | CV initialization request. While TRUE, set CVEU to the value of CVInitValue. This signal will normally be controlled by the In Hold status on the analog output module controlled by CVEU or from the InitPrimary output of a secondary IMC loop. | Default = FALSE |
CVInitValue | REAL | CVEU initialization value, scaled in CVEU units. When CVInitializing is TRUE set CVEU equal to CVInitValue and CV to the corresponding percentage value. CVInitValue will normally come from the feedback of the analog output controlled by CVEU or from the setpoint of a secondary loop. The function block initialization is disabled when CVFaulted or CVEUSpanInv are TRUE (bad). | Valid = any float Default = 0.0 |
CVProg | REAL | CV Program-Manual value. CV is set to this value when in Program control and Manual mode. If value of CVProg or CVOper < 0 or > 100, or < CVLLimit or > CVHLimit when CVManLimiting is TRUE, set unique Status bit and limit value used for CV. | Valid = 0.0 to 100.0 Default = 0.0 |
CVOper | REAL | CV Operator-Manual value. CV is set to this value when in Operator control and Manual mode. If not Operator-Manual mode, set CVOper to the value of CV at the end of each function block execution. If value of CVProg or CVOper < 0 or > 100, or < CVLLimit or > CVHLimit when CVManLimiting is TRUE, set unique Status bit and limit value used for CV. | Valid = 0.0 to 100.0 Default = 0.0 |
CVOverrideValue | REAL | CV Override value. CV set to this value when in Override mode. This value should correspond to a safe state output of the IMC loop. If value of CVOverrideValue < 0 or >100, set unique Status bit and limit value used for CV. | Valid = 0.0 to 100.0 Default = 0.0 |
CVTrackValue | REAL | CV track value. When CVTrackReq is enabled and the IMC function block is in Manual, the CVTrackValue will be ignored, and the IMC internal model will update its historical data with the CVOper or CVProg value. When CVTrackReq is enabled and the IMC function block is in Auto, the internal model will update its historical data based on the value of CVTrackValue. The CV in this case will be allowed to move as if the IMC function block was still controlling the process. This is useful in multiloop selection schemes where you want the IMC function block to follow the output of a different controlling algorithm, where you would connect the output of the controlling algorithm into the CVTrackValue. | Valid = 0.0 to 100.0 Default = 0.0 |
CVManLimiting | BOOL | Limit CV in Manual mode request. If Manual mode and CVManLimiting is TRUE, CV will be limited by the CVHLimit and CVLLimit values. | Default = FALSE |
CVEUMax | REAL | Maximum value for CVEU. The value of CVEU that corresponds to 100% CV. If CVEUMax = CVEUMin, set bit in Status. | Valid = any float Default = 100.0 |
CVEUMin | REAL | Minimum value of CVEU. The value of CVEU that corresponds to 0% CV. If CVEUMax = CVEUMin, set bit in Status. | Valid = any float Default = 0.0 |
CVHLimit | REAL | CV high limit value. This is used to set the CVHAlarm output. It is also used for limiting CV when in Auto or CascadeRatio modes or Manual mode if CVManLimiting is TRUE. If CVLLimit < 0, if CVHLimit > 100, if CVHLimit < CVLLimit, set bit in Status. If CVHLimit < CVLLimit, limit CV by using the value of CVLLimit. | Valid = CVLLimit < CVHLimit ≤ 100.0 Default = 100.0 |
CVLLimit | REAL | CV low limit value. This is used to set the CVLAlarm output. It is also used for limiting CV when in Auto or CascadeRatio modes or Manual mode if CVManLimiting is TRUE. If CVLLimit < 0, if CVHLimit > 100, if CVHLimit < CVLLimit, set bit in Status. If CVHLimit < CVLLimit, limit CV by using the value of CVLLimit. | Valid = 0.0 ≤ CVLLimit < CVHLimit Default = 0.0 |
CVROCPosLimit | REAL | CV increasing rate of change limit, in percent per second. Rate of change limiting is only used when in Auto or CascadeRatio modes or Manual mode if CVManLimiting is TRUE. A value of zero disables CV ROC limiting. If value of CVROCPOSLimit < 0, set bit in Status and disable CV ROC limiting. | Valid = 0.0 to maximum positive float Default = 0.0 |
CVROCNegLimit | REAL | CV decreasing rate of change limit, in percent per second. Rate of change limiting is only used when in Auto or CascadeRatio modes or Manual mode if CVManLimiting is TRUE. A value of zero disables CV ROC limiting. If value of CVROCNegLimit < 0, set bit in Status and disable CV ROC limiting. | Valid = 0.0 to maximum positive float Default = 0.0 |
HandFB | REAL | CV HandFeedback value. CV set to this value when in Hand mode and HandFBFault is FALSE (good health). This value would typically come from the output of a field mounted hand/auto station and would be used to generate a bumpless transfer out of Hand mode. If value of HandFB < 0 or > 100, set unique Status bit and limit value used for CV. | Valid = 0.0…100.0 Default = 0.0 |
HandFBFault | BOOL | HandFB value bad health indicator. If the HandFB value is read from an analog input, then HandFBFault will normally be controlled by the status of the analog input channel. If HandFBFault is TRUE, it indicates an error on the input module, set bit in Status. | Default = FALSE FALSE = Good Health |
WindupHIn | BOOL | Windup high request. When TRUE, CV will not be allowed to increase in value. This signal will typically be the WindupHOut output from a secondary loop. | Default = FALSE |
WinduplIn | BOOL | Windup low request. When TRUE, CV will not be allowed to decrease in value. This signal will typically be the WindupLOut output from a secondary loop. | Default = FALSE |
GainEUSpan | BOOL | ModelGain units in EU or as % of span. CV ModelGain units in EU or % of span. Set to interpret ModelGain as EU, reset to interpret ModelGain as % of Span. | Default = FALSE TRUE = Gain in EU FALSE = Gain in % of span |
ProcessGainSign | BOOL | Used only for Autotuning. Sign of the process gain (Delta PV/Delta CV). Set to indicate a negative process gain (increase in output causes a decrease in PV). Reset to indicate a positive process gain (increase in output causes an increase in PV). | Default = FALSE |
ProcessType | DINT | Process type selection (1=Integrating, 0=non-integrating) | Default = 0 |
ModelGain | REAL | The internal model gain parameter. Enter a positive or negative gain depending on process direction. | Valid = maximum negative float −> maximum positive float Default = 0.0 |
ModelTC | REAL | The internal model time constant in seconds. | Valid = 0.0 to maximum positive float Default = 0.0 |
ModelDT | REAL | The internal model deadtime in seconds. | Valid = 0.0 to maximum positive float Default = 0.0 |
RespTC | REAL | The tuning parameter that determines the speed of the control variable action in seconds. | Valid = 0.0 to maximum positive float Default = 0.0 |
PVTracking | BOOL | SP track PV request. Set TRUE to enable SP to track PV. Ignored when in CascadeRatio or Auto modes. | Default = FALSE |
CVTrackReq | BOOL | CV Track request. Set true to enable CV Tracking when autotune is OFF. Ignored in Hand and Override mode. | Default = FALSE |
AllowCasRat | BOOL | Allow CascadeRatio mode permissive. Set TRUE to allow CascadeRatio mode to be selected by using either ProgCasRatReq or OperCasRatReq. | Default = FALSE |
ManualAfterInit | BOOL | Manual mode after initialization request. When TRUE, the function block will be placed in the Manual mode when CVInitializing is set TRUE unless the current mode is Override or Hand. When ManualAfterInit is FALSE, the function block's mode will not be changed. | Default = FALSE |
ProgProgReq | BOOL | Program Program Request. Set TRUE by the user program to request Program control. Ignored if ProgOperReq is TRUE. Holding this TRUE and ProgOperReq FALSE can be used to lock the function block into program control. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
ProgOperReq | BOOL | Program Operator Request. Set TRUE by the user program to request Operator control. Holding this TRUE can be used to lock the function block into operator control. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
ProgCasRatReq | BOOL | Program-Cascade/Ratio mode request. Set TRUE by the user program to request Cascasde/Ratio mode. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
ProgAutoReq | BOOL | Program-Auto mode request. Set TRUE by the user program to request Auto mode. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
ProgManualReq | BOOL | Program-Manual mode request. Set TRUE by the user program to request Manual mode. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
ProgOverrideReq | BOOL | Program-Override mode request. Set TRUE by the user program to request Override mode. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
ProgHandReq | BOOL | Program-Hand mode request. Set TRUE by the user program to request Hand mode. This value will usually be read as a digital input from a hand/auto station. When ProgValueReset is TRUE, the function block resets the input to FALSE. | Default = FALSE |
OperProgReq | BOOL | Operator Program Request. Set TRUE by the operator interface to request Program control. The function block resets this parameter to FALSE. | Default = FALSE |
OperOperReq | Operator Operator Request. Set TRUE by the operator interface to request Operator control. The function block will reset this parameter to FALSE. | Default = FALSE | |
OperCasRatReq | BOOL | Operator-CascadeRatio mode request. Set TRUE by the operator interface to request CascadeRatio mode. The function block will reset this parameter to FALSE. | Default = FALSE |
OperAutoReq | BOOL | Operator-Auto mode request. Set TRUE by the operator interface to request Auto mode. The function block will reset this parameter to FALSE. | Default = FALSE |
OperManualReq | BOOL | Operator-Manual mode request. Set TRUE by the operator interface to request Manual mode. The function block will reset this parameter to FALSE. | Default = FALSE |
ProgValueReset | BOOL | Reset Program control values. When TRUE, the Prog_xxx_Req inputs are reset to FALSE. When TRUE and Program control, set SPProg equal to SP and CVProg equal to CV. When ProgValueReset is TRUE, the function block resets this parameter to FALSE. | Default = FALSE |
TimingMode | DINT | Selects Time Base Execution mode. Value/Description 0 = Periodic mode 1 = Oversample mode 2 = Real time sampling mode For more information about timing modes, see Function Block Attributes. | Valid = 0…2 Default = 0 |
OverSampleDT | REAL | Execution time for Oversample mode. | Valid = 0 to max. TON_Timer elapsed time (4194.303 seconds) Default = 0 |
RTSTime | DINT | Module update period for Real Time Sampling mode. | Valid = 1 to 32,767 1 count = 1 ms |
RTSTimeStamp | DINT | Module time stamp value for Real Time Sampling mode. | Valid = 0 to 32,767 (wraps from 32,767 to 0) 1 count = 1 ms |
PVTuneLimit | REAL | PV tuning limit scaled in the PV units. When Autotune is running and predicted PV exceeds this limit, the tuning will be aborted. | Range: any float Default=0 |
AtuneTimeLimit | REAL | Maximum time for autotune to complete following the CV step change. When autotune exceeds this time, tuning will be aborted. | Valid range: any float > 0. Default = 60 minutes |
NoiseLevel | DINT | An estimate of the noise level expected on the PV to compensate for it during tuning. The selections are: 0=low, 1=medium, 2=high | Range: 0 to 2 Default=1 |
CVStepSize | REAL | CV step size in percent for the tuning step test. Step size is directly added to CV subject to high/low limiting. | Range: -100% … 100% Default=10% |
ResponseSpeed | DINT | Desired speed of closed loop response. Slow response: ResponseSpeed=0 Medium response: ResponseSpeed=1 Fast response: ResponseSpeed=2. If ResponseSpeed is less than 0, Slow response is used. If ResponseSpeed is greater than 2, Fast response is used. | Range: 0 to 2 Default=1 |
ModelInit | BOOL | Internal model initialization switch. | Default = FALSE |
Factor | REAL | Non-integrating model approximation factor. Only used for integrating process types. | Default = 100 |
AtuneStart | BOOL | Start Autotune request. Set True to initiate auto tuning of the function block. Ignored when IMC is not in Manual mode. The function block will reset this parameter to FALSE. | Default = FALSE |
AtuneUseModel | BOOL | Use Autotune model request. Set True to replace the current model parameters with the calculated Autotune model parameters. The function block sets the input parameter to FALSE. | Default = FALSE |
AtuneAbort | BOOL | Abort Autotune request. Set True to abort the auto tuning of the IMC function block. The function block sets input parameter to FALSE. | Default = FALSE |
Output Parameters | Data Type | Description | Valid and Default Values |
---|---|---|---|
EnableOut | BOOL | Indicates if instruction is enabled. Cleared to false if CVEU overflows. | |
CVEU | REAL | Scaled control variable output. Scaled by using CVEUMax and CVEUMin, where CVEUMax corresponds to 100% and CVEUMin corresponds to 0%. This output is typically used to control an analog output module or a secondary loop. CVEU = (CV * CVEUSpan / 100) + CVEUMin CVEU span calculation: CVEUSpan = ( CVEUMax − CVEUMin ) | |
CV | REAL | Control variable output. This value will always be expressed as 0…100%. CV is limited by CVHLimit and CVLLimit when in Auto or CascadeRatio mode or Manual mode if CVManLimiting is TRUE; otherwise limited by 0 and 100%. | |
DeltaCV | REAL | Difference between the Current CV and the previous CV (Current CV - previous CV). | |
CVInitializing | BOOL | Initialization mode indicator. Set TRUE when CVInitReq or function block FirstScan are TRUE, or on a TRUE to FALSE transition of CVFault (bad to good). CVInitializing is set FALSE after the function block has been initialized and CVInitReq is no longer TRUE. | |
CVHAlarm | BOOL | CV high alarm indicator. TRUE when the calculated value for CV > 100 or
CVHLimit. | |
CVLAlarm | BOOL | CV low alarm indicator. TRUE when the calculated value for CV < 0 or CVLLimit. | |
CVROCPosAlarm | BOOL | CV rate of change alarm indicator. TRUE when the calculated rate of change for CV exceeds CVROCPosLimit. | |
CVROCNegAlarm | REAL | CV rate of change alarm indicator. TRUE when the calculated rate of change for CV exceeds CVROCNegLimit. | |
SP | REAL | Current setpoint value. The value of SP is used to control CV when in the Auto, the CascadeRatio, or the PV Tracking mode, scaled in PV units. | |
SPPercent | REAL | The value of SP expressed in percent of span of PV. SPPercent = ((SP − PVEUMin ) * 100) / PVSpan where PVSpan = PVEUMax − PVEUMin | |
SPHAlarm | BOOL | SP high alarm indicator. TRUE when the SP ≥ SPHLimit. | |
SPLAlarm | BOOL | SP low alarm indicator. TRUE when the SP ≤ SPLLimit. | |
PVPercent | REAL | PV expressed in percent of span. PVPercent = (( PV − PVEUMin ) * 100) / PVSpan PV Span calculation: PVSpan =
( PVEUMax − PVEUMin ) | |
E | REAL | Process error. Difference between SP and PV, scaled in PV units. | |
EPercent | REAL | The error expressed as a percent of span. | |
InitPrimary | BOOL | Initialize primary loop command. TRUE when not in CasRat mode or when CVInitializing is TRUE. This signal normally would be used by the CVInitReq input of a primary loop. | |
WindupHOut | BOOL | Windup high indicator. TRUE when either a SP high or CV high/low limit has been reached. This signal will typically be used by the WindupHIn input to limit the windup of the CV output on a primary loop. | |
WindupLOut | BOOL | Windup low indicator. TRUE when either a SP or CV high/low limit has been reached. This signal will typically be used by the WindupLIn input to limit the windup of the CV output on a primary loop. | |
Ratio | REAL | Current ratio multiplier, no units. | |
RatioHAlarm | BOOL | Ratio high alarm indicator. TRUE when Ratio > RatioHLimit. | |
RatioLAlarm | BOOL | Ratio low alarm indicator. TRUE when Ratio < RatioLLimit. | |
ProgOper | BOOL | Program/Operator control indicator. TRUE when in Program control. FALSE when in Operator control. | |
CasRat | BOOL | CascadeRatio mode indicator. TRUE when in the CascadeRatio mode. | |
Auto | BOOL | Auto mode indicator. TRUE when in the Auto mode. | |
Manual | BOOL | Manual mode indicator. TRUE when in the Manual mode. | |
Override | BOOL | Override mode indicator. TRUE when in the Override mode. | |
Hand | BOOL | Hand mode indicator. TRUE when in the Hand mode. | |
DeltaT | REAL | Elapsed time between updates in seconds. | |
StepSizeUsed | REAL | Actual CV step size used for tuning. | |
GainTuned | REAL | The calculated value of the internal model gain after tuning is completed. | |
TCTuned | REAL | The calculated value of the internal model time constant after tuning is completed. | |
DTTuned | REAL | The calculated value of the internal model deadtime after tuning is completed. | |
RespTCTunedS | REAL | The calculated value of the control variable time constant in slow response speed after tuning is completed. | |
RespTCTunedM | REAL | The calculated value of the control variable time constant in medium response speed after tuning is completed. | |
RespTCTunedF | REAL | The calculated value of the control variable time constant in fast response speed after tuning is completed. | |
AtuneOn | BOOL | Set True when auto tuning has been initiated. | |
AtuneDone | BOOL | Set True when auto tuning has completed successfully. | |
AtuneAborted | BOOL | Set True when auto tuning has been aborted by user or due to errors that occurred during the auto tuning operation. | |
AtuneStatus | DINT | Indicates the block tuning status. | |
AtuneFault | BOOL | Autotune has generated any of the following faults. | Bit 0 of AtuneStatus |
AtunePVOutOfLimit | BOOL | Either PV or the deadtime-step ahead prediction of PV exceeds PVTuneLimit during Autotuning. When True, Autotuning is aborted. | Bit 1 of AtuneStatus |
AtuneModeInv | BOOL | The IMC mode was not Manual at start of Autotuning or the IMC mode was changed from Manual during Autotuning. When True, Autotuning is not started or is aborted. | Bit 2 of AtuneStatus |
AtuneCVWindupFault | BOOL | WindupHIn or WindupLIn is True at start of Autotuning or during Autotuning. When True, Autotuning is not started or is aborted. | Bit 3 of AtuneStatus |
AtuneStepSize0 | BOOL | StepSizeUsed = 0 at start of Autotuning. When True, Autotuning is not started. | Bit 4 of AtuneStatus |
AtuneCVLimitsFault | BOOL | CVLimitsInv and CVManLimiting are True at start of Autotuning or during Autotuning. When True, Autotuning is not started or is aborted. | Bit 5 of AtuneStatus |
AtuneCVInitFault | BOOL | CVInitializing is True at start of Autotuning or during Autotuning. When True, Autotuning is not started or is aborted. | Bit 6 of AtuneStatus |
AtuneEUSpanChanged | BOOL | CVEUSpan or PVEUSpan changes during Autotuning. When True, Autotuning is aborted. | Bit 7 of AtuneStatus |
AtuneCVChanged | BOOL | CVOper is changed when in Operatior control or CVProg is changed when in Program control or CV becomes high/low or ROC limited during Autotuning. When True, Autotuning is aborted. | Bit 8 of AtuneStatus |
AtuneTimeout | BOOL | Elapsed time is greater then AtuneTimeLimit since step test is started. When True, Autotuning is aborted. | Bit 9 of AtuneStatus |
AtunePVNotSettled | BOOL | The PV is changed too much to Autotune. When True, Autotuning is aborted. Wait until PV is more stable before autotuning. | Bit 10 of AtuneStatus |
Status1 | DINT | Bit mapped status of the function block. | |
Status2 | DINT | Additional bit mapped status for the function block. | |
InstructFault | BOOL | Function block has generated a fault. Indicates state of bits in Status1 and status2. A value of 0 indicates that no faults have occurred. Any parameters that could be configured with an invalid value must have a status parameter to indicate their invalid status. | Bit 0 of Status1 |
PVFaulted | BOOL | Process variable PV health bad. | Bit 1 of Status1 |
CVFaulted | BOOL | Control variable CV faulted | Bit 2 of Status1 |
HandFBFaulted | BOOL | HandFB value health bad | Bit 3 of Status1 |
PVSpanInv | BOOL | The span of PV invalid, PVEUMax < PVEUMin. | Bit 4 of Status1 |
SPProgInv | BOOL | SPProg < SPLLimit or > SPHLimit. Limit value used for SP. | Bit 5 of Status1 |
SPOperInv | BOOL | SPOper < SPLLimit or > SPHLimit. Limit value used for SP. | Bit 6 of Status1 |
SPCascadeInv | BOOL | SPCascade < SPLLimit or > SPHLimit. Limit value used for SP. | Bit 7 of Status1 |
SPLimitsInv | BOOL | Limits invalid: SPLLimit < PVEUMin, SPHLimit > PVEUMax, or SPHLimit < SPLLimit. If SPHLimit < SPLLimit, then limit value using SPLLimit. | Bit 8 of Status1 |
RatioLimitsInv | BOOL | Ratio high-low limits invalid, low limit < 0 or high limit < low limit. | Bit 9 of Status1 |
RatioProgInv | BOOL | RatioProg < RatioLLimit or > RatioHLimit. Limit value used for Ratio. | Bit 10 of Status1 |
RatioOperInv | BOOL | RatioOper < RatioLLimit or > RatioHLimit. Limit value used for Ratio. | Bit 11 of Status1 |
CVProgInv | BOOL | CVProg < 0 or > 100, or < CVLLimit or > CVHLimit when CVManLimiting is TRUE. Limit value used for CV. | Bit 12 of Status1 |
CVOperInv | BOOL | CVOper < 0 or > 100, or < CVLLimit or > CVHLimit when CVManLimiting is TRUE. Limit value used for CV. | Bit 13 of Status1 |
CVOverrideValueInv | BOOL | CVOverrideValue < 0 or > 100. Limit value used for CV. | Bit 14 of Status1 |
CVTrackValueInv | BOOL | CVTrackValue < 0 or > 100. Limit value used for CV. | Bit 15 of Status1 |
CVEUSpanInv | BOOL | The span of CVEU invalid, CVEUMax equals CVEUMin. | Bit 16 of Status1 |
CVLimitsInv | BOOL | CVLLimit < 0, CVHLimit > 100, or CVHLimit <= CVLLimit. If CVHLimit <= CVLLimit, limit CV by using CVLLimit. | Bit 17 of Status1 |
CVROCLimitInv | BOOL | CVROCLimit < 0, disables ROC limiting. | Bit 18 of Status1 |
HandFBInv | BOOL | HandFB < 0 or > 100. Limit value used for CV. | Bit 19 of Status1 |
SampleTimeTooSmall | BOOL | Model DeadTime / DeltaT must be less than or equal to 200. | Bit 20 of Status1 |
FactorInv | BOOL | Factor < 0. | Bit 21 of Status1 |
ModuleGainInv | BOOL | ModelGain is 1.#QNAN or -1.#IND (Not A Number), or ±1.$ ( Infinity ∞) | Bit 22 of Status1 |
ModelTCInv | BOOL | ModelTC < 0. | Bit 23 of Status1 |
ModelDTInv | BOOL | ModelDT < 0. | Bit 24 of Status1 |
RespTCInv | BOOL | RespTC < 0. | Bit 25 of Status1 |
TimingModelInv | BOOL | TimingMode invalid. If the current mode is not Override or Hand then set to Manual mode. | Bit 27 of Status2 |
RTSMissed | BOOL | Only used when in Real Time Sampling mode. Is TRUE when ABS(DeltaT - RTSTime) > 1 millisecond. | Bit 28 of Status2. |
RTSTimeInv | BOOL | RTSTime invalid. | Bit 29 of Status2. |
RTSTimeStampInv | BOOL | RTSTimeStamp invalid. If the current mode is not Override or Hand then set to Manual mode. | Bit 30 of Status2. |
DeltaTInv | BOOL | DeltaT invalid. If the current mode is not Override or Hand then set to Manual mode. | Bit 31 of Status2. |
Description
The following illustration shows the IMC function block configuration.

At each execution, the IMC function block compares the actual PV measurement with PV prediction. The result is called disturbance estimate, which is the effect of unmeasured process disturbances combined with the modeling imprecision. The disturbance estimate is used as a bias for the setpoint of the control variable. In the ideal case of no disturbances and perfect modeling, the disturbance estimate (the feedback signal) becomes equal to zero.
First Order Model | M = K/(T*s+1)*exp(-D*s) | |
Inverse of Model | Inv = (T*s+1)/K | |
First Order Filter | F = 1/(e*s+1) |
PV prediction = exp(-D*s)/(e*s+1) * (SP - Dist. estimate)
K... | Model gain |
T... | Model time constant |
D... | Model deadtime |
e... | Response time constant |
s... | Laplace variable |
The function block then calculates the CV value (CVHLimit, CVLLimit, and rate of change limits are imposed) and the PV prediction.
The IMC function block can be used in place of a PID function block with the advantage over the PID control variable when controlling processes with large deadtimes.
For an integrating process type (such as level control and position control), an internal nonintegrating model is used to approximate the integrating process. The Factor parameter is used to convert the identified integrating-process model to a nonintegrating internal model that is used for CV calculation. This is necessary to provide for stable IMC execution.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State | Action Taken |
---|---|
Prescan | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is false | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is true | EnableIn and .EnableOut bits are set to true. The instruction executes. |
Instruction first run | N/A |
Instruction first scan | N/A |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
Condition/State | Action Taken |
Prescan | See Prescan in the Function Block table. |
Normal Execution | See Tag.EnableIn is true in the Function Block table. |
Postscan | See Postscan in the Function Block table. |
Examples
Function Block

Structured Text
imcTag.PV := imcInput1;
imcTag.SPProg := imcInput2;
imcTag.CVProg := imcInput3;
IMC(imcTag);
imcOutput1 := imcTag.CVEU;
Provide Feedback