Configure X, Y arrays for Function Generator (FGEN) instructions

Use the
X, Y Arrays
tab on the
Properties
dialog to configure X and Y arrays for Function Generator (FGEN) instructions.
TIP: To open the X, Y Arrays tab on the Properties dialog:
  • In the editor, insert an FGEN instruction.
    When you add an FGEN instruction in a Function Block Diagram, Logix Designer creates a backing tag for the instruction.
    In the Ladder editor, you create a backing tag for the instruction: Select DotsIcon_v31 to open the
    Properties
    dialog.
  • On the instruction, select the
    Configuration
    icon DotsIcon_v31.
This table describes the parameters on the tab.
Parameter
Description
Table 1 Array
Select the tags for X1 Array and Y1 Array for Table 1. These arrays must be at least as
large as the displayed value for
Table 1 - # elements required
. This setting is controlled by the
XY1Size
parameter. Select the
Parameters
tab on the
Properties
dialog box to configure
XY1Size
. The values of the selected tag arrays appear in Table 1.
Table 2 Array (optional)
Select the tags for X2 Array and Y2 Array for Table 2. These arrays must be at least as
large as the displayed value for
Table 2 - # elements required
. This setting is controlled by the
XY2Size
parameter. Select the
Parameters
tab on the
Properties
dialog box to configure
XY2Size
. The values of the selected tag arrays appear in Table 2.
New Tag
Click
New Tag
to create a new tag for an array.
Status
Displays read-only status information for blocks containing status bits. If none of the status bits are set, an
OK
message appears in this field. Otherwise, a list of the status bits that are set appears here. This list is comprised of the parameter names associated with the status bits, and typically explain which parameters were configured with invalid values.
Execution Order Number (only applicable to Function Block Diagrams)
Displays the block's execution number if the routine is in a verified state. If the routine is not yet verified, a
Routine not verified
message displays. Note that this item is read-only.
Never display description in a routine (only applicable to Function Block Diagrams)
Select this check box to prevent the description from appearing in the routine.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal