Alarm (ALM)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers.
The Alarm (ALM) instruction provides alarming for any analog signal.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram logic.
Function Block
ALM_FB_avail_v31
Structured Text
ALM(ALM_tag)
Operands
Function Block
Operand
Type
Format
Description
ALM tag
ALARM
structure
ALM structure
Structured Text
Operand
Type
Format
Description
ALM tag
ALARM
structure
ALM structure
See
Structured Text Syntax
for more information on the syntax of expressions within structured text.
ALARM Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true.
In
REAL
The analog signal input.
Valid = any float
Default = 0.0
HHLimit
REAL
The high-high alarm limit for the input.
Valid = any real value
Default = maximum positive value
HLimit
REAL
The high alarm limit for the input.
Valid = any real value
Default = maximum positive value
LLimit
REAL
The low alarm limit for the input.
Valid = any real value
Default = maximum negative value
LLLimit
REAL
The low-low alarm limit for the input.
Valid = any real value
Default = maximum negative value
Less than or equal to Deadband
REAL
The alarm deadband for the high-high to low-low limits
Valid = any real value Greater than or equal to 0.0
Default = 0.0
ROCPosLimit
REAL
The rate-of-change alarm limit in units per second for a positive (increasing) change in the input. Set ROCPosLimit = 0 to disable ROC positive alarming. If invalid, the instruction assumes a value of 0.0 and sets the appropriate bit in Status.
Valid = any real value Less than or equal to 0.0
Default = 0.0
ROCNegLimit
REAL
The rate-of-change alarm limit in units per second for a negative (decreasing) change in the input. Set ROCNegLimit = 0 to disable ROC negative alarming. If invalid, the instruction assumes a value of 0.0 and sets the appropriate bit in Status.
Valid = any real value Less than or equal to 0.0
Default = 0.0
ROCPeriod
REAL
Time period in seconds for calculation (sampling interval) of the rate of change value. Each time the sampling interval expires, a new sample of In is stored, and ROC is re-calculated. Instead of an enable bit like other conditions in the analog alarm, the rate-of-change detection is enabled by putting any non-zero value in the ROCPeriod.
Valid = 0.0 to 32767.0
Default = 0.0.
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled. Cleared to false if ROC overflows.
HHAlarm
BOOL
The high-high alarm indicator.
Default = false
HAlarm
BOOL
The high alarm indicator.
Default = false
LAlarm
BOOL
The low alarm indicator.
Default = false
LLAlarm
BOOL
The low-low alarm indicator.
Default = false
ROCPosAlarm
BOOL
The rate-of-change positive alarm indicator.
Default = false
ROCNegAlarm
BOOL
The rate-of-change negative alarm indicator.
Default = false
ROC
REAL
The rate-of-change output.
Status
DINT
Status of the function block.
InstructFault (Status.0)
BOOL
The instruction detected one of the following execution errors. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
DeadbandInv (Status.1)
BOOL
Invalid Deadband value.
ROCPosLimitInv (Status.2)
BOOL
Invalid ROCPosLimit value.
ROCNegLimitInv (Status.3)
BOOL
Invalid ROCNegLimit value.
ROCPeriodInv (Status.4)
BOOL
Invalid ROCPeriod value.
Description
The ALM instruction provides alarm indicators for high-high, high, low, low-low, rate-of-change positive, and rate-of-change negative. An alarm deadband is available for the high-high to low-low alarms. A user-defined period for performing rate-of-change alarming is also available.
High-high to Low-low Alarm
The high-high and low-low alarm algorithms compare the input to the alarm limit and the alarm limit plus or minus the deadband.
ALM_High to High Low to Low
Rate-of-change Alarm
The rate-of-change (ROC) alarm compares the change of the input over the ROCPeriod to the rate-of-change limits. The ROCPeriod provides a type of deadband for the rate-of-change alarm. For example, define an ROC alarm limit of 2
O
F/second with a period of execution of 100 ms. If you use an analog input module with a resolution of 1
O
F, every time the input value changes, an ROC alarm is generated because the instruction calculates an effective rate of 10°F/second. However, enter an ROCPeriod of 1 sec and the instruction only generates an alarm if the rate truly exceeds the 2
O
F/second limit.
The ROC alarm calculates the rate-of-change as:
ALM_Rate of Change
The instruction performs this calculation when the ROCPeriod expires. Once the instruction calculates the ROC, it determines alarms as:
ALM Determine alarms
Monitoring the ALM Instruction
There is an operator faceplate available for the ALM instruction.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See
Common Attributes
for operand-related faults.
Execution
Function Block
Condition/State
Action Taken
Prescan
Rung-condition-in bits are cleared to false.
Rung-condition-in is false
Rung-condition-in bits are cleared to false.
Rung-condition-in is true
Rung-condition-in bits are set to true.
The instruction executes.
Postscan
Rung-condition-in bits are cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal Execution
See Rung-condition-in is true in the Function Block table.
Postscan
See Postscan in the Function Block table.
Example
The ALM instruction is typically used either with analog input modules (such as 1771 I/O modules) that do not support on-board alarming, or to generate alarms on a calculated variable. In this example, an analog input from a 1771-IFE module is first scaled to engineering units using the SCL instruction. The Out of the SCL instruction is an input to the ALM instruction to determine whether to set an alarm. The resulting alarm output parameters could then be used in your program and/or viewed on an operator interface display.
Function Block
ALM_FB_ex_v31
Structured Text
SCL_01.IN := Input0From1771IFE;
SCL(SCL_01);
ALM_01.IN := SCL_01.Out;
ALM(ALM_01);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal