Process Run Time and Start Counter (PRT)
This information applies to CompactLogix 5380P, ControlLogix 5580P, and ControlLogix 5590P
controllers.
The Process Run Time and Start Counter (PRT) instruction records the total run time and number of instances the motor or other equipment starts. The PRT is a software implementation of the mechanical hour meter that displays the total motor runtime. Maintenance personnel use the run time and equipment start variables to create a maintenance schedule for the applicable equipment.
Available Languages
Ladder Diagram

Function Block Diagram

Structured Text
PRT(PRT_01);
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand | Type | Format | Description |
---|---|---|---|
PRT | P_RUN_TIME | tag | PRT structure |
P_RUN_TIME Structure
Public Input Members | Data Type | Description |
---|---|---|
EnableIn | BOOL | Enable Input – System Defined Parameter. |
Inp_Starting | BOOL | 1 = Equipment is starting. Default = false. |
Inp_Running | BOOL | 1 = Equipment is confirmed running. Default = true. |
PCmd_ClearStarts | BOOL | Program Command to clear count of starts. The instruction clears this operand automatically. Default = false. |
PCmd_ClearMaxHrs | BOOL | Program Command to clear the maximum, continuous runtime for any start. The instruction clears this operand automatically. Default = false. |
PCmd_ClearTotHrs | BOOL | Program Command to clear the total run time. The instruction clears this operand automatically. Default = false. |
Public Output Members | Data Type | Description |
---|---|---|
EnableOut | BOOL | Enable Output – System Defined Parameter. |
Val_Starts | DINT | Total number of equipment starts or attempts. |
Val_CurRunHrs | REAL | Current running time this start (hours). |
Val_MaxRunHrs | REAL | Maximum continuous running time for a given start (hours). |
Val_TotRunHrs | REAL | Total accumulated running time (hours). |
Private Input Members | Data Type | Description |
---|---|---|
MCmd_ClearStarts | BOOL | Maintenance Command to clear count of starts. The instruction clears this operand automatically. Default = false. |
MCmd_ClearMaxHrs | BOOL | Maintenance Command to clear the maximum, continuous runtime for any start. The instruction clears this operand automatically. Default = false. |
MCmd_ClearTotHrs | BOOL | Maintenance Command to clear the total run time. The instruction clears this operand automatically. Default = false. |
Operation
The PRT instruction:
- Accumulates and displays the total running time for the associated equipment.
- Accumulates and displays the count of starts or start attempts for the associated equipment.
- Shows the amount of run time since the last start, or the length of the current run. This total is held after the equipment is stopped, until the next start, when it is reset to zero.
- Shows the maximum amount of time for any single run; this is the highest value achieved by the previous total.
- Allows maintenance personnel, but not operators, to clear individually the total run time, starts count, or maximum single run time. This lets the times be reset when the motor or other equipment is serviced, rebuilt or replaced.
This diagram illustrates the functionality of the PRT instruction:

Configuration of Strings for HMI
Configure strings for HMI faceplates (
FactoryTalk View
) and for the Logix Designer
configuration dialog box. The strings are set to extended properties of tag items. Configure the strings in the Logix Designer
application only.- Description
- Label for graphic symbol
- Display Library for HMI Faceplate call-up
- Instruction name
- Area name
- URL link
Implementation
Normal Ladder implementation
This illustration shows normal implementation with the input condition mapped to Inp_Running and Inp_Starting on a separate branch.

Rung-in-condition Ladder Implementation
The PRT instruction is designed so it can be used on a Ladder Diagram rung, using the rung-in condition to provide the state of the motor, running (rung-in condition TRUE) or stopped (rung-in condition FALSE):

When the motor is starting or running, the main logic of the PRT instruction is executed.
For this to accumulate run time, the parameter Inp_Running must be set to 1. When the motor
is stopped, the rung is false and the EnableInFalse logic of the PRT instruction is
executed, and the motor is treated as stopped.
Function Block Implementation (Inp_Running pin always indicates 1)
To ensure that a Ladder Diagram implementation of this application works correctly and that starts and run time are accumulated, the PRT instruction writes a 1 into Inp_Running each scan after executing its logic. This helps avoid having the input inadvertently cleared to 0, which results in the PRT instruction treating the motor as always stopped.
A side effect of this is that when monitoring a Function Block Diagram implementation of this strategy with input pin values displayed, the Inp_Running pin will always show a value of 1, even though the logic on the wire is correctly sending a 0 to the instruction:

This is normal, and the PRT instruction correctly accumulates starts and run time.
NOTE:
This discrepancy is only apparent if the Function Block Diagram editor is configured to display the value of connected (wired) input pins.
To show the value of these pins in the editor:
- In the Logix Designer application, selectTools > Optionsto open the Workstation Options dialog.
- In the Categories list, selectFBD Editor.
- SelectShow values of Input Pins. Make sure theUnwired Pins Onlycheck box is not selected.
Monitor the PRT instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | Total run time, Maximum run time and starts count are retained through a power cycle. Current run time is reset (internally only, Val_CurHours is maintained for display). All Prog, Maint, commands that are automatically cleared each execution are cleared. |
Instruction first run | Total run time, Maximum run time and starts count are retained through a power cycle. Current run time is reset (internally only, Val_CurHours is maintained for display). All Prog, Maint, commands that are automatically cleared each execution are cleared. |
Rung-condition-in is false | EnableIn False is treated the same as Motor Stopped: Commands are still processed, total run time is held, the Starts counter is prepared for the next start, and the Current Run Time is cleared. Command Processing This object has no Command Source and commands are accepted regardless of Source. Commands should be restricted to authorized personnel (typically at a maintenance level).
|
Rung-condition-in is true | Set rung-condition-out to rung-condition-in. The instruction executes. |
Function Block Diagram
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in the Ladder Diagram table. |
Instruction first run | See Instruction first run in the Ladder Diagram table. |
Instruction first scan | See Instruction first run in the Ladder Diagram table. |
EnableIn is false | See Rung-condition-in is false in the Ladder Diagram table. |
EnableIn is true | See Rung-condition-in is true in the Ladder Diagram table. |
Structured Text
In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic, it will execute.
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in the Ladder Diagram table. |
Instruction first run | See Instruction first run in the Ladder Diagram table. |
EnableIn is true | See Rung-condition-in is true in the Ladder Diagram table. |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Example
In the following example, tag A100_MR_001 is the motor value monitored by the PRT instruction. This tag provides a Boolean indication of motor run time value.
Inp_Running is connected to the Motor Running status tag (A100_MR_001.Sts_Running) that comes from the Sts_Running output of the P_Motor instruction instance for this motor (A100_MR_001). Inp_Starting is connected to the Motor Starting status tag (A100_MR_001.Sts_Starting) that comes from the Sts_Starting output of the P_Motor instruction instance for this motor (A100_MR_001).
Finally, A100_MR_001_RT.Val_TotRunHrs is the output tag that will indicate the total running hours of A100_MR_001. There is also current running hours (A100_MR_001_RT.Val_CurRunHrs) of the motor and maximum running hours (A100_MR_001_RT.Val_MaxRunHrs) of the motor available.
Ladder Diagram

Function Block Diagram

Structured Text
PRT_01.Inp_Starting:=A100_MR_001.Sts_Starting;
PRT_01.Inp_Running:=A100_MR_001.Sts_Running;
PRT(PRT_01);
Provide Feedback