Process Analog HART (PAH)
This information applies to CompactLogix 5380P, ControlLogix 5580P, and ControlLogix 5590P
controllers.
The Process Analog HART (PAH) instruction is used to provide HART digital data for an intelligent analog device alongside the analog input (PAI) or analog output (PAO) instruction for that device. It provides:
- HART Dynamic Variables (PV, SV, TV and QV) values with engineering units and variable status, and the digital value of the device’s analog loop current (in milliamps DC).
- Analog range (min, at 4 mA, and max, at 20 mA).
- Analog units of measure.
- Device information such as Tag and Description text.
- Additional device status (HART “Command 48 additional status” bit array).
- Lookup of diagnostic message and severity based on the Command 48 bits that are set (for the first three diagnostics found in the array).
- Additional status information received from the device via HART, such as Field Device Status bits.
Available Languages
Ladder Diagram

Function Block Diagram

Structured Text
PAH(PAH_tag, Ref_HARTData, Ref_DiagTable, Ref_UnitsTable)
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand | Type | Format | Description |
---|---|---|---|
PlantPAx ControlPlantPAx Control | P_ANALOG_HART | tag | Data structure required for proper operation of instruction. |
Ref_HARTData | PAX_HART_DEVICE:I:0 | tag | HART device data for PlantPAx. |
Ref_DiagTable | P_HART_CODE_DESC_STATUS[2] | tag | Lookup table for diagnostic bit number (to message and status). |
Ref_UnitsTable | RAC_CODE_DESCRIPTION[2] | tag | Lookup table for units of measure code (to units text). |
The PAX_HART_DEVICE:I:0 data type is associated with the Add-On Profile for Highly Integrated HART modules such as the 5094-IF8IH.
P_ANALOG_HART Structure
Public members are standard, visible tag members that are programmatically accessible. Private, hidden members are used in HMI faceplates and are not programmatically accessible. Private members are listed in separate tables after public members.
Public Input Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
---|---|---|---|---|---|
EnableIn | BOOL | Not Visible | Not Required | Input | Enable input. Ladder Diagram: Corresponds to the rung condition. Default is true. |
Inp_InitializeReq | BOOL | Not Visible | Not Required | Input | 1 = Request to initialize the instruction. The instruction is normally initialized in instruction first run. Use this request to re-initialize. The instruction clears this operand automatically. Default is true. |
Cfg_HasHARTPV | BOOL | Not Visible | Not Required | Input | 1 = Has a HART digital PV, display on faceplate; 0 = HART digital PV not used. Default is false. |
Cfg_HasHARTSV | BOOL | Not Visible | Not Required | Input | 1 = Has a HART digital SV, display on faceplate; 0 = HART digital SV not used. Default is false. |
Cfg_HasHARTTV | BOOL | Not Visible | Not Required | Input | 1 = Has a HART digital TV, display on faceplate; 0 = HART digital TV not used. Default is false. |
Cfg_HasHARTQV | BOOL | Not Visible | Not Required | Input | 1 = Has a HART digital QV, display on faceplate; 0 = HART digital QV not used. Default is false. |
Cfg_UseHARTVarSts | BOOL | Not Visible | Not Required | Input | 1 = Use HART Communication Status to generate SrcQ, 0 = assume good. Default is true. |
Cfg_UseHARTText | BOOL | Not Visible | Not Required | Input | 1 = Use text received from HART device, 0 = use extended properties for text. Default is false. |
Cfg_HARTPVDecPlcs | SINT | Not Visible | Not Required | Input | Number of decimal places for HART PV display. Valid = 0,1,2,3,4,5,6. Default is 2. |
Cfg_HARTSVDecPlcs | SINT | Not Visible | Not Required | Input | Number of decimal places for HART SV display. Valid = 0,1,2,3,4,5,6. Default is 2. |
Cfg_HARTTVDecPlcs | SINT | Not Visible | Not Required | Input | Number of decimal places for HART TV display. Valid = 0,1,2,3,4,5,6. Default is 2. |
Cfg_HARTQVDecPlcs | SINT | Not Visible | Not Required | Input | Number of decimal places for HART QV display. Valid = 0,1,2,3,4,5,6. Default is 2. |
Cfg_HasMoreObj | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI an object with more information is available for navigation. Default is false. |
Cfg_HasNav | BOOL | Not Visible | Not Required | Input | 1 = Tells HMI a related analog input or output object is available for navigation. Default is false. |
Set_VirtualHARTPV | REAL | Not Visible | Not Required | Input | HART PV used in Virtual (when Sts_Virtual = 1) (PV engineering units). Default is 0.0. |
Set_VirtualHARTSV | REAL | Not Visible | Not Required | Input | HART SV used in Virtual (when Sts_Virtual = 1) (SV engineering units). Default is 0.0. |
Set_VirtualHARTTV | REAL | Not Visible | Not Required | Input | HART TV used in Virtual (when Sts_Virtual = 1) (TV engineering units). Default is 0.0. |
Set_VirtualHARTQV | REAL | Not Visible | Not Required | Input | HART QV used in Virtual (when Sts_Virtual = 1) (QV engineering units). Default is 0.0. |
PCmd_Virtual | BOOL | Not Visible | Not Required | Input | Program command to select Virtual (simulated) device operation. The instruction clears this operand automatically. Default is false. |
PCmd_Physical | BOOL | Not Visible | Not Required | Input | Program command to select Physical device operation (not simulated). The instruction clears this operand automatically. Default is false. |
Public Output Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
---|---|---|---|---|---|
EnableOut | BOOL | Not Visible | Not Required | Output | This output state always reflects EnableIn input state. |
Val_HARTPV | REAL | Visible | Not Required | Output | Digital HART PV value in PV engineering units (after Substitution, if used). |
Val_HARTSV | REAL | Visible | Not Required | Output | Digital HART SV value in SV engineering units (after Substitution, if used). |
Val_HARTTV | REAL | Visible | Not Required | Output | Digital HART TV value in TV engineering units (after Substitution, if used). |
Val_HARTQV | REAL | Visible | Not Required | Output | Digital HART QV value in QV engineering units (after Substitution, if used). |
Val_HARTLoopCurrent | REAL | Visible | Not Required | Output | Digital HART value for Loop Current in milliamps. |
Val_InpRawMinFromHART | REAL | Not Visible | Not Required | Output | Analog input unscaled signal minimum from HART module (in module units). |
Val_InpRawMaxFromHART | REAL | Not Visible | Not Required | Output | Analog input unscaled signal maximum from HART module (in module units). |
Val_PVEUMinFromHART | REAL | Not Visible | Not Required | Output | Analog input scaled range minimum from HART device (in engineering units). |
Val_PVEUMaxFromHART | REAL | Not Visible | Not Required | Output | Analog input scaled range maximum from HART device (in engineering units). |
Sts_eHARTDiagCode1 | INT | Not Visible | Not Required | Output | HART Diagnostic Code #1 (bit number in Command 48, 255 = none). |
Sts_eHARTDiagCode2 | INT | Not Visible | Not Required | Output | HART Diagnostic Code #2 (bit number in Command 48, 255 = none). |
Sts_eHARTDiagCode3 | INT | Not Visible | Not Required | Output | HART Diagnostic Code #3 (bit number in Command 48, 255 = none). |
Sts_bHARTDiagSts | SINT | Not Visible | Not Required | Output | Overall HART diagnostic status, .0 = Info, .1 = Maintenance Required, .2 = Off Specification, .3 = Function Check, .4 = Failed. |
Sts_bHARTDiagSts1 | SINT | Not Visible | Not Required | Output | Diagnostic status for HART Diagnostic Code #1, .0 = Info, .1 = Maintenance Required, .2 = Off Specification, .3 = Function Check, .4 = Failed. |
Sts_bHARTDiagSts2 | SINT | Not Visible | Not Required | Output | Diagnostic status for HART Diagnostic Code #2, .0 = Info, .1 = Maintenance Required, .2 = Off Specification, .3 = Function Check, .4 = Failed. |
Sts_bHARTDiagSts3 | SINT | Not Visible | Not Required | Output | Diagnostic status for HART Diagnostic Code #3, .0 = Info, .1 = Maintenance Required, .2 = Off Specification, .3 = Function Check, .4 = Failed. |
Sts_Initialized | BOOL | Not Visible | Not Required | Output | 1 = Instruction is initialized. Use Inp_InitializeReq to reinitialize. |
Sts_Virtual | BOOL | Not Visible | Not Required | Output | 1 = Using virtual PV instead of the input from the device (Inp_PVData) to calculate output. 0 = The instruction uses input parameter Inp_PVData to calculate output. Sts_Virtual is a copy of Inp_Virtual. |
Sts_ConnectionFault | BOOL | Not Visible | Not Required | Output | 1 = HART data input connection fault, 0 = connection OK. |
Sts_DvcMalfunction | BOOL | Not Visible | Not Required | Output | 1 = HART device reports it has a malfunction. |
Sts_CurrentSaturated | BOOL | Not Visible | Not Required | Output | 1 = HART reports analog current is limited. |
Sts_CurrentFixed | BOOL | Not Visible | Not Required | Output | 1 = Loop Current set to fixed value via HART command. |
Sts_CurrentMismatch | BOOL | Not Visible | Not Required | Output | 1 = Loop Current reported via HART does not match analog signal. |
Sts_DiagnosticActive | BOOL | Not Visible | Not Required | Output | 1 = HART data input diagnostic active. |
Val_DiagnosticSeqCount | SINT | Not Visible | Not Required | Output | HART data input diagnostic sequence count (per change in diagnostic data, wraps). |
SrcQ_IO | SINT | Not Visible | Not Required | Output | Source and quality of primary input or output (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ | SINT | Not Visible | Not Required | Output | Source and quality of primary value or status (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ_HARTPV | SINT | Not Visible | Not Required | Output | Source and quality of HART digital PV (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ_HARTSV | SINT | Not Visible | Not Required | Output | Source and quality of HART digital SV (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ_HARTTV | SINT | Not Visible | Not Required | Output | Source and quality of HART digital TV (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ_HARTQV | SINT | Not Visible | Not Required | Output | Source and quality of HART digital QV (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
SrcQ_HARTLoopCurrent | SINT | Not Visible | Not Required | Output | Source and quality of HART loop current value (enumerated): 0=Good, live, confirmed good 1=Good, live, assumed good 2=Good, no feedback, assumed good 8=Test, virtualized 9=Test, loopback 10=Test, manually entered 16=Uncertain, live, off-spec 17=Uncertain, substituted at device or bus 18=Uncertain, substituted at instruction 19=Uncertain, using last known good 20=Uncertain, using replacement value 32=Bad, signal failure 33=Bad, channel fault 34=Bad, module or communication fault 35=Bad, invalid configuration |
Sts_eSts | SINT | Not Visible | Not Required | Output | Device confirmed status: 0 = Live, 1 = diagnostic information, 2 = maintenance required, 3 = off-spec (uncertain), 4 = function check (substituted), 5 = failure, 6 = HART communication lost, 7 = Virtualized. |
Sts_eFault | INT | Not Visible | Not Required | Output | Device fault status: 0 = None, 1 = a dynamic variable is bad, 2 = device diagnostic indicates a failure, 3 = HART communication lost, 4 = module connection fault, 5 = device reports malfunction. |
Val_HARTRevision | SINT | Not Visible | Not Required | Output | HART Spec major revision received from device. |
Private Input Members | Data Type | Description |
---|---|---|
MCmd_Physical | BOOL | Maintenance command to select Physical device operation (not simulated). The instruction clears this operand automatically. Default is false. |
MCmd_Virtual | BOOL | Maintenance command to select Virtual (simulated) device operation. The instruction clears this operand automatically. Default is false. |
Private Output Members | Data Type | Description |
---|---|---|
MRdy_Physical | BOOL | 1 = Ready for MCmd_Physical, enable HMI button. |
MRdy_Virtual | BOOL | 1 = Ready for MCmd_Virtual, enable HMI button. |
Sts_sHARTDesc | String_16 | Description text from HART device. |
Sts_sHARTDiagMsg1 | String_32 | HART device diagnostic message #1. |
Sts_sHARTDiagMsg2 | String_32 | HART device diagnostic message #2. |
Sts_sHARTDiagMsg3 | String_32 | HART device diagnostic message #3. |
Sts_sHARTPVEU | String_16 | Text of HART digital PV's engineering units. |
Sts_sHARTQVEU | String_16 | Text of HART digital QV's engineering units. |
Sts_sHARTSVEU | String_16 | Text of HART digital SV's engineering units. |
Sts_sHARTTag | String_32 | Tag text from HART device. |
Sts_sHARTTVEU | String_16 | Text of HART digital TV's engineering units. |
Sts_sPVEU | String_16 | Text of analog PV's engineering units. |
Public InOut Members | Data Type | FBD Default Visibility | FBD Wiring required | Usage | Description |
---|---|---|---|---|---|
Ref_HARTData | PAX_HART_DEVICE:I:0 | Visible | Required | InOut | HART data from I/O module assembly. |
Ref_DiagTable | P_HART_CODE_DESC_STATUS[2] | Visible | Required | InOut | Lookup table for diagnostic bit number (to message and status). |
Ref_UnitsTable | RAC_CODE_DESCRIPTION[2] | Visible | Required | InOut | Lookup table for units of measure code (to units text). |
PAX_HART_DEVICE:I:O Structure
The PAX_HART_DEVICE:I:O structure is the input assembly subtype used by Highly-Integrated HART I/O modules to provide all the HART data required for this instruction:
Members | Data Type | Description |
---|---|---|
RunMode | BOOL | Always 0, not used by this instruction |
ConnectionFaulted | BOOL | The network connection to the I/O module has been lost |
DiagnosticActive | BOOL | I/O module has at least one diagnostic available |
DiagnosticSequenceCount | SINT | This count increments each time the diagnostic information from the I/O module changes. It counts to +127, then loops back to -128, skipping zero. |
CurrentSaturated | BOOL | The analog signal has reached its minimum or maximum value and does not represent the actual process variable |
CurrentFixed | BOOL | The analog signal has been fixed by command and does not represent the actual process variable |
MoreStatusAvailable | BOOL | At least one Command 48 (additional device status) bit is set and diagnostics should be displayed |
CurrentMismatch | BOOL | I/O module reports digital value for loop current and actual analog loop current disagree significantly |
ConfigurationChanged | BOOL | Device reports configuration data (scaling, text, units) have changed |
Malfunction | BOOL | Device reports malfunction detected |
LoopCurrent | CHANNEL_AI:I:O | HART digital value for device analog loop current (mA DC) |
PV | CHANNEL_AI_HART:I:O | HART dynamic Primary Variable with units and status |
SV | CHANNEL_AI_HART:I:O | HART dynamic Secondary Variable with units and status |
TV | CHANNEL_AI_HART:I:O | HART dynamic Tertiary Variable with units and status |
QV | CHANNEL_AI_HART:I:O | HART dynamic Quaternary Variable with units and status |
Static | AB_5000_HART_Static_Struct:I:O | HART "static" data, such as device scale range, analog signal units of measure, and device text strings for description and tag name |
ChDataAtSignal4 | REAL | The value provided by the I/O module analog channel when a 4.0 mA DC signal is received, provided for scaling use by an associated PAI or PAO instruction |
ChDataAtSignal20 | REAL | The value provided by the I/O module analog channel when a 20.0 mA DC signal is received, provided for scaling use by an associated PAI or PAO instruction |
P_HART_CODE_DESC_STATUS Structure
The P_HART_CODE_DESC_STATUS structure is used to look up the diagnostic text and device status associated with a particular Command 48 diagnostic bit. The device provides a 200-bit (25 byte) array of data, where each bit set indicates a particular diagnostic condition. An array of members of this type is used to allow the instruction to display a text description and status for a given bit.
This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, the diagnostic bit lookup function is not performed.
Members | Data Type | Description |
---|---|---|
Code | DINT | Diagnostic code. This is the diagnostic bit number (0 to 199) in the array of 200 bits returned in HART Command 48 (Additional Device Status), or -1 if no diagnostic bit is set. |
Desc | STRING_32 | Diagnostic text. |
bSts | SINT | Device Status (bitmapped): .0 = Information .1 = Maintenance Required .2 = Off Specification .3 = Function Check .4 = Failed |
RAC_CODE_DESCRIPTION[x] Structure
The RAC_CODE_DESCRIPTION[x] structure is an array of engineering unit code numbers and corresponding engineering units text pairs, used as a lookup table. The instruction searches the table for the engineering units code received from the device and displays the corresponding engineering unit text for the variable. This parameter links the instruction to an external tag that contains necessary data for the instruction to operate. The external tag must be of the data type shown, or may be NULL. If NULL, the unit code lookup function is not performed.
Members | Data Type | Description |
---|---|---|
Code | DINT | Code for which to look up Description. |
Desc | STRING | Description for given Code. |
Operation
This diagram illustrates functionality of the PAH instruction:

Virtualization
Use virtualization for instruction testing and operator training. Command virtual operation using program command PCmd_Virtual or maintenance command MCmd_Virtual. After finishing virtual operation, use program command PCmd_Physical or maintenance command MCmd_Physical to return to normal physical device operation.
When Virtualization is active, the output dynamic variable (PV, SV, TV, QV) values of the PAH instruction are set using Virtual value settings (Set_VirtualPV, etc.) and I/O faults are ignored. Manipulate the instruction to operate as if a working HART process device were present.
Initialization
The instruction is normally initialized in the instruction first run. Request re-initialization by setting Inp_InitializeReq = 1. For proper initialization, when adding the instruction while performing an online edit of the code, make sure that Inp_InitializeReq = 1, the default value.
Configuration of Strings for HMI
Configure strings for HMI faceplates (FT View) and for the Logix Designer configuration dialog box. The strings are set to extended properties of tag items.
- Description
- Label for graphic symbol
- Display Library for HMI Faceplate call-up
- Instruction name
- Area name
- URL link
- Engineering units for raw analog signal
- Engineering units for analog signal PV
- Engineering units for HART PV
- Engineering units for HART SV
- Engineering units for HART TV
- Engineering units for HART QV
- Label for HART PV
- Label for HART SV
Monitor the PAH Instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | Instruction flagged for initialization on first scan / first run |
Instruction first run | Internal data such as pointers and timers are initialized |
Rung-condition-in is false | Set rung-condition-out to rung-condition-in. The instruction executes. HART data, units and status are provided. |
Rung-condition-in is true | Set rung-condition-out to rung-condition-in. The instruction executes. HART data, units and status are provided. |
Postscan | Rung-condition-out is cleared to false. |
Function Block Diagram
Condition/State | Action Taken |
---|---|
Prescan | Instruction flagged for initialization on first scan / first run |
Instruction first run | Internal data such as pointers and timers are initialized |
Instruction first scan | Internal data such as pointers and timers are initialized |
EnableIn is false | EnableOut is set to false. The instruction executes. HART data, units and status are provided. |
EnableIn is true | EnableOut is set to true. The instruction executes. HART data, units and status are provided. |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic it will execute.
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in the Function Block Diagram table. |
Instruction first run | See Instruction first run in the Function Block Diagram table. |
EnableIn is true | See EnableIn is true in the Function Block Diagram table. |
Postscan | See Postscan in the Function Block Diagram table. |
Example
In the following example, the PAH instruction is used alongside a PAI (Process Analog Input) instruction. The PAI provides processing for the analog (4 to 20 mA DC) signal from the HART analog input module, and the PAH instruction provides processing for the digital HART data overlaid upon the analog signal, received from the same field device. As a result, an analog real-time signal is provided for closed-loop control (not shown), and four digital dynamic variables are provided for additional process monitoring.
Ladder Diagram

Function Block Diagram

Structured Text
PAH(TI_301_Dvc, ProMag400_I:I.PAxDevice, HART_DiagTable_Flow, HART_EUTable_Generic);
TI_301.Cfg_InpRawMin:=TI_301_Dvc.Val_InpRawMinFromHART;
TI_301.Cfg_InpRawMax:=TI_301_Dvc.Val_InpRawMaxFromHART;
TI_301.Cfg_PVEUMin:=TI_301_Dvc.Val_PVEUMinFromHART;
TI_301.Cfg_PVEUMax:=TI_301_Dvc.Val_PVEUMaxFromHART;
TI_301.Inp_PVData:=TI_301_Inp_PVData;
TI_301.Inp_ModFault:=TI_301_Inp_ModFault;
TI_301.Inp_ChanFault:=TI_301_Inp_ChanFault;
TI_301.Inp_PVUncertain:=TI_301_Inp_PVUncertain;
PAI(TI_301, 0);
Provide Feedback