Returned Calculated Data Parameter
The returned Calculated Data value for Coordinated System Motion instructions is outlined in the table.
Mode | Returned Calculated Data Parameter |
---|---|
Master Driven | The returned Calculated Data parameter is the incremental delta Master position that is needed to make the Slave Coordinate System move from the point at which Slave Coordinate System is locked to the Master and starts moving along the programmed path to the point where distance to go is less than the specified Event Distance. (See Example 3. In example 3, the MSP for all event distances is point P0.) ![]()
![]() |
Time Driven | The returned data in the Calculated Data parameter is the total time in seconds that is needed to make the Slave Coordinate System move from the move’s start point to a point where distance to go is less than the specified Event Distance. If the specified data in the Event Distance is array element is 0.0, then the time it takes the entire move to complete is returned. |
Provide Feedback