Motion Calculate Transform Position (MCTP)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers.
Use the Motion Calculate Transform Position (MCTP) instruction to calculate the position of a point in one coordinate system to the equivalent point in a second coordinate system.
IMPORTANT: Tags used for the motion control attribute of instructions should only be used once. Re-use of the motion control tag in other instructions can cause unintended operation. This may result in damage to equipment or personal injury.
Architecture and safety support
Architecture
Standard
Safety
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
No
Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers
Yes
No
Available Languages
Ladder Diagram
MCTP_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
MCTP(Source System, Target System, Motion Control, Orientation, Translation, Transform Direction, Reference Position, Transform Position);
Operands
Ladder Diagram and Structured Text
Operand
Type
Format
Description
Source System
COORDINATE_SYSTEM
Tag
Cartesian coordinate system for Cartesian positions of the robot
For controllers that support the REF_TO motion data types, the coordinate system operand type can be replaced by the REF_TO_COORDINATE_SYSTEM type.
Target System
COORDINATE_SYSTEM
Tag
Non-Cartesian coordinate system that controls the actual equipment. For controllers that support the REF_TO motion data types, the coordinate system operand type can be replaced by the REF_TO_COORDINATE_SYSTEM type.
Motion Control
MOTION_INSTRUCTION
Tag
Control tag for the instruction.
Translation
REAL[3]
Array
Do you want to offset the target position along the X1, X2, or X3 axis?
If
Then
No
Leave the array values at zero.
Yes
Enter the offset distances into the array. Enter the offset distances in coordinate units. Put the offset distance for X1 in the first element of the array, and so on.
Use an array of three REALs even if a coordinate system has only one or two axes.
Operand
Type
Format
Description
Transform Direction
DINT
Immediate
For Robot Type
To calculate
With the base turned to the
And the robot is
Select
All
Cartesian Position
MCTP Arrow
MCTP Arrow
Forward
Cartesian Delta 2D Delta 3D SCARA Delta
Joint Angles
MCTP Arrow
MCTP Arrow
Inverse
Articulated Independent
Articulated Dependent
SCARA Independent
Joint Angles
Same Quadrant as the Point
Right Arm Configuration
Inverse Right Arm
Left Arm Configuration
Inverse Left Arm
Opposite Quadrant from the Point
Right Arm Configuration
Inverse Right Arm Mirror
Left Arm Configuration
Inverse Left Arm Mirror
Reference Position
REAL[3]
Array
If the transform direction is:
Then enter an array that has the:
Forward
Joint Angles
Inverse
Cartesian Positions
Transform Position
REAL[3]
Array
Array that stores the calculated position
Enter the transform direction without spaces. For example, a transform direction of Inverse Left Arm is entered as InverseLeftArm.
See Structured Text Syntax for more information on the syntax of expressions within structured text.
MOTION_INSTRUCTION Data Type
To see if
Check if this bit is on
Data Type
Notes
The rung is true
EN
BOOL
Sometimes the EN bit stays on even if the rung goes false. This happens if the rung goes false before the instruction is done or an error has occurred.
RSL5K_MCTP EN bit
The instruction is done.
DN
BOOL
An error happened
ER
BOOL
Identify the error number listed in the error code field of the Motion control tag then, refer to Motion Error Codes .ERR.
RSL5K_MCTP Instruction
The MCTP instruction is similar to the MCT instruction except the MCTP instruction doesn't start a transform. It calculates a position once each time you execute it.
Programming Guidelines
Follow these guidelines to use an MCTP instruction.
MCTP Instruction Guidelines
Guideline
Example and Notes
Toggle the rung from false to true to execute the instruction.
This is a transitional instruction. In a ladder diagram, toggle the Rung-condition-in from false to true each time you want to execute the instruction.
In structured text, condition the instruction so that it only executes on a transition.
In structured text, instructions execute each time they are scanned. Condition the instruction so that it only executes on a transition. Use either of these methods:
Qualifier of an SFC action
Structured text construct
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or a reference of the incorrect type is passed to the Coordinate System operands. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN, .DN, .ER, and .IP bits are cleared to false.
Rung-condition-in is false
The .EN bit is cleared to false if either the .DN or .ER bit is true.
Rung-condition-in is true
The .EN bit is set to true and the instruction executes.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Normal execution
See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Error Codes
See Motion Error Codes .ERR for Motion Instructions.
Extended Error Codes
Use Extended Error Codes (EXERR) for more instruction about an error. A major fault can occur if an uninitialized reference or a reference of the incorrect type is passed to the Coordinate System operands. See Motion Error Codes .ERR for Motion Instructions.
Changes to Status Bits
None
Data Flow of MCTP Instruction Between Two Coordinate Systems
The following illustrations show the flow of data when an MCTP Instruction is executed to perform a forward transformation and an inverse transformation. The CS1 indicator represents a Cartesian coordinate system containing X1, X2 and X3 axes as the source of the MCTP instruction. The CS2 indicator represents the joint coordinate system containing J1, J2 and J3 axes as the target of the MCTP instruction.
Data Flow When a Move is Executed with an MCTP Instruction - Forward Transform
L5K_MCTP Forward transform_v32
Data Flow When a Move is Executed with an MCTP Instruction - Inverse Transform
MCTP Inverse Transform Data Flow
Examples
Ladder Diagram
MCTP_LD_ex3_v31
Structured Text
MCTP(myMctpSourceSystem, myMctpTargetSystem, myMctpMotionControl, myMctpOrientation, myMctpTranslation, InverseRightArmMirror, myMctpReferencePos, myMctpTransformPos);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal