Motion Coordinated Stop (MCS)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers.The Motion Coordinated Stop (MCS) instruction initiates a controlled stop of coordinated motion. Any pending motion profiles are canceled.
IMPORTANT:
Tags used for the motion control attribute of instructions should only
be used once. Re-use of the motion control tag in other instructions can cause unintended
operation. This may result in damage to equipment or personal injury.
IMPORTANT:
Risk of Velocity and/or End Position Overshoot
If you change move
parameters dynamically by any method, that is by changing move dynamics (MCD or MCCD) or
by starting a new instruction before the last one has completed, be aware of the risk of
velocity and/or end position overshoot.
A Trapezoidal velocity profile can overshoot
if maximum deceleration is decreased while the move is decelerating or is close to the
deceleration point.
An S-curve velocity profile can overshoot if:
- maximum deceleration is decreased while the move is decelerating or close to the deceleration point; or
- maximum acceleration jerk is decreased and the axis is accelerating. Keep in mind, however, that jerk can be changed indirectly if it is specified in % of time.
Architecture | Standard | Safety |
---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No |
Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580,
and ControlLogix 5590 controllers | Yes | No |
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
MCS(CoordinateSystem, MotionControl,StopType, ChangeDecel, DecelRate,DecelUnits, ChangeDecelJerk,DecelJerk, JerkUnits);
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversions.
Ladder Diagram and Structured Text
Operand | Type | Format | Description | |
---|---|---|---|---|
Coordinate System | COORDINATE_SYSTEM | Tag | Name of the coordinate system. Reference to the coordinate system. For controllers that support the REF_TO
Motion data types, the coordinate system operand type can be replaced by the
REF_TO_COORDINATE_SYSTEM type. | |
Motion Control | MOTION_INSTRUCTION | Tag | Control tag for the instruction. | |
Stop Type | DINT | Immediate | If you want to | Choose this Stop Type |
Stop all motion for the axes of the coordinate system and stop any transform that the coordinate system is a part of. | All (0) - For each axis, all motion generators, including the coordinated motion, are taken into account when computing the initial dynamics (i.e., acceleration rate and velocity) to be used in the Decel. Every axis in the coordinated system is stopped independently using the computed initial dynamics. | |||
Stop only coordinated moves. | Coordinated Move (2) | |||
Cancel any transform that the coordinate system is a part of. | Coordinated Transform (3) | |||
Change Decel(1) | DINT | Immediate | If you want to | Then Choose |
Use the maximum deceleration rate of the coordinate system. | No (0) | |||
Specify the deceleration rate. | Yes (1) | |||
Decel Rate | REAL | Immediate or Tag |
IMPORTANT:
An axis could overshoot its target
position if you reduce the deceleration while a move is in process.
Deceleration along the path of the coordinated move. The instruction uses this value:
Enter a value greater than 0. | |
Decel Units | DINT | Immediate | 0 = Units per Sec 2 1 = % of Maximum Only "% of Maximum" is allowed on Cartesian geometries with coordinate definition = XYZRxRyRz. % of Cartesian max is used for XYZ and "% of orientation max" is used for Rx, Ry and Rz. | |
Change Decel Jerk | SINT, INT, or DINT | Immediate | 0 = No 1 = Yes | |
Decel Jerk | SINT, INT, DINT, or REAL | Immediate or Tag | You must always enter a value for the Decel Jerk operand. This instruction only uses the value if the Profile is configured as S-curve. Decel Jerk is the deceleration jerk rate for the coordinate system. Use these values to get started.
| |
Jerk Units | SINT, INT, or DINT | Immediate | 0 = Units per sec 3 1 = % of Maximum 2 = % of Time (use this value to get started) Only "% of Time" is allowed on Cartesian geometries with coordinate definition = XYZRxRyRz. |
(1) Overshoot may occur if MCS is executed close to or beyond the deceleration point and the deceleration limit is decreased. Keep in mind that deceleration may be decreased indirectly by setting ChageDecel to NO if configured maximum deceleration rate is less than the active deceleration rate.
Structured Text
Enter the stop type and decel units without spaces.
See Structured Text Syntax for
more information on the syntax of expressions within structured text.
For example, enter the Coordinate System operand as CoordinateSystem.
How Stop Types Affect Transforms
This table describes how the stop types affect coordinate systems that are a part of a transform.
This Operand | Description |
---|---|
All | This stop type:
|
Coordinate Move | This stop type stops only the coordinated moves. Any transforms stay active. |
Coordinated Transform | This stop type cancels the transforms associated with the specified coordinate system. All transform-related motion stops on all associated target coordinate systems. However, source coordinate axes will continue to move as instructed. Example If four coordinate systems are linked via three transforms. And the first coordinate system (CS1) is the source and is processing commanded motion. ![]() Executing an MCS instruction on CS2 and using a stop type of coordinated transform results in:
In an Motion Axis Stop (MAS) instruction, a stop type of all also cancels transforms. |
MOTION_INSTRUCTION Data Type
To see if | Check if this bit is on | Data Type | Notes |
---|---|---|---|
The rung is true | EN | BOOL | Sometimes the EN bit stays on even if the rung goes false. This happens if the rung goes false before the instruction is done or an error has occurred. ![]() |
The stop was successfully initiated | DN | BOOL | |
An error happened | ER | BOOL | |
The axis is stopping | IP | BOOL | Any of these actions ends the MCS instruction and turns off the IP bit:
|
The axis is stopped | PC | BOOL | The PC bit stays on until the rung makes a false-to-true transition. |
Master Driven Speed Control (MDSC) and the MCS Instruction
If an MCS is issued when in Master Driven Mode, a switch is made to Time Driven Mode and the axes are stopped in Time Driven Mode. MCS All resets the IP bit of the Master Driven Coordinate Control (MDCC) instruction. Other stop types do not reset the IP bit.
The MCS All instruction clears the pending Master Axis for all future coordinated motion instructions. However, MCS ALL on the Master axis does not break the MDSC link.
The AC bit of the MDCC instruction is reset when the axis is stopped.
The instruction queue is cleared when an MCS All or MCS Coordinated is executed (goes IP).
The status bit CalculatedDataAvailable in an active motion instruction status word for an MCLM or MCCM instruction clears when an MCS is executed (goes IP). The CalculatedData is not recomputed.
Note that if a stop is issued very close to the programmed endpoint, the actual stop may be beyond the programmed endpoint, especially if run in Master Driven Mode.
MCS is a transitional instruction:
- In relay ladder, toggle the Rung-condition-in from false to true each time the instruction should execute.
- In structured text, condition the instruction so that it only executes on a transition.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or
a reference of the incorrect type is passed to the Coordinate System operands. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if either the .DN or .ER bit is true. |
Rung-condition-in is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in the Ladder Diagram table. |
Normal execution | See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table. |
Postscan | See Postscan in the Ladder Diagram table. |
Error Codes:
See Motion Error Codes .ERR for motion
instructions.
Extended Error Codes
See Extended Error Codes for Motion Instructions. It has information about how to use the
extended error codes. See Motion Error Codes .ERR for
motion instructions.
Changes to Status Bits
The instruction changes these status bits when it executes.
In the tag for the | This bit | When the stop type is | Turns |
---|---|---|---|
Axis | CoordinatedMotionStatus | ![]() | Off when the coordinated move stops |
TransformStatus | Coordinated Move | Unchanged | |
| Off | ||
ControlledByTransformStatus | Coordinated Move | Off when the axes stop and the PC bit of the MCS instruction turns on | |
| Off | ||
Coordinate System | MotionStatus | ![]() | Off when the coordinated move stops |
AccelStatus | ![]() | Off | |
DecelStatus | ![]() | On during the stop and then off when the stop completes | |
StoppingStatus | ![]() | On during the stop and then off when the PC bit turns on | |
MoveStatus | ![]() | Off | |
MoveTransitionStatus | ![]() | Off | |
TransformSourceStatus | Coordinated Move | Unchanged | |
| Off | ||
TransformTargetStatus | Coordinated Move | Unchanged | |
| Off |
How Stop Types Affect Transforms an Axis Motion Example
Suppose you have this situation.

Where:
- Coordinate system 1 (CS1) contains the X, Y, and Z axes.
- Coordinate system 2 (CS2) contains the Y, Z, and S axes.
- Coordinate system 3 (CS3) contains the A, B, and C axes.
- Transform (T1) links source coordinate CS2 to target CS3.
- CS2 (XYS) axes are mapped to CS3 (ABC) axes.
- MAM instructions executed on the Y, Z, and S axes.
- MCLM instruction executed on CS2.
- MCT instruction executed with CS2 as the source and CS3 as the target.
- No coordinate instructions were executed on CS2 or CS3.
This table shows the results of executing various MCS and MAS instructions with different stop types.
Instruction | Stop Type | Result |
---|---|---|
MCS on CS1 | All | The MCLM instruction on CS2 will stop. |
The MAM on Y will stop. | ||
The MAM on Z will stop. | ||
The MAM on S will continue. | ||
T1 is canceled. | ||
Axes ABC will stop due to canceling the transform. | ||
MCS on CS2 | All | The MCLM instruction on CS2 will stop. |
The MAM on Y will stop. | ||
The MAM on S will stop. | ||
The MAM on Z will continue. | ||
T1 is canceled. | ||
Axes ABC will stop due to canceling the transform. | ||
MCS on CS3 | All | The MCLM instruction on CS2 will continue. |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 is canceled. | ||
Axes ABC will stop due to canceling the transform. | ||
MCS on CS1 | Coordinated Move | The MCLM instruction on CS2 will continue. |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MCS on CS2 | Coordinated Move | The MCLM instruction on CS2 will stop. |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MCS on CS3 | Coordinated Move | The MCLM instruction on CS3 will stop. |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MAS on Y | All | The MCLM instruction on CS2 will stop. |
The MAM on Y will stop. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 is canceled. | ||
Axes ABC will stop due to canceling the transform. | ||
MAS on Y | Move | The MCLM instruction on CS2 will continue. |
The MAM on Y will stop. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MAS on Z | All | The MCLM instruction on CS2 will continue. |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will stop. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MAS on Z | Move | The MCLM instruction on CS2 will continue. |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will stop. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MCS on CS1 | Coordinated Transform | The MCLM instruction on CS2 will continue |
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
T1 stays active. | ||
Axes ABC will follow the respective CS2 axes. | ||
MCS on CS2 | Coordinated Transform | T1 is canceled. |
The MCLM instruction on CS2 will continue. | ||
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
Axes ABC will stop due to canceling the transform. | ||
MCS on CS3 | Coordinated Transform | T1 is canceled. |
The MCLM instruction on CS2 will continue. | ||
The MAM on Y will continue. | ||
The MAM on S will continue. | ||
The MAM on Z will continue. | ||
Axes ABC will stop due to canceling the transform. |
Example
Ladder Diagram

Structured Text
MCS(myMcsCoordinateSystem,myMcsMotionControl,All,Yes,myMcsDecelRate,Unitspersec2,Yes,100.0,%ofTime);
Provide Feedback