Motion Coordinated Circular Move (MCCM)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers.Use the Motion Coordinated Circular Move (MCCM) instruction to initiate a two or
three-dimensional circular coordinated move for the specified axes within a Cartesian
coordinate system. New position is defined as either an absolute or incremental position and
done at the desired speed. The actual speed of the MCCM is a function of the mode of the
move (commanded speed or percent of maximum speed). The speed of the move is based on the
time it takes to complete the circular move using the programmed axes. Each axis is
commanded to move at a speed that allows for all axes to reach the endpoint (target
position) at the same time.
The dimension of the circle is defined by the number of axes contained within the coordinate system. For example, if you have a coordinate system that contained three axes with an MCCM instruction that has motion in only two dimensions, the resultant move is still considered a three-dimensional arc or circle.
IMPORTANT:
Tags used for the motion control attribute of instructions should only
be used once. Re-use of the motion control tag in other instructions can cause unintended
operation. This may result in damage to equipment or personal injury.
IMPORTANT:
Risk of Velocity and/or End Position Overshoot
If you change move
parameters dynamically by any method, that is by changing move dynamics (MCD or MCCD) or
by starting a new instruction before the last one has completed, be aware of the risk of
velocity and/or end position overshoot.
A Trapezoidal velocity profile can overshoot
if maximum deceleration is decreased while the move is decelerating or is close to the
deceleration point.
An S-curve velocity profile can overshoot if:
maximum
deceleration is decreased while the move is decelerating or close to the deceleration
point; or
maximum acceleration jerk is decreased and the axis is accelerating. Keep
in mind, however, that jerk can be changed indirectly if it is specified in % of
time.
Architecture | Standard | Safety |
---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No |
Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580,
and ControlLogix 5590 controllers | Yes | No |
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
MCCM (CoordinateSystem, MotionControl, MoveType, Position, CircleType, Via/Center/Radius, Direction, Speed, SpeedUnits, AccelRate, AccelUnits, DecelRate, DecelUnits, Profile, AccelJerk, DecelJerk, JerkUnits,Terminationtype, Merge, Mergespeed, CommandTolerance, LockPosition, LockDirection, EventDistance, CalculatedData);
Operands
There are data conversion rules for mixed data types within an instruction. See Data Conversions.
Ladder Diagram and Structured Text
Operand | Type | Format | Description | ||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Coordinate System | COORDINATE_SYSTEM | Tag | Coordinated group of axes. Reference to coordinated group of axes. For controllers that support the REF_TO motion data types, the coordinate system operand type can be replaced by the REF_TO_COORDINATE_SYSTEM type. | ||||||||||
Motion Control | MOTION_INSTRUCTION | Tag | Structure used to access instruction status parameters. | ||||||||||
Move Type | SINT, INT, or DINT | Immediate or Tag | Select the Move Type: 0 = Absolute 1 = Incremental | ||||||||||
Position | REAL | Array tag [ ] | [coordinate units] | ||||||||||
Circle Type | SINT, INT, or DINT | Immediate or Tag | 0 = Via 1 = Center 2 = Radius 3 = Center Incremental | ||||||||||
Via/Center/Radius | REAL | array tag[] (via/center) Immediate or tag (radius) | [coordinate units] | ||||||||||
Direction | SINT, INT, or DINT | Immediate or Tag |
| ||||||||||
Speed | SINT, INT, DINT, or REAL | Immediate or Tag | [coordinate units] | ||||||||||
Speed Units | SINT, INT, or DINT | Immediate | 0 = Units per Sec 1 = % of Maximum 4= Units per MasterUnit | ||||||||||
Accel Rate | SINT, INT, DINT, or REAL | Immediate or Tag | [coordinate units] | ||||||||||
Accel Units | SINT, INT, or DINT | Immediate | 0 = Units per Sec 2 1 = % of Maximum 4= Units per MasterUnit 2 | ||||||||||
Decel Rate | SINT, INT, DINT, or REAL | Immediate or Tag | [coordinate units] | ||||||||||
Decel Units | SINT, INT, or DINT | Immediate | 0 = Units per Sec 2 1 = % of Maximum 4= Units per MasterUnit 2 | ||||||||||
Profile | SINT, INT, or DINT | Immediate | 0 = Trapezoidal 1 = S-curve | ||||||||||
Accel Jerk | SINT, INT, DINT, or REAL | Immediate or Tag | You must always enter values for the Accel and Decel Jerk operands. This instruction only uses the values if the Profile is configured as S-curve. Accel Jerk is the acceleration jerk rate for the coordinate system. Decel Jerk is the deceleration jerk rate for the coordinate system. Enter the jerk rates in these Jerk Units. 0 = Units per sec 3 1 = % of Maximum 2 = % of Time 4 = Units per MasterUnit 3 6 = % of Time-Master Driven Use these values to get started. Accel Jerk = 100 (% of Time) Decel Jerk = 100 (% of Time) Jerk Units = 2 | ||||||||||
Decel Jerk | SINT, INT, DINT, or REAL | Immediate or Tag | |||||||||||
Jerk Units | SINT, INT, or DINT | Immediate or Tag | |||||||||||
Termination Type | SINT, INT, or DINT | Immediate or Tag | 0 = Actual Tolerance 1 = No Settle 2 = Command Tolerance 3 = No Decel 4 = Follow Contour Velocity Constrained 5 = Follow Contour Velocity Unconstrained 6 = Command Tolerance Programmed See Choose a Termination Type in the Related Topics section below. | ||||||||||
Merge | SINT, INT, or DINT | Immediate | 0 = Disabled 1 = Coordinated Motion 2 = All Motion | ||||||||||
Merge Speed | SINT, INT, or DINT | Immediate | 0 = Programmed 1 = Current | ||||||||||
Command Tolerance | REAL | Immediate Real or Tag | The position on a coordinated move where blending should start. This parameter is used in place of Command Tolerance in the Coordinate System if Termination Type 6 is used. Tip : Termination type 2 is identical to Termination Type 6 except the Command Tolerance value from the coordinate system is used and this parameter is ignored. | ||||||||||
Lock Position | REAL | Immediate or Tag | Position on the Master Axis where a Slave should start following the master after the move has been initiated on the Slave Axis. See the Structure section below for more information. | ||||||||||
Lock Direction | UINT32 | Immediate | Specifies the conditions when the Lock Position should be used. See the Structure section below for more information. | ||||||||||
Event Distance | REAL ARRAY or 0 | Array | The position(s) on a move measured from the end of the move. See the Structure section below for more information. | ||||||||||
Calculated Data | REAL ARRAY or 0 | Array | Master Distance(s) (or time) needed from the beginning of the move to the Event Distance point. See the Structure section below for more information. |
Structured Text
See Structured Text Syntax for
more information on the syntax of expressions within structured text.
When entering enumerations for the operand value in structured text, multiple word enumerations must be entered without spaces. For example: when entering Decel Units the value is entered as unitspersec
2
rather than Units per Sec2
as displayed in the ladder logic.Use the entries in this table as a guide when entering structured text operands.
This Operand | Has These Options Which You | |||||||||
---|---|---|---|---|---|---|---|---|---|---|
Enter as Text | Or as | |||||||||
Coordinate System | No enumeration | Tag | ||||||||
Motion Control | No enumeration | Tag | ||||||||
Move Type | No enumeration | 0 (Absolute) 1 (Incremental) | ||||||||
Position | No enumeration | Array Tag | ||||||||
Circle Type | No enumeration | Tag 0 = Via 1 = Center 2 = Radius 3 = Center Incremental | ||||||||
Via/Center/Radius | No enumeration | Array Tag (via/center) Immediate or tag (radius) | ||||||||
Direction | No enumeration |
| ||||||||
Speed | No enumeration | Immediate or Tag | ||||||||
Speed Units | unitspersec %ofmaximum unitspermasterunit | 0 1 4 | ||||||||
Accel Rate | No enumeration | Immediate or Tag | ||||||||
Accel Units | unitspersec 2 %ofmaximum unitspermasterunit 2 | 0 1 4 | ||||||||
Decel Rate | No enumeration | Immediate or Tag | ||||||||
Decel Units | unitspersec 2 %ofmaximum unitspermasterunit 2 | 0 1 4 | ||||||||
Profile | trapezoidal s-curve | 0 1 | ||||||||
Accel Jerk | No enumeration | Immediate or tag You must always enter a value for the Accel and Decel Jerk operands. This instruction only uses the values if the Profile is configured as S-curve. Use these values to get started. Accel Jerk = 100 (% of Time) Decel Jerk = 100 (% of Time) Jerk Units = 2 | ||||||||
Decel Jerk | No enumeration | |||||||||
Jerk Units | Unitspersec 3 %ofmaximum %oftime unitspermasterunit3 %oftimemasterdriven | 0 1 2 (use this value to get started) 4 6 | ||||||||
Termination Type | No enumeration | 0 = Actual Tolerance 1 = No Settle 2 = Command Tolerance 3 = No Decel 4 = Follow Contour Velocity Constrained 5 = Follow Contour Velocity Unconstrained 6 = Command Tolerance Programmed See Choose a Termination Type in the Related Topics section below. | ||||||||
Merge | disabled coordinatedmotion allmotion | 0 1 2 | ||||||||
Merge Speed | programmed current | 0 1 | ||||||||
Command Tolerance | No enumeration | Immediate or Tag | ||||||||
Lock Position | No enumeration | Immediate, Real, or Tag | ||||||||
Lock Direction | None immediateforwardonly Immediatereverseonly positionforward positionreverse | 0 1 2 3 4 | ||||||||
Event Distance | No enumeration | Array | ||||||||
Calculated Data | No enumeration | Array |
Coordinate System
The Coordinate System operand specifies the system of motion axes that define the dimensions of a Cartesian coordinate system. For this release, the coordinate system supports up to three (3) primary axes. Only the axes configured as primary axes (up to 3) are included in speed calculations. Only primary axes participate in the actual circular move.
Motion Control
The following control bits are affected by the MCCM instruction.
Mnemonic | Description |
---|---|
.EN (Enable) Bit 31 | The Enable bit is set when the rung transitions from false to true and resets when the rung goes from true to false. |
.DN (Done) Bit 29 | The Done bit sets when the coordinated instruction has been verified and queued successfully. Because it’s set at the time it’s queued it may appear as set when a runtime error is encountered during the verify operation after it comes out of the queue. It resets when the rung transitions from false to true. |
.ER (Error) Bit 28 | The Error bit resets when the rung transitions from false to true. It sets when the coordinated move fails to initiate successfully. It can also be set with the Done bit when a queued instruction encounters a runtime error. |
.IP (In Process) Bit 26 | The In Process bit sets when the coordinated move is successfully initiated. It resets when there is a succeeding move and the coordinated move reaches the new position, or when there is no succeeding move and the coordinated move reaches the termination type specifications, or when the coordinated move is superseded by another MCCM or MCLM instruction with a Merge Type of Coordinated Move or when terminated by an MCS or an MCSD instruction. |
.AC (Active) Bit 23 | When you have a coordinated move instruction queued, the Active bit lets you know which instruction is controlling the motion. It sets when the coordinated move becomes active. It is reset when the Process Complete bit is set or when the instruction is stopped. |
.PC (Process Complete) Bit 27 | The Process Complete bit is reset when the rung transitions from false to true. It is set when there is no succeeding move and the coordinated move reaches the new position, or when there is a succeeding move and the coordinated move reaches the specified termination type. |
.ACCEL (Acceleration Bit) Bit 01 | The Acceleration bit sets while the coordinated move is in the acceleration phase. It resets while the coordinated move is in the constant velocity or deceleration phase, or when coordinated motion concludes. |
.DECEL (Deceleration Bit) Bit 02 | The Deceleration bit sets while the coordinated move is in the deceleration phase. It resets while the coordinated move is in the constant velocity or acceleration phase, or when coordinated motion concludes. |
Move Type
The Move Type operand determines the method used by the position array to indicate the path of the coordinated move and the method the via/center/radius parameter uses to indicate the via and center circle positions. The options are: Absolute or Incremental.
- Absolute - the coordinate system moves to the specified Position at the defined Speed, using the Accel and Decel Rates as designated by their respective operands, along a circular path.When an axis is configured for rotary operation, absolute moves are handled in the same manner as with linear axes. When the axis position exceeds the Unwind parameter, an error is generated.
- The sign of the specified position array is interpreted by the controller as the direction for the move. Negative position values instruct the interpolator to move the rotary axis in a negative direction to obtain the desired absolute position. A positive value indicates that positive motion is desired to reach the target position. To move to the unwind position in the negative direction a negative unwind position value must be used as 0 and -0 are treated as 0. When the position is greater than the unwind value, an error is generated. The axis can move through the unwind position but never incrementally more than one unwind value.
- Incremental - the coordinate system moves the distance as defined by the position array at the specified Speed, using the Accel and Decel rates determined by the respective operands, along a circular path.
The specified distance is interpreted by the interpolator and can be positive or negative. Negative position values instruct the interpolator to move the rotary axis in a negative direction, while positive values indicate positive motion is desired to reach the target position.
Position
The Position operand is a one dimensional array whose dimension is at least equivalent to the number of axes specified in the coordinate system. It is the position array that defines the new absolute or incremental position.
Circle Type
The Circle Type operand specifies how the array labeled via/center/radius is interpreted. The options are: Via, Circle, Radius, Center Incremental.
- Via indicates that the via/center/radius array members specify a via point between the start and end points.
- Center indicates that the via/center/radius array members contain the circle center.
- Radius indicates that the first via/center/radius array member contains the radius. Other members are ignored. Radius is valid only in two-dimensional coordinate systems.
- Center Incremental indicates that the via/center/radius array members define a position that always incrementally defines the center of the circle regardless of Move Type operand. Sign of the incremental value is measured from the start point to the center.
Via/Center/Radius
Depending on the selected Move Type and Circle Type, the via/center/radius position parameter defines the absolute or incremental value of a position along the circle, the center of the circle, or the radius of the circle as defined in the following table. If the Circle Type is via or center, the via/center/radius position parameter is a one-dimensional array, whose dimension is defined to be at least the equivalent of the number of axes specified in the coordinate system. If the Circle type is radius, the via/center/radius position parameter is a single value.
Move Type | Cycle Type | Behavior |
---|---|---|
Absolute | Via | The via/center/radius position array defines a position along the circle. For a non-full circle case, the Position parameter array defines the endpoint of the arc. For a full circle case, the Position parameter array defines any second point along the circle except the endpoint. |
Incremental | Via | The sum of the via/center/radius position array and the old position defines the position along the circle. For a non-full circle case, the sum of the Position parameter array and the old position defines the endpoint of the arc. For a full circle case, the sum of the Position parameter array and the old position defines any second point along the circle except the endpoint. |
Absolute | Center | The via/center/radius position array defines the center of the circle. For a non-full circle case, the Position parameter array defines the endpoint of the arc. For a full circle case, the Position parameter array defines any second point along the circle except the endpoint. |
Incremental | Center | The sum of the via/center/radius position array and the old position defines the center of the circle. For a non-full circle case, the sum of the Position parameter array and the old position defines the endpoint of the arc. For a full circle case, the sum of the Position parameter array and the old position defines any second point along the circle except the endpoint. |
Absolute or Incremental | Radius | The via/center/radius position single value defines the arc radius. The sign of the value is used to determine the center point to distinguish between the two possible arcs. A positive value indicates a center point that generates an arc less than 180 degrees. A negative value indicates a center point that generates an arc greater than 180 degrees. This Circle Type is only valid for two-dimensional circles. The position parameter array follows the Move Type to define the endpoint of the arc. |
Absolute | Center Incremental | The sum of the via/center/radius position array and the old position defines the center position of the circle. For a non-full circle case, the Position parameter array defines the endpoint of the arc. For a full circle case, the Position parameter array defines any second point along the circle except the endpoint. |
Incremental | Center Incremental | The sum of the via/center/radius position array and the old position defines the center position of the circle. For a non-full circle case, the sum of the Position parameter array and the old position defines the endpoint of the arc. For a full circle case, the sum of the Position parameter array and the old position defines any second point along the circle except the endpoint. |
Direction
The Direction operand defines the rotational direction of a 2D circular move as either clockwise or counterclockwise according to the right-hand screw rule. For a 3D circular move the direction is either Shortest or Longest. In both 2D and 3D it can also indicate if the circular move is to be a full circle.
Speed
The Speed operand defines the maximum vector speed along the path of the coordinated move.
Speed Units
The Speed Units operand defines the units applied to the Speed operand either directly in coordinate units or as a percentage of the maximum values defined in the coordinate system.
Accel Rate
The Accel Rate operand defines the maximum acceleration along the path of the coordinated move.
Accel Units
The Accel Units operand defines the units applied to the Accel Rate operand either directly in coordinate units of the specified coordinate system or as a percentage of the maximum values defined in the coordinate system.
Decel Rate
The Decel Rate operand defines the maximum deceleration along the path of the coordinated move.
Decel Units
The Decel Units operand defines the units applied to the Decel Rate operand either directly in coordinate units of the specified coordinate system or as a percentage of the maximum values defined in the coordinate system.
Profile
The Profile operand determines whether the coordinated move uses a trapezoidal or an S-curve velocity profile.
Accel Jerk
Accel Jerk defines the maximum acceleration jerk for the programmed move. For more information on calculating Accel Jerk, refer to the Jerk Units section below.
Decel Jerk
Decel Jerk defines the maximum deceleration jerk for the programmed move. For more
information on calculating Decel Jerk, refer to the Jerk Units section below.
Jerk Units
The jerk units define the units that are applied to the values entered in the Accel Jerk
and Decel Jerk operands. The values are entered directly in the position units of the
specified coordinate system or as a percentage. When configured using % of Maximum, the
jerk is applied as a percentage of the Maximum Acceleration Jerk and Maximum Deceleration
Jerk operands specified in the coordinate system attributes. When configured using % of
Time, the value is a percentage based on the Speed, Accel Rate, and Decel Rate specified in
the instruction.
If you want to convert engineering units to % of Time, use these equations.

If you want to convert % of Time to engineering units, use these equations.

Important Consideration
If you program tangent circles with different Jerk rates (Decel Jerk of first circle and Accel Jerk of the second circle), then you might get a slight velocity discontinuity at the intersection of the two circles. The size of the discontinuity depends on magnitude of the Jerk difference. In other words, the smaller the Jerk difference, the smaller the velocity glitch. Therefore, we recommend that you do not program Jerk rates on tangent circles.
Termination Type
For Master Driven Speed Control (MDSC), when all sequential instructions run in the same mode (Master Driven Mode or Time Driven Mode), then all termination types are supported. If the termination type switches in the coordinated motion queue, errors may generate depending on the sequence of motion types.
The following is only applicable if a move on a slave Coordinate System uses a Blending Termination Type (Termination Types 2, 3, or 6) and is programmed in MDSC mode.
If you use the Calculated Data returned in the last MCCM instruction of a motion sequence to program the length that the master axis has to move for the motion sequence to go PC, then there is the possibility that you will have to add a small safety margin to the Calculated Data. If you do not add this margin, there is a chance that the motion of the master axes completes before the entire motion sequence programmed on the Slave Coordinate System finishes. If this occurs, the last motion instruction on the Slave Coordinate System remains active and does not go PC. The value of the small safety margin is dependent on the Command Tolerance used for the first and last move in the motion sequence as follows:
CUP = Coarse Update Period
MAS = Master Axis Speed
- If a Command Tolerance value of 100% is used for the first move in the sequence then:
SafetyMargin1 = CUP * MAS
else
SafetyMargin1 = CUP * MAS * .02
- For all other moves in the blending sequence between first and last:
SafetyMargin2 = CUP * MAS * .02 * number of blending moves between 1st and last
- If a Command Tolerance value of 100% is used for the last in the sequence then:
SafetyMargin3 = CUP * MAS
else
SafetyMargin3 = CUP * MAS * .02
- Final SafetyMargin = SafetyMargin1 + SafetyMargin2 + SafetyMargin3
Once a sequence is programmed and verified, it will repeat.
Click the link Choose a Termination Type in the Related Topics section below for information.
Merge
The merge defines whether or not to turn the motion of all specified axes into a pure coordinated move. The options are: Merge Disabled, Coordinated Motion, or All Motion.
- Merge Disabled - Any currently executing single axis motion instructions involving any axes defined in the specified coordinate system are not affected by the activation of this instruction, and result in superimposed motion on the affected axes. An error is flagged if a second instruction is initiated in the same coordinate system or in another coordinate system containing any axes in common with the coordinate system that is active.
- Coordinated Motion - Any currently executing coordinated motion instructions involving the same specified coordinate system are terminated, and the active motion is blended into the current move at the speed defined in the merge speed parameter. Any pending coordinated motion instructions in the specified coordinate system are canceled. Any currently executing system single axis motion instructions involving any axes defined in the specified coordinate system are not affected by the activation of this instruction, and result in superimposed motion on the affected axes.
- All Motion - Any currently executing single axis motion instructions involving any axes defined in the specified coordinate system and any currently executing coordinated motion instructions are terminated. The prior motion is merged into the current move at the speed defined in Merge Speed parameter. Any pending coordinated move instructions are canceled.
Merge Speed
The Merge Speed operand defines whether the current speed or the programmed speed is used as the maximum speed along the path of the coordinated move when Merge is enabled. Current speed is the vector sum of all motion (for example, jogs, MAM’s, and geared motion) for all axes defined in the current coordinate system.
MCCM Target Position Entry Dialog Box
The MCCM Target Position Entry Dialog box is accessed by pressing the ellipsis button to the right of the position operand of the ladder instruction faceplate. The Target Position Entry box can only be accessed if the coordinate system for the instruction has been named, has a valid tag name for the Position operand that contains enough elements to accommodate the number of axes, selected a valid Move Type and a valid Circle Type. If these criteria have not been satisfied, an error message is displayed on the status bar.
MCCM Ladder Valid Values for Accessing Target Position Entry Box

Press the ellipsis and the
Target Position Entry Position
tab dialog box displays.
NOTE:
This action is not possible for a reference.
Target Position Entry Dialog Box Fields
Feature | Description |
---|---|
Axis Name | This column has the names of each axis in the coordinate system named in the ladder faceplate. These names are not editable. |
Target Position/Target Increment | The values in this column are numeric. They show the endpoint or incremental departure of the move depending on the active Move Type. The column heading indicates which is displayed. |
Actual Position | This column contains the current actual position of the axes in the coordinate system. These values update dynamically when on-line and the Coordinate System Auto Tag Update is enabled. |
Via Position/Via Increment Center Position/Center Increment Radius | Depending on the Circle Type selected, this column contains the Via point position or increment, the Center Position or increment. |
Set Targets = Actuals | This button is enabled when the Move Type is Absolute and is used to copy the value from the Actual Position fields to the Target Position fields. |
Set Vias = Actuals | This button is only active if the Move Type is Absolute. It is used to copy the values from the Actual Position fields to the Vias Fields. |
The Move Type and Circle Type selected govern the appearance of this dialog box. This table illustrates how the screen is affected by the combinations of Move Type and Circle Type selected.
Target Position Entry Dialog Box Changes
Move Type | Circle Type | Behavior |
---|---|---|
Absolute | Via | Target column is entitled Target Position. Via column is entitled Via Position. Set Targets = Actuals button is active. Set Vias = Actuals button is active. |
Incremental | Via | Target column is entitled Target Increment. Via Column is entitled Via Increment. Set Targets = Actuals button is inactive (appears dimmed). Set Vias = Actuals button is inactive (appears dimmed). |
Absolute | Center | Target column is entitled Target Position. Center column is entitled Center Position. Set Targets = Actuals button is active. Set Vias = Actuals button is active. |
Incremental | Center | Target column is entitled Target Increment. Center Column is entitled Center Increment. Set Targets = Actuals button is inactive (appears dimmed). Set Vias = Actuals button is inactive (appears dimmed). |
Absolute | Radius | Target column is entitled Target Position. Radius column is entitled Radius. Set Targets = Actuals button is active. Set Vias = Actuals button is inactive (appears dimmed). |
Incremental | Radius | Target column is entitled Target Increment. Radius Column is entitled Radius. Set Targets = Actuals button is inactive (appears dimmed). Set Vias = Actuals button is inactive (appears dimmed). |
Absolute | Center Incremental | Target column is entitled Target Position. Center Incremental column is entitled Center Incremental. Set Targets = Actuals button is active. Set Vias = Actuals button is inactive (appears dimmed). |
Incremental | Center Incremental | Target column is entitled Target Increment. Center Incremental column is entitled Center Incremental. Set Targets = Actuals button is inactive (appears dimmed). Set Vias = Actuals button is inactive (appears dimmed). |
MCCM is a transitional instruction:
- In relay ladder, toggle the Rung-condition-in from false to true each time the instruction should execute.
- In structured text, condition the instruction so that it only executes on a transition. See Structured Text Syntax.
Structure
See Input and Output Parameters Structure for Single Axis Motion
Instructions for the input and output parameters that are available for the MCCM instruction
via the Master Driven Speed Control (MDSC) function. Before any of these parameters is
active, you must execute an MDCC instruction and it must be active (IP bit is set).
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or
a reference of the incorrect type is passed to the Coordinate System operand. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if either the .DN or .ER bit is true. |
Rung-condition-in is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
---|---|
Prescan | See Prescan in the Ladder Diagram table. |
Normal execution | See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table. |
Postscan | See Postscan in the Ladder Diagram table. |
Runtime Error Conditions
You cannot switch from Time Driven Mode to Master Driven Mode if the master speed is zero unless the slave speed is zero too.
Extended Error Codes
Extended Error codes help to further define the error message given for this particular instruction. Their behavior is dependent upon the Error Code with which they are associated.
The Extended Error Codes for Servo Off State (5), Shutdown State (7), Axis Type Not Servo (8), Axis Not Configured (11), Homing In Process Error (16), and Illegal Axis Data type (38) errors all function in the same fashion. A number between 0...n is displayed for the Extended Error Code. This number is the index to the Coordinate System indicating the axis that is in the error condition.
For Error Code Axis Not Configured (11) there is an additional value of -1 which indicates that Coordinate System was unable to setup the axis for coordinate motion.
For the MCCM instruction, Error Code 13 - Parameter Out of Range, Extended Errors return a number that indicates the offending parameter as listed on the faceplate in numerical order from top to bottom beginning with zero. For example, 2 indicates the parameter value for Move Type is in error.
Referenced Error Code and Number | Extended Error Numeric Indicator | Instruction Parameter | Description |
---|---|---|---|
Parameter Out Of Range (13) | 0 | Coordinate System | Number of primary axes is not 2 or 3. |
Parameter Out Of Range (13) | 2 | Move Type | Move Type is either less than 0 or greater than 1. |
Parameter Out Of Range (13) | 3 | Position | The position array is not large enough to provide positions for all the axes in the coordinate system. |
Parameter Out Of Range (13) | 4 | Circle Type | Circle Type is either less than 0 or greater than 4. |
Parameter Out Of Range (13) | 5 | Via/Center/Radius | The size of the Via/Center array is not large enough to provide positions for all of the axes in the defining via/center point. |
Parameter Out Of Range (13) | 6 | Direction | Direction is either less than 0 or greater than 3. |
Parameter Out of Range (13) | 7 | Speed | Speed is less than 0. |
Parameter Out of Range (13) | 9 | Accel Rate | Accel Rate is less than or equal to 0. |
Parameter Out of Range (13) | 11 | Decal Rate | Decel Rate is less than or equal to 0. |
Parameter Out of Range (13) | 14 | Termination Type | Termination Type is less than 0 or greater than 3. |
For the Error Code 54 – Maximum Deceleration Value is Zero, if the Extended Error returns a positive number (0-n) it’s referring to the offending axis in the coordinate system. Go to the Coordinate System Properties General Tab and look under the Brackets ([ ])column of the Axis Grid to determine which axis has a Maximum Deceleration value of 0. Click on the ellipsis button next to the offending axis to access the Axis Properties screen. Go to the Dynamics tab and make the appropriate change to the Maximum Deceleration Value. If the Extended Error number is -1, this means the Coordinate System has a Maximum Deceleration Value of 0. Go to the Coordinate System Properties Dynamics Tab to correct the Maximum Deceleration value.
MCCM Changes to Status Bits:
Status bits provide a means for monitoring the progress of the motion instruction. There are three types of Status bits that provide pertinent information.
- Axis Status bits
- Coordinate System
- Coordinate Motion
When the MCCM instruction initiates, the status bits undergo these changes.
Axis Status Bits
Bit Name | Meaning |
---|---|
CoordinatedMotionStatus | Sets when the MCCM instruction executes and is cleared when the instruction completes. |
Coordinate System Status Bits
Bit Name | Meaning |
---|---|
MotionStatus | Sets when the MCCM instruction is active and the Coordinate System is connected to its associated axes. |
Coordinated Motion Status Bits
Bit Name | Meaning |
---|---|
AccelStatus | Sets when vector is accelerating. Clears when a blend is in process or when vector move is at speed or decelerating. |
DecelStatus | Sets when vector is decelerating. Clears when a blend is in process or when vector move is accelerating or when move completes. |
ActualPosToleranceStatus | Sets for Actual Tolerance termination type only. The bit is set after the following two conditions have been met. 1) Interpolation is complete. 2) The actual distance to the programmed endpoint is less than the configured coordinate system’s Actual Tolerance value. It remains set after the instruction completes. It is reset when a new instruction is started. |
CommandPosToleranceStatus | Sets for all termination types whenever the distance to the programmed endpoint is less than the configured coordinate system’s Command Tolerance value and remains set after the instruction completes. It is reset when a new instruction is started. The CommandPosToleranceStatus (CS_CMD_POS_TOL_STS) status bit in the Coordinate System is set as follows: TT0, TT1, TT4, TT5 - Bit is set when the distance to the endpoint is less than the Command Tolerance value. The bit is cleared when the first move is complete. TT2, TT6 - Bit is set when the distance to the endpoint is less than the Command Tolerance value. The bit is cleared when the blend is started (that is, when the second move is started). Thus, you may not see the bit if the blend is started at the Command Tolerance (CT) point. The blend may have been deferred slightly beyond the CT point if the next move is a short move or for time matching of the acceleration and deceleration of the two adjacent moves. TT3 - Bit is set when the distance to the endpoint is less than the Command Tolerance value (like TT2 and TT6). The bit is cleared when the blend is started. Thus, you may not see the bit if the blend is started at the deceleration point. The blend may have been deferred slightly beyond the deceleration point if the next move is a short move or for time matching of the acceleration and deceleration of the two adjacent moves. |
StoppingStatus | The Stopping Status bit is cleared when the MCCM instruction executes. |
MoveStatus | Sets when MCCM begins axis motion. Clears on the .PC bit of the last motion instruction or a motion instruction executes which causes a stop. |
MoveTransitionStatus | Sets when No Decel or Command Tolerance termination type is satisfied. When blending collinear moves the bit is not set because the machine is always on path. It clears when a blend completes, the motion of a pending instruction starts, or a motion instruction executes which causes a stop. Indicates not on path. |
MovePendingQueueFullStatus | Sets when the instruction queue is full. It clears when the queue has room to hold another new coordinated move instruction. |
CoorMotionLockStatus | Set when an axis lock is requested for an MCLM or MCCM instruction and the axis has crossed the Lock Position. Cleared when an MCLM or MCCM is initiated. For the enumerations Immediate Forward Only and Immediate Reverse Only, the bit is set immediately when the MCLM or MCCM is initiated. When the enumeration is Position Forward Only or Position Reverse Only, the bit is set when the Master Axis crosses the Lock Position in the specified direction. The bit is never set if the enumeration is NONE. The CoordMotionLockStatus bit is cleared when the Master Axis reverses direction and the Slave Axis stops following the Master Axis. The CoordMotionLockStatus bit is set again when the Slave Coordinate System resumes following the Master Axis. The CoordMotionLockStatus bit is also cleared when an MCCS is initiated. |
Currently, Coordinated Motion supports the queueing of one coordinated motion instruction. Therefore the MovePendingStatus bit and the MovePendingQueueFullStatus bit are always the same.
Circular Programming Reference Guide
Circle Type | Used in 2D/3D/Both | Validation Errors | Direction - 2D | Direction - 3D | Comment |
---|---|---|---|---|---|
Radius | 2D | Error 25; Illegal Instruction Error 45 Endpoint = Startpoint Error 49; R too small (|R| < .001) or R too short to span programmed points. | CW/CCW as viewed from the + perpendicular to the circular plane. | N/A | A + radius forces arc length to be <= 180° (Shortest arc). A - radius forces arc length to be => 180° (Longest arc). Full Circles can be programmed. For full circles: set Position to be any point on circle except Startpoint and use one of the Full direction types. |
Center Point | Both | Error 44; Collinearity (3D only) Error 45; Endpoint = Startpoint (3D only) Error 46; Start/End radius mismatch (|R1 - R2| > .15 * R1). | CW/CCW as viewed from the + perpendicular to the circular plane. | Shortest/Longest arc. In Full circles, placement of endpoint defines shortest/longest paths referred to by direction parameter. | Full Circles can be programmed. In 2D only, Endpoint = Startpoint is legal. Therefore, full circles may be generated: By setting Endpoint = Startpoint, in which case, all direction types produce full circles. By setting Endpoint not = Startpoint and using Full direction type. For 3D Full Circles: set Position to be any point on the circle except Startpoint, and use one of the Full direction types. Position defines both arc and Shortest direction types. |
Via Point | Both | Error 44; Collinearity Error 45; Endpoint = Startpoint | Via point always determines direction. | Via point always determines direction. Direction operand is only used to determine if circle is partial or full. | Full Circles can be programmed. For full circles: set Position to be any point on circle except Startpoint and use one of the Full direction types. |
Master Driven Speed Control (MDSC) and Motion Direct Command Support
The Motion Direct commands are not available in the instruction tree for the MCCM instruction. You must program an MCCM in one of the supported programming languages before you execute an MAM or MAJ in Time Driven Mode. A runtime error will occur if an MCCM is not previously executed in an MAM and MAJ in Master Driven Mode.
Example 1
Ladder Diagram

Example 2
Via/Center/Radius parameter as an array type.
Ladder Diagram

Structured Text
MCCM(myMccmCoordinateSystem, myMccmMotionControl, myMccmMoveType, myMccmPosition[0], myMccmCircleType, myMccmRadius[0], myMccmDirection, myMccmSpeed, Unitspersec, myMccmAccelRate, Unitspersec2, myMccmDecelRate, Unitspersec2, Trapezoidal, 100.0, 100.0, %ofTime, myMccmTermType, CoordinatedMotion, Programmed, 0, 0, None, 0, 0);
Example 3
Relay Ladder

Structured Text
MCCM(myMccmCoordinateSystem,myMccmMotionControl,myMccmMoveType,myMccmPosition[0],myMccmCircleType,myMccmViaCenter_Radius1,myMccmDirection,myMccmSpeed,Unitspersec,myMccmAccelRate,%ofMaximum,myMccmDecelRate,UnitsperMasterUnit2,Trapezoidal,myMccmAccelJerk,myMccmDecelJerk,Unitspersec3,myMccmTerminationType,CoordinatedMotion,Programmed,myMccmCommandTolerance,myMccmLockPosition,PositionReverseOnly,myMccmEventDistance[0],myMccmCalculatedData[0]);
Provide Feedback