Masked Move with Target (MVMT)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
The MVMT instruction copies the Source to a Destination and allows portions of the data to be masked.
Available Languages
Ladder Diagram
This instruction is not available in Ladder Diagram.
Function Block
MVMT_FBD_avail_v31
Structured Text
MVMT(MVMT_tag);
Operands
Structured Text
Variable
Type
Format
Description
MVMT tag
FBD_MASKED_MOVE
Structure
MVMT structure
See Structured Text Syntax for information on the syntax of expressions within structured text.
Function Block
Operand
Type
Format
Description
MVMT tag
FBD_MASKED_MOVE
Structure
MVMT structure
FBD_MASKED_MOVE Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
If cleared, the instruction does not execute and outputs are not updated. If set, the instruction executes.
Default is set.
Source
DINT
Input value to move to Destination based on value of Mask.
Valid = any integer
Mask
DINT
Mask of bits to move from Source to Dest. All bits set to one cause the corresponding bits to move from Source to Dest. All bits that are set to zero cause the corresponding bits not to move from Source to Dest.
Valid = any integer
Target
DINT
Input value to move to Dest prior to moving Source bits through the Mask.
Valid = any integer
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled.
Dest
DINT
Result of the masked move operation.
Description
When enabled, the MVMT instruction uses a Mask to pass or block Source data bits. A "1" in the mask means the data bit is passed. A "0" in the mask means the data bit is blocked.
If you mix integer data types, the instruction fills the upper bits of the smaller integer data types with 0s so that they are the same size as the largest data type.
Entering an immediate mask value using an Input Reference
When you enter a mask, the programming software defaults to decimal values. If you want to enter a mask using another format, precede the value with the correct prefix.
Prefix
Description
16#
hexadecimal (e.g., 16#0F0F)
8#
octal (e.g., 8#16)
2#
binary (e.g., 2#00110011)
Affects Math Status Flags
Controllers
Affects Math Status Flags
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
No
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes for the output
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State
Action Taken
Prescan
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is false
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is true
EnableIn and EnableOut bits are set to true.
The instruction executes.
Instruction first run
N/A
Instruction first scan
N/A
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal execution
See Tag.EnableIn is true in the Function Block table.
Postscan
See Postscan in the Function Block table.
Examples
Step 1
The controller copies Target into Dest.
MVMT Example step 1
Step 2
The instruction masks Source and compares it to Dest. Any required changes are made in Dest, which becomes and input parameter to value_masked. Source and Target remain unchanged. A 0 in the mask restrains the instruction from comparing that bit.
MVMT Example step 2
Function Block
MVMT_FBD_ex_v31
Structured Text
MVMT_01.Source := value_1;
MVMT_01.Mask := mask_1;
MVMT_01.Target := target;
MVMT(MVMT_01);
value_masked := MVMT_01.Dest;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal