Boolean OR (BOR)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
The BOR instruction logically ORs up to eight Boolean inputs. To perform a bitwise OR, refer to
Bitwise Or (OR)
.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram.
Function Block Diagram
Function Block Diagram supports these elements:
FBD Block
BOR_FBD_avail_v31
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
BOR_avail lang
Structured Text
This instruction is not available in structured text.
Operands
Function Block Diagram
FBD Block
Operand
Data Type
Format
Description
BOR tag
FBD_BOOLEAN_OR
structure
BOR structure
FBD_BOOLEAN_OR Structure
Input Members
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Set to 0 on first download.
In1
BOOL
First Boolean input.
Set to 0 on first download.
In2
BOOL
Second Boolean input.
Set to 0 on first download.
In3
BOOL
Third Boolean input.
Set to 0 on first download.
In4
BOOL
Forth Boolean input.
Set to 0 on first download.
In5
BOOL
Fifth Boolean input.
Set to 0 on first download.
In6
BOOL
Sixth Boolean input.
Set to 0 on first download.
In7
BOOL
Seventh Boolean input.
Set to 0 on first download.
In8
BOOL
Eighth Boolean input.
Set to 0 on first download.
Output Members
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled.
Out
BOOL
The output of the instruction.
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
Input Operands (Left Pins)
Data Type
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Description
In1
BOOL
First Boolean input.
In2
BOOL
Second Boolean input.
Output Operand (Right Pin)
Data Type
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Description
Out
BOOL
The output of the instruction.
Operation
FBD Block
The BOR instruction ORs up to eight Boolean inputs. If an input is not used, it defaults to cleared (0).
Out = In1 OR In2 OR In3 OR In4 OR In5 OR In6 OR In7 OR In8
IMPORTANT: When removing an input wire from the BOR instruction during an edit, make sure the input is cleared (0).
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
The FBD Function ORs two Boolean inputs.
Out = In1 OR In2
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction.
Execution
Function Block Diagram
FBD Block
Condition/State
Action Taken
Prescan
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is false
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is true
EnableIn and EnableOut bits are set to true. The instruction executes as described in the Operation section.
Instruction first run
N/A
Instruction first scan
N/A
Postscan
EnableIn and EnableOut bits are cleared to false.
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
Condition/State
Action Taken
Prescan
N/A
Normal Scan
Out = In1 OR In2
Instruction first run
N/A
Instruction first scan
N/A
Postscan
N/A
Example
Function Block Diagram
FBD Block
In this example, bool_in1 is copied into BOR_02.In1, bool_in2 is copied into BOR_02.In2, the result of performing OR of all BOR_02 inputs is placed into BOR_02.Out, and BOR_02.Out is then copied into value_result_or.
If bool_in1 is:
If bool_in2 is:
Then value_result_or is:
0
0
0
0
1
1
1
0
1
1
1
1
BOR_FBD_ex_v31
FBD Function
FBD Funct_exam
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal