Bitwise Exclusive Or (XOR)

This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
The XOR instruction performs a bitwise XOR operation using the bits in Source A and Source B and places the result in Dest.
Available Languages
Ladder Diagram
XOR_LD_avail_v31
Function Block Diagram
Function Block Diagram supports these elements:
Function Block
XOR_FBD_avail_v31
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
XOR_avail_FBDFunction_v33
Structured Text
This instruction is not available in structured text.
TIP: Use XOR as an operator in an expression to compute the same result. Refer to Structured Text Syntax for more information on the syntax of expressions and assignments within structured text.
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data Conversions.
Ladder Diagram
Operand
Data Type
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Data Type
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Format
Description
Source A
SINT
INT
DINT
REAL
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
immediate
tag
Value to XOR with Source B. //Float includes REAL and LREAL data types.
TIP: Float inputs are converted to integer which may cause an overflow.
Source B
SINT
INT
DINT
REAL
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
immediate
tag
Value to XOR with Source A.
NOTE: Float inputs are converted to integer which may cause an overflow.
Dest
SINT
INT
DINT
REAL
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
tag
Tag to store result of the instruction.
TIP: If the destination type is Float, the resultant value will be converted to Float.
TIP: When integer promotion is required for the inputs, the smaller type is converted to the larger type using zero extension.
Function Block
Operand
Data Type
Format
Description
XOR
FBD_LOGICAL
tag
XOR structure
FBD_LOGICAL Structure
Input Members
Data Type
Description
EnableIn
BOOL
Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true.
SourceA
DINT
Value to XOR with SourceB.
SourceB
DINT
Value to XOR with SourceA.
Output Members
Data Type
Description
EnableOut
BOOL
Indicates if the instruction executed without fault when it was enabled.
Dest
DINT
Result of the instruction.
FBD Function
Input Operands (Left Pins)
Data Type
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Description
SourceA (top)
SINT
USINT
INT
UINT
DINT
UDINT
LINT
ULINT
REAL
LREAL
Value to OR with Source B.
SourceB (bottom)
SINT
USINT
INT
UINT
DINT
UDINT
LINT
ULINT
REAL
LREAL
Value to OR with Source A.
Output Operand (Right Pin)
Data Type
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Description
Dest
DINT
UDINT
LINT
ULINT
Result of the function.
Description
When enabled, the instruction evaluates the bitwise XOR operation:
Dest = Source A XOR Source B
If the bit in
Source A is:
And the bit in
Source B is:
The bit in
Dest is:
0
0
0
0
1
1
1
0
1
1
1
0
Affects Math Status Flags
Controllers
Affects Math Status Flags
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Conditional
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in
Dest is set as described in the Description section.
Postscan
N/A
Function Block
Condition/State
Action Taken
Prescan
N/A
EnableIn is false
Set EnableOut to EnableIn
EnableIn is true
Set EnableOut to EnableIn
Dest is set as described in the Description section.
Instruction first run
N/A
Instruction first scan
N/A
Postscan
N/A
Examples
Ladder Diagram
L5K_XOR_LD_ex_v31
Function Block
XOR_FBD_ex_v31
FBD Function
XOR_example_FBDFunction_v33
Structured Text
value_result_XOR := value_1 XOR value_2;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal