Motion Axis Shutdown (MASD)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
ControlLogix
5580,
GuardLogix
5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
Use the Motion Axis Shutdown (MASD) instruction to force a specified axis into the Shutdown state. The Shutdown state of an axis is the condition where the drive output is disabled, servo loop deactivated, and any available or associated OK solid-state relay contacts open. The axis remains in the Shutdown state until either an Axis or Group Shutdown Reset is executed.
Architecture and safety support
Architecture
Standard
Safety
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
No
Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers
Yes
No
Available Languages
Ladder Diagram
MASD_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
MASD(Axis,MotionControl);
Operands
Ladder Diagram and Structured Text
Operand
Type
CompactLogix
5380,
ControlLogix
5580,
Compact GuardLogix
5380,
GuardLogix
5580, and ControlLogix 5590 controllers
Type
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370, and
GuardLogix
5570 controllers
Format
Description
Axis
AXIS_CIP_DRIVE
AXIS_VIRTUAL
AXIS_CIP_DRIVE
AXIS_GENERIC
AXIS_GENERIC_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE
AXIS_VIRTUAL
TIP: AXIS_GENERIC is supported by the
ControlLogix
5570 and the
GuardLogix
5570 controllers only.
Tag
Name of the axis on which to perform operation.For controllers that support the REF_TO motion data types, the supported axis operand type can be replaced by an equivalent REF_TO type.
Motion
MOTION_INSTRUCTION
Structure used to access instruction status parameters.
See Structured Text Syntax for more information on the syntax of expressions within structured text.
MOTION_INSTRUCTION Structure
Mnemonic
Description
.EN (Enable) Bit 31
It is set when the rung makes a false-to-true transition and remains set until the servo message transaction is completed and the rung goes false.
.DN (Done) Bit 29
It is set when the axes have been successfully set to Shutdown state.
.ER (Done) Bit 28
It is set to indicate that the instruction detected an error, such as if you specified an unconfigured axis.
Description
The MASD instruction directly and immediately disables drive output, disables the servo loop, and opens any associated OK contacts. This action places the axis into the Shutdown state.
Another action initiated by the MASD instruction is the clearing of all motion processes in progress and the clearing of all the motion status bits. Associated with this action, the command also clears all motion instruction IP bits that are currently set for the targeted axis.
The MASD instruction forces the targeted axis into the Shutdown state. One of the unique characteristics of the Shutdown state is that, when available, the OK solid state relay contact for the motion module or drive is Open. Where available this feature can be used to open up the E-Stop string that controls main power to the drive system. Note that there is typically only one OK contact per motion module which means that execution of an MASD instruction for either axis associated with a given module opens the OK contact.
Another characteristic of the Shutdown state is that any instruction that initiates axis motion is blocked from execution. Attempts to do so result in an execution error. Only by executing one of the Shutdown Reset instructions can motion be successfully initiated.
The axis remains in the shutdown state until a Motion Axis Shutdown Reset (MASR), a Motion Group Shutdown Reset (MGSR), or a Motion Coordinate Shutdown Reset (MCSR) instruction executes. If the axis is associated with a Coordinate System, the axis will be reset if the Motion Coordinate Shutdown Reset (MCSR) instruction executes.
IMPORTANT: The instruction execution may take multiple scans to execute because it requires multiple coarse updates to complete the request. The Done (.DN) bit is not set immediately, but only after the request is completed.
Additionally, for CIP motion, the MASD instruction supports canceling the Motion Drive Start (MDS) instruction. This includes clearing the MDS In Process (.IP) bit, and clearing the DirectVelocityControlStatus and the DirectTorqueControlStatus bit in the Motion Status attribute.
In this transitional instruction, the relay ladder, toggle the Rung-condition-in from cleared to set each time the instruction should execute.
Master Driven Speed Control (MDSC) and the MASD Instruction
When the axis is shut down:
  • The IP bit of the Master Driven Axis Control (MDAC) instruction is reset on an axis that is shutdown.
  • The AC bit of the MDAC instruction is reset when the axis is stopped as it is shutdown.
  • The MASD instruction clears the pending Master Axis for all future single motion instructions.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction.A major fault can occur if an uninitialized reference or a reference of the incorrect type is passed to the Axis operand. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
The .EN, .DN, and .ER are cleared to false.
Rung-condition-in is false
The .EN bit is cleared to false if the .DN or .ER bit is true.
Rung-condition-in is true
The .EN bit is set to true and the instruction executes. If the EN bit is set to false, then there is no action taken.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table
Normal execution
See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table.
Error Codes
See Motion Error Codes .ERR for Motion Instructions.
Extended Error Codes
Extended Error Codes provide additional instruction-specific information for the error codes that are generic to many instructions. See Motion Error Codes .ERR for Motion Instructions.
MASD Changes to Single Axis Status Bits
Axis Status Bits
Bit Name
State
Meaning
ServoActionStatus
FALSE
The axis is in the Servo Off state with the servo loop inactive.
DriveEnableStatus
FALSE
The drive enable output is inactive.
ShutdownStatus
TRUE
The axis is in the shutdown state.
Motion Status Bits
Bit Name
State
Meaning
AccelStatus
FALSE
Axis is not Accelerating.
DecelStatus
FALSE
Axis is not Decelerating.
MoveStatus
FALSE
Axis is not Moving.
JogStatus
FALSE
Axis is not Jogging.
GearingStatus
FALSE
Axis is not Gearing.
HomingStatus
FALSE
Axis is not Homing.
StoppingStatus
FALSE
Axis is not Stopping.
PositionCamStatus
FALSE
Axis is not Position Camming.
TimeCamStatus
FALSE
Axis is not Time Camming.
PositionCamPendingStatus
FALSE
Axis does not have a Position Cam Pending.
TimeCamPendingStatus
FALSE
Axis does not have a Time Cam Pending.
GearingLockStatus
FALSE
Axis is not in a Gear Locked condition.
PositionCamLockStatus
FALSE
Axis is not in a Cam Locked condition.
DirectVelocityControlStatus
FALSE
Axis is not under Direct Velocity Control.
DirectTorqueControlStatus
FALSE
Axis is not under Direct Torque Control.
Examples
Ladder Diagram
Ladder Diagram
Structured Text
MASD(myAxis, myMotionControl);
Relay Ladder
L5K_MASD_LD_ex_v31
Structured Text
MASD(myAxis, myMotionControl);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal