MVC wiring and programming example
This topic demonstrates how to wire the Guard I/O module and program the instruction in the safety control portion of an application.
TIP:
The standard control portion of the application is not shown in the following
diagram.
Wiring Diagram

This programming diagram shows the Main Valve Control (MVC) instruction with inputs and outputs.
Programming Diagram

Ladder Diagram

Module Definition
The following sections provide examples of how to use the programming software to set the Guard I/O module configuration operands.

Rockwell Automation suggests selecting
Exact Match
for the Electronic Keying
as shown. It also acceptable to select Compatible Match
.Module Input Configuration

Module Test Output Configuration

Module Output Configuration

Provide Feedback