EPMS wiring and programming example

This topic demonstrates how to wire the Guard I/O module and the instruction in the safety control portion of an application.
TIP: The standard control portion of the application is not shown in the following diagram.
Wiring Diagram
EPSM wiring example
Programming Diagram
This programming diagram shows the instruction with inputs and outputs.
EPMS programming diagram
Ladder Diagram
EPMS_Other_Pg297_v31
Module Definition
The following sections provide examples of how to use the programming software to set the
Guard I/O
module configuration operands
L5K_EPMS_Other_Pg298_1_v31
Rockwell Automation suggests selecting
Exact Match
for the
Electronic Keying
as shown.
Compatible
Match
is also acceptable.
Module Input Configuration
EPMS_Other_Pg298_2_v31
Module Output Configuration
EPMS_Other_Pg299_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal