Clutch Brake Single Stroke Mode (CBSSM)
This instruction applies to the Compact GuardLogix 5370, GuardLogix 5570, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers.
The Clutch Brake Single Stroke Mode (CBSSM) instruction is used in single-cycle press applications.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
This instruction is not available in structured text.
WARNING:
Do not use automatic acknowledgment when access within the danger zone
can go undetected. This instruction, when configured for automatic acknowledgment, must be
used in combination with other instructions, at least one of which must fulfill the manual
reset requirement.
Reset controls must be located within sight, but out of reach of the
danger zone.
See section 5.4.1.3 of EN692-2005 for details.
WARNING:
ATTENTION:
This instruction is specified with the intent that the
Slide Zone input is sourced only by the Slide Zone output of the Crankshaft Position Monitor
(CPM) instruction or application logic that satisfies the Slide Zone requirements listed in
this instruction.This instruction is specified with the intent that the Enable input is
sourced only by an Ox output1 of the Eight Position Mode Selector (EPMS) instruction that
is not already sourcing the Enable input of another (CBIM), Clutch Brake Single Stroke
Mode (CBSSM), or Clutch Brake Continuous Mode (CBCM) instruction.
1 Where x = 1 through 8
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Structure operands are shared by multiple instructions.
WARNING:
The CBSSM structure contains internal state information. If any of the
configuration operands are changed while in run mode, the state information must be
re-initialized by making the rung-condition-in false.
The following table provides the operands used to configure the instruction.
Operand | Data Type | Format | Description | ||
---|---|---|---|---|---|
CBSSM | CB_SINGLE_STROKE_MODE | tag | Data structure required for proper operation of instruction. | ||
Ack Type | BOOL | list item | This operand specifies how to acknowledge a Safety Enable OFF (0) to ON (1) transition. This acknowledgment must be made before Output 1 can be energized. | ||
AUTOMATIC (1) | The acknowledgment is made automatically when the Safety Enable input transitions from OFF (0) to ON (1). | ||||
MANUAL (0) | The acknowledgment is made when Safety Enable Ack transitions from OFF (0) to ON (1) after the Safety Enable input transitions from OFF (0) to ON (1). | ||||
Takeover Mode | BOOL | list item | This operand determines where the press is stopped when the Safety Enable and/or Start input transitions from ON (1) to OFF (0) while the slide is in the Up zone.
IMPORTANT:
When using this instruction with
Takeover Mode Enabled, safety devices that are continuously active, such as
E-stops, must directly drive the Enable operand of the CBSSM instruction. The
application developer is responsible for determining the safety devices that are
not continuously active, such as certain light curtains, two-hand run stations,
and others, which may be used to drive the Safety Enable operand and can be muted
during press upstroke.
| ||
ENABLED (1) | The press is stopped when the slide enters the Top zone. | ||||
DISABLED (0) | The press is stopped immediately. |
The following table explains the instruction inputs.
Operand | Data Type | Format | Description | |||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Enable | BOOL | tag | This input is the signal to activate this instruction; for example, by an Eight Position Mode Selector (EPMS) Ox output, where x = 1 through 8. ON (1): The instruction is selected and operational. OFF (0): The instruction is not operating. All instruction outputs are de-energized. | |||||||||||||||||||||||||
Safety Enable | BOOL | tag | This input represents the status of safety-related permissive devices such as E-stops, light curtains or safety gates. ON (1): Permissive devices are actively guarding the danger zone. Permits the energizing of Output 1. OFF (0): Permissive devices are in a state that doesn't allow Output 1 to be energized. | |||||||||||||||||||||||||
Standard Enable | BOOL | tag | Indicates the state of non safety-related permissive devices. ON (1): Permits the energizing of Output 1. OFF (0): Prevents the energizing of Output 1. This operand is not safety-related. | |||||||||||||||||||||||||
Start | BOOL | tag | Input to start press movement. ON (1): Energize Output 1 if all input conditions have been met. OFF (0): Output 1 is de-energized. | |||||||||||||||||||||||||
Press In Motion | BOOL | tag | Source this input by Output 1 of the Camshaft Monitor (CSM) instruction or by user application logic. Feedback from the press safety valve needs to be included in the building of this signal. ON (1): Indicates that the press is moving. OFF (0): Indicates that the press is stopped. | |||||||||||||||||||||||||
Slide Zone | DINT | tag | This input represents the position of the slide and the position information status. It is sourced by the Crankshaft Position Monitor (CPM) instruction's Slide Zone output or user application logic that provides the following bit-mapped information. Bit 0: Status OFF (0) - The Slide Zone information is invalid. Prevents the energizing of Output 1 on an initial start or immediately stops the press. ON (1) - Slide Zone information is valid. Bits 1 and 2: Slide Zone The following table lists how Bits 0 to 2 are used to represent the valid slide zones.
| |||||||||||||||||||||||||
Motion Monitor Fault | BOOL | tag | Stops the press immediately when a press motion problem has been detected. This input is sourced by inverting the Fault Present output coming from the Camshaft Monitor (CSM) instruction or application logic that performs motion diagnostics. ON (1): Indicates that press motion is valid. Permits Output 1 to be energized. OFF (0): Indicates that a press motion problem exists. Prevents Output 1 from being energized or immediately de-energizes Output 1. | |||||||||||||||||||||||||
Safety Enable Ack | BOOL | tag | This input is required when the configured Ack Type is Manual. OFF (0)->ON (1): Acknowledges that the Safety Enable input has transitioned from OFF (0) to ON (1). |
The following table explains the instruction outputs.
Operand | Data Type | Description |
---|---|---|
Output 1 (01) | BOOL | Output used to source the Actuate input of the Main Valve Control (MVC) instruction. ON (1): The output is energized. OFF (0): The output is de-energized. See Energizing Output 1 and De-energizing Output 1. |
Diagnostic Code | DINT | This operand is not safety-related. See Diagnostic Codes. |
IMPORTANT:
Do not write to any instruction output tag under any
circumstances.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Condition/State | Action Taken |
---|---|
Prescan | Same as Rung-condition-in is false. |
Rung-condition-in is false | The .O1 is cleared to false. The Diagnostic Code output is set to 0. |
Rung-condition-in is true | The instruction executes as described in the Operation section. |
Postscan | Same as Rung-condition-in is false. |
Operation
Energizing Output 1
Output 1 is energized only when the Start input transitions from OFF (0) to ON (1) and all of these conditions are met:
- The Enable input is ON (1).
- The Safety Enable input has been acknowledged.
- The Standard Enable input is ON (1).
- The Slide Zone input represents the Top zone.
- The Motion Monitor Fault input is ON (1).
- The Press In Motion input is OFF (0).
- The Safety Enable Ack input is OFF (0).IMPORTANT: If the Ack Type is Manual, an acknowledgment of the Safety Enable input is required when the Enable input transitions from OFF (0) to ON (1) and before the Start input turns ON (0).
WARNING:
When the configured Ack Type is Automatic, Output 1 is energized when the
Safety Enable, Standard Enable, Press In Motion, and Motion Monitor Fault inputs return to
the active or valid state at the same time the Start input transitions from OFF (0) to ON
(1).
WARNING:
Output 1 can be re-energized when the Slide Zone input is Down, providing
that Output 1 had been initially energized when the Slide Zone input was Top, and Output 1
was de-energized because the Start input turned OFF (0).
Any other reason for Output 1
being de-energized requires that the slide be inched back to the Top position.
WARNING:
The cam switches that determine slide position are monitored by the CPM
instruction. This instruction uses the Slide Zone output of the CPM instruction as a
representation of the cam switches that determine slide position.
Energizing Output 1 Timing
This diagram demonstrates the acknowledgment of the Safety Enable input, at (A) and the energizing of Output 1 when the Start input transitions from OFF (0) to ON (1) at (B) and all input conditions have been met. The safety enable acknowledgment only needs to be made once while the Safety Enable input is ON (1) when the configured Ack Type is Manual.

De-energizing Output 1
Once energized, Output 1 is de-energized when one or more of the following occurs:
- The Enable input transitions from ON (1) to OFF (0).
- The Start input transitions from ON (1) to OFF (0).When this transition occurs while the slide is in the Up zone and the Takeover Mode is Enabled, Output 1 is de-energized when the slide enters the Top zone. Otherwise, when the Takeover Mode is Disabled, Output 1 is de-energized immediately. Output 1 is also de-energized immediately when this transition occurs while the slide is in the Top or Down zones.
- The Safety Enable input transitions from ON (1) to OFF (0). When this transition occurs while the slide is in the Up zone and Takeover Mode is enabled, Output 1 is de-energized when the slide enters the Top zone. Otherwise, when the Takeover Mode is disabled, Output 1 is de-energized immediately. Output 1 is also de-energized immediately when this transition occurs while the slide is in the Top or Down zones.
- The Standard Enable input transitions from ON (1) to OFF (0). When this transition occurs while the slide is in the Up zone, Output 1 is de-energized when the slide enters the Top zone. Otherwise, Output 1 is de-energized immediately.
- The Slide Zone input value becomes invalid.
- The slide transitions to the Top zone.
- The Monitor Motion Fault input transitions from ON (1) to OFF (0).
- The direction of the press appears to be running in reverse.
- The Press In Motion input is OFF (0) when the slide transitions from Top to Down.
- The Press in Motion input transitions from ON (1) to OFF (0).
This diagram shows the de-energizing of Output 1 when the Safety Enable input transitions from ON (1) to OFF (0) at (A). An acknowledgment of the Safety Enable input is required when the Safety Enable input transitions from OFF (0) to ON (1) at (B) before Output 1 can be re-energized.

False Rung State Behavior
When the instruction is executed on a false rung, all instruction outputs are de-energized.
Diagnostic Codes and Corrective Actions
Diagnostics 2000H through 200AH are detected when attempting to start press movement by energizing Output 1. Diagnostics 2020H through 202D are used to diagnose the reason for stopping press movement by de-energizing Output 1.
The diagnostic codes are listed in hexadecimal format followed by decimal format.
Diagnostic Code | Description | Corrective Action | |
---|---|---|---|
0 | No fault. | None. | |
16#2000 8192 | Output 1 failed to energized when the Start input turned ON (1), due to an invalid Slide Zone input value. | Check the Crankshaft Position Monitor (CPM) instruction or the application logic used to source this input. This diagnostic is cleared when a valid Slide Zone is established. | |
16#2001 8193 | Output 1 failed to energize when the Start input turned ON (1) due to the Press In Motion input being ON (1). |
This diagnostic is cleared when the Press In Motion input turns OFF (0). | |
16#2002 8914 | Output 1 failed to energize when the Start input turned ON (1) prior to the acknowledgement of the Safety Enable input. |
| |
16#2003 8915 | Output 1 failed to energize when the Start input turned ON (1) due to the Standard Enable input being OFF (0). | Verify that the devices used to source the Standard Enable input are functioning properly. This diagnostic is cleared when the Standard Enable input is ON (1). | |
16#2008 8200 | Output 1 failed to energize when the Start input turned ON (1) due to the Motion Monitor Fault input being OFF (0). | Check the Camshaft Monitor (CSM) instruction or the application logic used to monitor press movement. This diagnostic is cleared when the motion monitor functions are properly monitoring motion and the Motion Monitor Fault input is ON (1). | |
16#2009 8201 | Manual Ack Type | Output 1 failed to energize when the Start input turned ON (1) due to the Safety Enable Ack input being ON (1). | Turn the Safety Enable Ack input OFF (0). This diagnostic is cleared when the Safety Enable Ack input turns OFF (0). |
Automatic Ack Type | N/A | ||
16#200A 8202 | Output 1 failed to energize when the Start input turned ON (1) due to the slide being in the Up or Down zone. | The slide must be in the Top zone to initiate press movement. This diagnostic is cleared when the slide is inched back to the Top zone. | |
16#2020 8224 | Output 1 is de-energized due to the Slide Zone input value becoming invalid. | Check the Crankshaft Position Monitor (CPM) instruction or the application logic used to source this input. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2021 8225 | Output 1 is de-energized due to the Motion Monitor Fault input turning OFF (0). | Check the Camshaft Monitor (CSM) instruction or the application logic used to monitor press movement. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2022 8226 | Output 1 is de-energized due to the detection of press movement in the reverse direction. | Verify the direction of the press. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2023 8227 | Output 1 is de-energized due to the Safety Enable input turning OFF (0) while the slide was in the Top or Down zone. | Verify that the AOPDs and ESPEs used to source the Safety Enable input are protecting their respective areas. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2024 8228 | Output 1 is de-energized due to the Standard Enable input turning OFF (0) while the slide was in the Top or Down zone. | Verify that the devices and application logic used to source the Standard Enable input are functioning properly. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2025 8229 | Output 1 is de-energized due to the Start input turning OFF (0) while the slide was in the Top or Down zones. | Output 1 is always de-energized when the Start input turns OFF (0) while the slide is in the Top or Down zones. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2026 8230 | Not used by this instruction. | ||
16#2027 8231 | Output 1 is de-energized immediately when the Safety Enable input turned OFF (0) while the slide was in the Up zone and the Takeover Mode is Disabled. | Verify that the AOPDs and ESPEs used to source the Safety Enable input are protecting their respective areas. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2028 8232 | Output 1 is de-energized when the slide entered the Top zone due to the Standard Enable input turning OFF (0) while the slide was in the Up zone. | Verify that the devices and application logic used to source the Standard enable input are functioning properly. This diagnostic is cleared at the next attempt to begin press movement. | |
16#2029 8233 | Output 1 is de-energized immediately when the Start input turned OFF (0) while the slide was in the Up zone and the Takeover Mode is Disabled. | This diagnostic is cleared at the next attempt to begin press movement. | |
16#202A 8234 | Output 1 is de-energized due to the slide entering the Top zone. | Output 1 is always de-energized when the slide enters the Top zone. This diagnostic is cleared at the next attempt to begin press movement. | |
16#202B 8235 | Output 1 is de-energized due to the Press In Motion input remaining OFF (0) when the slide entered the Down zone or the Press In Motion input transitioned from ON (1) to OFF (0. | Check the Camshaft Monitor (CSM) instruction or the application logic used to monitor press movement. This diagnostic is cleared at the next attempt to begin press movement. | |
16#202C 8236 | Output 1 is de-energized when the slide entered the Top zone and the Safety Enable input turned OFF (0) while the slide was in the Up zone, when the Takeover Mode is Enabled. | Verify that the AOPDs and ESPEs used to source the Safety Enable input are protecting their respective areas. This diagnostic is cleared at the next attempt to begin press movement. | |
16#202D 8237 | Output 1 is de-energized when the slide entered the Top zone and the Start input turned OFF (0) while the slide was in the Up zone when the Takeover Mode is Enabled. | This diagnostic is cleared at the next attempt to begin press movement. |
Examples
Ladder Diagram

Provide Feedback