AVC wiring and programming example

This topic demonstrates how to program the instruction in the safety control portion of an application.
TIP: The standard control portion of the application is not shown in the following diagram.
Wiring Diagram
Logix5000AVCWirDiag
Programming Diagram
This programming diagram shows the Auxiliary Valve Control (AVC) instruction used with a Main Valve Control (MVC) instruction.
Logix5000AVCPgmDiag
Ladder Diagram
AVC_Other_LD_v31
The Logix Designer application is used to configure the input and test output operands of the Guard I/O, as illustrated.
Module Definition
AVC_mod input config_v31
Rockwell Automation
suggests using Exact Match, as shown. However, setting Electronic Keying to Compatible Match is allowed.
Module Input Configuration
AVC_Other_Pg320_2_v31
Module Test Output Configuration
AVC_mod test output config_v31
Module Output Configuration
AVC_module output configure_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal