Reference (REF)

This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
The Reference (REF) Instruction associates a reference with the address of an axis or coordinate system concrete tag.
This is a transitional instruction. Follow these steps when using it:
  • In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
  • In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Instructions
Ladder Diagram
l5k_ref_ld_ex_v36.png
Function Block
This instruction is not available in function block.
Structured Text
REF(Source, Reference);
Operands
Operand
Type
Format
Description
Source
AXIS_CIP_DRIVE
AXIS_CONSUMED
AXIS_GENERIC_DRIVE
AXIS_SERVO
AXIS_SERVO_DRIVE
AXIS_VIRTUAL COORDINATE_SYSTEM
Immediate Tag
Name of the axis or coordinate system to reference.
Reference
REF_TO_AXIS_CIP_DRIVE
REF_TO_AXIS_CONSUMED
REF_TO_AXIS_GENERIC_DRIVE
REF_TO_AXIS_SERVO
REF_TO_AXIS_SERVO_DRIVE
REF_TO_AXIS_VIRTUAL
REF_TO_COORDINATE_SYSTEM
Tag
Name of the reference to be populated.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction.
Execution
Condition/State
Action Taken
Prescan
The instruction uses the Source address to populate the Reference.
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in. The instruction uses the Source address to populate the Reference.
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in. The instruction uses the Source address to populate the Reference.
Postscan
The instruction uses the Source address to populate the Reference.
Error Codes
None specific to this instruction.
Example
Relay Ladder
Structured Text
REF(AxisCip, Ref_AxisCip);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal