Access the AddOnInstructionDefinition Object

The
AddOnInstructionDefinition
object lets you customize instructions for sets of commonly-used logic, provides a common interface to this logic, and provides documentation for the instruction.
Attribute
Data Type
Instruction within Standard Task
Instruction within Safety Task
Description
LastEditDate
LINT
GSV
None
Coordinated Universal Time (UTC) value of the last time the AOI was edited.
The LastEditDate is a 64-bit µS value referenced from 0000 hours, January 1, 1970.
MajorRevision
DINT
GSV
None
Major revision number of the Add-On Instruction (AOI).
MinorRevision
DINT
GSV
None
Minor revision number of the AOI.
Name
String
GSV
GSV
Name of the AOI.
RevisionExtendedText
String
GSV
None
Text describing the revision of the AOI.
SafetySignature ID
DINT
GSV
None
Calculated by firmware based on the AOI compiled logic. Used only for a Safety AOI.
SignatureID
DINT
GSV
None
Calculated by software based on the AOI definition.
Vendor
String
GSV
None
Vendor that created the AOI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal