Faceplate Control - General
Use this tab to define/modify how the control operates.
Parameters
Communication
Select
RSLinx Classic
OPC Server or FactoryTalk Linx
. If you select RSLinx Classic
OPC Server, you must also specify: - whether to launch remotely
- the access path to the remote machine
If you select
FactoryTalk Linx
, you must also specify the FactoryTalk
Area.Tag
Enter the name of a specific function block instruction to connect with this control.
Update Rate
Enter the Update Rate of the control in seconds. You can click the arrows to increment this value in 0.25 second increments. The default value is 1.00 second.
Provide Feedback