Equipment Sequence Clear Failure (SCLF)
This instruction applies to the
Logix Designer
5580P controllers and to ControlLogix 5590P
controllers. Logix Designer
5580P controllers and ControlLogix 5590P controllers
also support controller redundancy.
TIP:
When using this instruction with
ControlLogix
redundancy system, outputs controlled by this
instruction may not be bumpless during redundancy switchover, if the instruction and
sequence program are not scheduled in the highest priority task.
WARNING:
When using redundancy with an
Equipment Sequence
, sequence execution may not be as expected after switchover if the phase and sequence are not scheduled on the same task.Use the
Equipment Sequence
Clear Failure (SCLF) instruction to clear the failure
code of an Equipment Sequence
. Keep this in mind when using the SCLF instruction.- A CLR instruction, MOV instruction, or assignment does not change the failure code of anEquipment Sequence.
- TheEquipment Sequencecannot have other owners when you use the SCLF instruction. The SCLF instruction does not clear the failure code if theLogix Designerapplication,FactoryTalk Batchsoftware, or another program owns theEquipment Sequence.
- AnEquipment Sequencerefuses a RESUME command until it is cleared of failures.
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
The SCLF instruction is available in these languages.
- Ladder diagram
- Structured text: SCLF(SequenceName)
Supported Operands
The SCLF instruction uses these operands.
Operand | Type | Format | Description |
Sequence Name | Sequence | name of the Equipment Sequence | Equipment Sequence for which you want to clear a failure
code. |
Result | DINT | Immediate tag | For an instruction to return a success or failure code, enter a DINT tag where the result code is stored. Otherwise, enter 0 . |
Arithmetic status flags and fault conditions
Arithmetic status flags are not affected by the SCLF instruction. The SCLF instruction cannot trigger a fault, so there are no fault conditions for this instruction.
Instruction execution
The table describes the execution steps for SCLF instructions.
Condition | ![]() | ![]() |
Prescan | The rung-condition-out is set to false. | No action taken. |
Rung-condition-in is false | The rung-condition-out is set to false. | N/A |
Rung-condition-in is true |
| N/A |
Scan of structured text | N/A | In structured text, instructions execute each time they are scanned. To limit the scan of an instruction, use a qualifier of an SFC action or a structured text construct that includes a condition, such as if, then, or else. |
Instruction execution | The instruction clears the value of the failure code for the specified Equipment Sequence . | The instruction clears the value of the failure code for the specified Equipment Sequence . |
Postscan | The rung-condition-out is set to false. | No action taken. |
Provide Feedback