Attach to Equipment Sequence (SATT)
This instruction applies to the
Logix Designer
5580P controllers and to ControlLogix 5590P
controllers. Logix Designer
5580P controllers and ControlLogix 5590P controllers
also support controller redundancy.
TIP:
When using this instruction with
ControlLogix
redundancy system, outputs controlled by this
instruction may not be bumpless during redundancy switchover, if the instruction and
sequence program are not scheduled in the highest priority task.
WARNING:
When using redundancy with an
Equipment Sequence
, sequence execution may not be as expected after switchover if the phase and sequence are not scheduled on the same task.Use the Attach to
Equipment Sequence
(SATT) instruction to take ownership of an Equipment Sequence
. An Equipment Sequence
may be commanded by a program if the program either owns the Equipment Sequence
or the Equipment Sequence
has no owners. A tag must be assigned to store the result code of an SATT instruction.The SATT instruction returns one of five result codes. Result code 0 indicates that the SATT instruction ran successfully. The other four codes indicate that the instruction did not run successfully and provide additional information about the reason for the instruction failure.
This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Function Block Diagram
This instruction is not available in function block.
Structured Text:
SATT(Sequence Name, Result)
Operands
Ladder Diagram
Operand | Data Type | Format | Description |
Sequence Name | SEQUENCE | name of the Equipment Sequence | Equipment Sequence that you want to change to own (attach) to command. |
Result | DINT | Tag | For the instruction to return a success or failure code, enter a DINT tag where the result code is to be stored. Otherwise, enter 0. |
Structured Text
The operands are the same as for the Ladder Diagram.
Guidelines for using the SATT Instruction
Guideline | Details |
---|---|
Remember that the Logix Designer application overrides ownership of the Equipment Sequence . | Regardless of whether a program or FactoryTalk Batch software owns an Equipment Sequence , the option exists to use Logix Designer to override ownership and command the Equipment Sequence . |
The Equipment Sequence must be either owned by the program to command it or have no owners for the program to command it. | The ownership instructions are Attach (SATT) and Detach (SDET).Internal Sequencers (programs), external sequencers ( FactoryTalk Batch ), and operators use an Attach command to command an Equipment Sequence . |
When the Equipment Sequence is done, relinquish ownership. | To relinquish ownership, use a Detach from Equipment Sequence (SDET) instruction. |
Avoid making unnecessary command requests if the Equipment Sequence is generating sequence events. | Unnecessary command requests can flood the event processing buffers and cause you to miss significant events. |
Use the Result code to verify ownership, and include steps that should take place if the attachment fails because the Equipment Sequence is owned by another program or operator. | Use the Result operand to get a code that shows the success or failure of the SATT instruction.On each execution, the SATT instruction tries to take ownership of the Equipment Sequence . When a program or operator owns an Equipment Sequence , another execution of the SATT instruction fails and produces result code 24582. When you use the SATT instruction, either:
|
SATT Result Codes
Code (Dec) | Description |
---|---|
0 | The command was successful. |
24579 | The Equipment Sequence cannot be commended.Logix Designer already owns the Equipment Sequence . The caller attached to the Equipment Sequence , but it is not the current commanding owner.
|
24582 | The program already owns the Equipment Sequence . |
24593 | One of these already owns the Equipment Sequence .
|
24594 | The Equipment Sequence is unscheduled, inhibited, or in a task that is inhibited. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index Through Arrays[1] for operand related faults.
Execution
At instruction execution, the SATT instruction attempts to take ownership of the
Equipment Sequence
.Ladder Diagram
Condition | Action Taken |
---|---|
Prescan | No action taken |
Rung-condition-in is false | No action taken |
Rung-condition-in is true |
|
Postscan | No action taken |
Structured Text
Condition | Action Taken |
---|---|
Prescan | No action taken |
Rung-condition-in is false | No action taken |
Rung-condition-in is true | The instruction executes |
Postscan | No action taken |
Example

Structured Text
if (AttachControl) then
SATT(Make_Product_101, Result);
end_if
Provide Feedback