Phase State Complete (PSC)
This instruction applies to the Compact GuardLogix 5370, Compact
GuardLogix 5380, CompactLogix 5370, CompactLogix 5380, GuardLogix 5570, GuardLogix 5580,
ControlLogix 5570, ControlLogix 5580, and ControlLogix 5590 controllers.
TIP:
When using this instruction with ControlLogix redundancy system, outputs
controlled by this instruction may not be bumpless during redundancy switchover, if the
instruction and phase program are not scheduled in the highest priority task.
The PSC instruction signals the completion of a phase state routine.

In the running state routine, use the PSC instruction to transition the equipment phase to the complete state.
- This is a transitional instruction. Follow these steps when using it:
- In ladder logic, insert an instruction to toggle the rung-condition-in from false to true each time the instruction should execute.
- In a Structured Text routine, insert a condition for the instruction to cause it to execute only on a transition.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
PSC( );
Operands
Ladder Diagram
None
Structured Text
None
Enter the parentheses ( ) after the instruction mnemonic, even though there are no operands.
Guidelines for using the PSC Instruction
Guideline | Details |
---|---|
Use the PSC instruction in each phase state routine that is added to an equipment phase. | Without a PSC instruction, the equipment phase remains in the state and does not go to the next state.
|
![]() | In the holding state routine, use the PSC instruction to let the equipment phase go to the Held state |
Remember that the PSC instruction does not stop the current scan of a routine. | When the PSC instruction executes, the controller scans the rest of the routine and then transitions the equipment phase to the next state. The PSC instruction does not terminate the execution of the routine. |
Do not use a PSC instruction in a prestate routine. | Use the PSC instruction only to signal the transition from one state to another. |
Affects Math Status Flags
No
Major/Minor Faults
A major fault will occur if: | Fault type | Fault code |
---|---|---|
Instruction is called from outside an equipment phase program. | 4 | 91 |
If an Add-On Instruction used a PSC instruction and a non-equipment phase program calls the Add-On Instruction,
Logix Designer
gives a warning. Check the Add-On Instruction for this instruction and disallow it. See Index Through Arrays
for operand-related faults.Execution
In structured text, instructions execute each time they are scanned. To limit the scan of an instruction, use a qualifier of an SFC action, a structured text construct, or both.
Condition/State | Action Taken |
---|---|
Prescan | No action taken. |
Postscan | No action taken. |
EnableIn is false | No action taken. |
EnableIn is true | The instruction executes. |
Examples
Ladder Diagram

Structured Text
If TagEnableRunning
And PSCTest.Running Then
PSC();
End_if;
Provide Feedback