S-Curve (SCRV)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
CompactLogix
5380,
ControlLogix
5580, and ControlLogix 5590 controllers.
The SCRV instruction performs a ramp function with an added jerk rate. The jerk rate is the maximum rate of change of the rate used to ramp output to input.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram.
Function Block
RSL5K_SCRV Function Block_v31
Structured Text
SCRV(SCRV_tag);
Operands
Function Block
Operand
Type
Format
Description
SCRV tag
S_CURVE
Structure
SCRV structure
Structured Text
Operand
Type
Format
Description
SCRV tag
S_CURVE
Structure
SCRV structure
See Structured Text Syntax for more information of the syntax of expressions within structured text.
S_CURVE Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set.
In
REAL
The analog signal input to the instruction.
Valid = any float
Default = 0.0
Initialize
BOOL
The Initialize input to the instruction. When set, the instruction holds Out = InitialValue
Default is cleared.
InitialValue
REAL
Initial value of S-Curve. When Initialize is set, Out = InitialValue.
Valid = any float
Default = 0.0
AbsAlgRamp
BOOL
Ramp type. If set, the instruction functions as an absolute value ramp. If cleared, the instruction functions as an algebraic ramp.
Default is set
AccelRate
REAL
Acceleration rate in input units per second
2
. A value of zero prevents Out form accelerating. When AccelRate < 0, the instruction assumes AccelRate = 0 and sets the appropriate bit in Status.
Valid = 0.0 to maximum positive float
Default = 0.0
DecelRate
REAL
Deceleration rate in input units per second
2
. A value of zero prevents Out form decelerating. When the DecelRate < 0, the instruction assumes DecelRate = 0 and sets the appropriate bit in Status.
Valid = 0.0 to maximum positive float
Default = 0.0
JerkRate
REAL
Jerk rate in input units per second
3
. Specifies the maximum rate of change in the acceleration and deceleration rates when ramping output to input. When (JerkRate * DeltaT) S AccelRate or DecelRate, the acceleration and deceleration rates are not bounded. In this situation, the instruction behaves as a ramp function. When JerkRate < 0, the instruction assumes JerkRate = 0 and sets the appropriate bit in Status.
Valid = 0.0 to maximum positive float
Default = 0.0
HoldMode
BOOL
S-Curve hold mode parameter. This parameter is used with the HoldEnable parameter. If HoldMode is set when HoldEnable is set and Rate = 0, the instruction holds Out constant. In this situation, the instruction holds Out as soon as HoldEnable is set, the JerkRate is ignored, and Out produces a "corner" in its profile. If HoldMode is cleared when HoldEnable is set, the instruction uses the JerkRate to bring Out to a constant value. Out is held when Rate = 0. Do not change HoldMode once HoldEnable is set because the instruction will ignore the change.
Default is cleared.
HoldEnable
BOOL
S-Curve hold enable parameter. When set, Out is held. When cleared, Out moves from its current value until it equals In.
Default is cleared.
TimingMode
DINT
Selects timing execution mode.
0 = periodic mode
1 = oversample mode
2 = real time sampling mode
For more information about timing modes, see Function Block Attributes.
Valid = 0 to 2
Default = 0
OversampleDT
REAL
Execution time for oversample mode.
Valid = 0 to 4194.303 seconds
Default = 0
RTSTime
DINT
Module update period for real time sampling mode
Valid = 1 to 32,767ms
Default = 1
RTSTimeStamp
DINT
Module time stamp value for real time sampling mode.
Valid = 0 to 32,767ms
Default = 0
Output Parameter
Data Type
Description
EnableOut
BOOL
Enable output.
S_Mode
BOOL
S_Mode Output. When (Jerk * DeltaT) Less than or equal to Rate and
Rate < Accel or Decel, S_Mode is set. Otherwise, S_Mode is cleared.
Out
REAL
The output of the S-Curve instruction. Math status flags are set for this output.
Rate
REAL
Internal change in the Out in units per second.
DeltaT
REAL
Elapsed time between updates. This is the elapsed time in seconds used by the control algorithm to calculate the process output.
Status
DINT
Status of the function block.
InstructFault (Status.0)
BOOL
The instruction detected one of the following execution errors. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
AcceRateInv (Status.1)
BOOL
AccelRate is negative.
DecelRateInv (Status.2)
BOOL
DecelRate is negative.
JerkRateInv (Status.3)
BOOL
JerkRate is negative.
TimingModeInv (Status.27)
BOOL
Invalid timing mode.
For more information about timing modes, see Function Block Attributes.
RTSMissed (Status.28)
BOOL
Only used in real time sampling mode. Set when
ABS | DeltaT - RTSTime | > 1 (.001 second).
RTSTimeInv (Status.29)
BOOL
Invalid RTSTime value.
RTSTimeStampInv (Status.30)
BOOL
Invalid RTSTimeStamp value.
DeltaT (Status.31)
BOOL
Invalid DeltaT value.
Description
The primary requirement of the SCRV instruction is to ensure that the rate never changes by more than the specified jerk rate.
You can configure the SCRV instruction to produce an S-Curve profile or a Ramp profile for a step input.
S-Curve Profile
To produce an S-Curve profile, set JerkRate such that (JerkRate * DeltaT) < AccelRate and/or DecelRate.
In S-Curve profile mode, the SCRV instruction ensures that the rate never changes more than the specified JerkRate. The algorithm used to produce the S-Curve profile is designed to produce a smooth, symmetric S-Curve for a step input. A trapezoidal integration of Out is incorporated to facilitate this. As a result, changes in Rate will be less than JerkRate during portions of the profile.
When a step change occurs on the input, rate is increased to the programmed AccelRate or DecelRate. The AccelRate or DecelRate is maintained until a point at which rate must begin decreasing in order for the output to reach input when rate reaches zero.
In some cases, depending on the values of acceleration, deceleration, and jerk, the acceleration rate or deceleration rate might not be reached before the rate must begin decreasing by jerk rate.
For very small step changes, the SCRV instruction will not attempt to produce an 'S' profile. In this mode the entire step will be output and Rate will reflect the change in output. This behavior will occur if Out = In and the next step change to In can be output with a rate less than or equal to the programmed JerkRate.
The SCRV instruction supports an algebraic ramp and an absolute value ramp. For an algebraic ramp, the acceleration condition is defined by an input that is becoming more positive, and the deceleration condition is defined by an input that is becoming more negative. For an absolute value ramp, the acceleration condition is defined by an input moving away from zero, and the deceleration condition is defined by an input moving towards zero.
Ramp Profile
To produce a Ramp profile, set JerkRate such that (JerkRate * DeltaT) Less than or equal to AccelRate and/or DecelRate.
In Ramp Profile mode, the SCRV instruction always produces a rate of change equal to the programmed AccelRate or DecelRate until the difference between Out and In requires less then AccelRate or DecelRate to reach endpoint.
HoldMode = 0 operates the same as HoldMode = 1. When HoldEnable is set, Out is immediately held and Rate becomes zero.
The following diagram illustrates how the instruction modifies Out.
SCRV Ramp Profile
(1)
When Initialize is set, the instruction sets the following:
Outn = InitialValue
Outn-1 = Outn
Raten = 0
Raten-1 = 0
(2)
When HoldMode is cleared, Out is moving toward In, and HoldEnable is set, the rate begins decreasing towards zero at the jerk rate. Due to the JerkRate, Out is held at whatever value it had when the rate reached zero. When the Out is finally held constant, it has a value that is different from the value it had the instant that HoldEnable was set.
When HoldMode is set, Out is moving toward In, and HoldEnable is set, the rate is immediately set to zero. Out is held at whatever value it had when HoldEnable was set.
Reducing the JerkRate during a transition might cause Out to overshoot the In. If overshoot occurs, it is the result of enforcing the entered JerkRate. You can avoid an overshoot by decreasing JerkRate in small steps while tuning or by changing JerkRate while Out = In (not during a transition).
The time that is required for Out to equal a change in the input is a function of AccelRate, JerkRate, and the difference between In and Out.
Calculating Output and Rate Values
In transition from an initial value to final value, Out goes through three regions. In region 1 and region 3, the rate of change of Out is based on JerkRate. In region 2, the rate of change of Out is based on AccelRate or DecelRate.
SCRV Calculating Output and Rate Values
The Out is calculated for each region as follows:
SCRV_fbd_Out_eq
with these equations for each region:
Region
Equation
region 1
SCRV_fbd_region1_eq
region 2
SCRV_fbd_region2_eq
region 3
SCRV_fbd_region3_eq
When:
SCRV_fbd_InitOutput_eq
the SCRV block does not reach the AccelRate or DecelRate. The Out does the following:
SCRV Graph
where:
SCRV_fbd_TotalTime_eq
Affects Math Status Flags
No
Fault conditions
Minor fault occurs when
Fault type
Fault code
Feature is enabled and overflow is detected.
4
4
See Common Attributes for operand-related faults.
Execution
Function Block
Condition
Function Block Action
Prescan
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is false
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is true
EnableIn and EnableOut bit bits are set to true
The instruction executes.
Instruction first run
N/A
Instruction first scan
Clear previous scan data.
Postscan
EnableIn and EnableOut bits are cleared to false
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal Execution
See Tag.EnableIn is true in the Function Block table.
Postscan
See Postscan in the Function Block table.
Example
In most coordinated drive applications, a master reference commands line speed for an entire group of drives. As various references are selected, the drives cannot be presented with "step" changes in speed reference because differences in load inertia, motor torque, and tuning would not allow the individual drive sections to react in a coordinated manner. The SCRV instruction is designed to ramp and shape the reference signal to the drive sections so that acceleration, deceleration, and jerk, (derivative of acceleration,) are controlled. This instruction provides a mechanism to allow the reference to the drives to reach the designated reference setpoint in a manner that eliminates excessive forces and excessive impact on connected machinery and equipment.
Function Block
RSL5K_SCRV Function Block Example_v31
Structured Text
SSUM_01.In1 := Master_reference;
SSUM_01.Select1 := master_select;
SSUM_01.In2 := Jog_reference;
SSUM_01.Select2 := jog_select;
SSUM(SSUM_01);
select_out := SSUM_01.Out;
SCRV_01.In := select_out;
SCRV_01.AccelRate := accel;
SCRV_01.DecelRate := accel;
SCRV_01.JerkRate := jerk_rate;
SCRV(SCRV_01);
scurve_out := SCRV_01.Out
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal