Proportional + Integral (PI)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
CompactLogix
5380,
ControlLogix
5580, and ControlLogix 5590 controllers.
The PI instruction provides two methods of operation. The first method follows the conventional PI algorithm in that the proportional and integral gains remain constant over the range of the input signal (error). The second method uses a non-linear algorithm where the proportional and integral gains vary over the range of the input signal. The input signal is the deviation between the setpoint and feedback of the process.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram.
Function Block
PI_FBD_avail_v31
Structured Text
PI(PI_tag);
Operands
Function Block
Operand
Type
Format
Description
PI tag
PROP_INT
structure
PI structure
Structured Text
Operand
Type
Format
Description
PI tag
PROP_INT
structure
PI structure
See
Structured Text Syntax
for more information on the syntax of expressions within structured text.
PROP_INT Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set.
In
REAL
The process error signal input. This is the difference between setpoint and feedback.
Valid = any float
Default = 0.0
Initialize
BOOL
The instruction initialization command. When set, Out and internal integrator are set equal to the value of InitialValue.
Default is cleared.
InitialValue
REAL
The initial value input. When Initialize is set, Out and integrator are set to the value of InitialValue. The value of InitialValue is limited using HighLimit and LowLimit.
Valid = any float
Default = 0
Kp
REAL
The proportional gain. This affects the calculated value for both the proportional and integral control algorithms. If invalid, the instruction clamps Kp at the limits and sets the appropriate bit in Status.
Valid = any float > 0.0
Default = minimum positive float
Wld
REAL
The lead frequency in radians/second. This affects the calculated value of the integral control algorithm. If invalid, the instruction clamps Wld at the limits and sets the appropriate bit in Status.
Valid = see the Description section below for valid ranges
Default = 0.0
HighLimit
REAL
The high limit value. This is the maximum value for Out. If HighLimit Less than or equal to LowLimit, the instruction sets HighAlarm and LowAlarm, sets the appropriate bit in Status, and sets Out = LowLimit.
Valid = LowLimit < HighLimit Less than or equal to maximum positive float
Default = maximum positive float
LowLimit
REAL
The low limit value. This is the minimum value for Out. If HighLimit Less than or equal to LowLimit, the instruction sets HighAlarm and LowAlarm, sets the appropriate bit in Status, and sets Out = LowLimit.
Valid = maximum negative float Less than or equal to LowLimit < HighLimit
Default = maximum negative float
HoldHigh
BOOL
The hold high command. When set, the value of the internal integrator is not allowed to increase in value.
Default is cleared.
HoldLow
BOOL
The hold low command. When set, the value of the internal integrator is not allowed to decrease in value.
Default is cleared.
ShapeKpPlus
REAL
The positive Kp shaping gain multiplier. Used when In is Greater than or equal to0. If invalid, the instruction clamps ShapeKpPlus at the limits and sets the appropriate bit in Status. Not used when NonLinearMode is cleared.
Valid = 0.1 to 10.0
Default = 1.0
ShapeKpMinus
REAL
The negative Kp shaping gain multiplier. Used when In is < 0. If invalid, the instruction clamps ShapeKpMinus at the limits and sets the appropriate bit in Status. Not used when NonLinearMode is cleared.
Valid = 0.1 to 10.0
Default = 1.0
KpInRange
REAL
The proportional gain shaping range. Defines the range of In (error) over which the proportional gain increases or decreases as a function of the ratio of | In | / KpInRange. When | In | > KpInRange, the instruction calculates the change in proportional error using entered the Kp shaping gain x (In - KpInRange). If invalid, the instruction clamps KpInRange at the limits and sets the appropriate bit in Status. Not used when NonLinearMode is cleared.
Valid = any float > 0.0
Default = maximum positive float
ShapeWldPlus
REAL
The positive Wld shaping gain multiplier. Used when In is Greater than or equal to 0. If invalid, the instruction clamps ShapeWldPlus at the limits and sets the appropriate bit in Status. Not used when NonLinearMode is cleared.
Valid = 0.0 to 10.0
Default = 1.0
ShapeWldMinus
REAL
The negative Wld shaping gain multiplier. Used when In is < 0. If invalid, the instruction clamps ShapeWldMinus at the limits and sets the appropriate bit in Status. Not used when NonLinearMode is cleared.
Valid = 0.0 to 10.0
Default = 1.0
WldInRange
REAL
The integral gain shaping range. Defines the range of In (error) over which integral gain increases or decreases as a function of the ratio of | In | / WldInRange. When
|In| > WldInRange, the instruction limits In to WldInRange when calculating integral error. If invalid, the instruction clamps WldInRange at the limits and sets the appropriate bit in Status. Not used when NonLinearMode is cleared.
Valid = any float > 0.0
Default = maximum positive float
NonLinearMode
BOOL
Enable the non-linear gain mode. When set, the instruction uses the non-linear gain mode selected by ParabolicLinear to compute the actual proportional and integral gains. When cleared, the instruction disables the non-linear gain mode and uses the Kp and Wld values as the proportional and integral gains.
Default is cleared.
ParabolicLinear
BOOL
Selects the non-linear gain mode. The modes are linear or parabolic. When set, the instruction uses the parabolic gain method of y=a * x
2
+ b to calculate the actual proportional and integral gains. If cleared, the instruction uses the linear gain method of y=a * x + b.
Default is cleared.
TimingMode
DINT
Selects timing execution mode.
0 = Periodic mode
1 = Oversample mode
2 = Real time sampling mode
For more information about timing modes, see Function Block Attributes.
Valid = 0 to 2
Default = 0
OversampleDT
REAL
Execution time for oversample mode.
Valid = 0 to 4194.303 seconds
Default = 0
RTSTime
DINT
Module update period for real time sampling mode
Valid = 1 to 32,767ms
Default = 1
RTSTimeStamp
DINT
Module time stamp value for real time sampling mode.
Valid = 0 to 32,767ms
Default = 0
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates the execution status of the instruction.
Out
REAL
The calculated output of the PI algorithm. Math status flags are set for this output.
HighAlarm
BOOL
The maximum limit alarm indicator. Set when the calculated value for Out Greater than or equal to HighLimit and the output and integrator are clamped at HighLimit.
LowAlarm
BOOL
The minimum limit alarm indicator. Set when the calculated value for Out Less than or equal to LowLimit and output and integrator are clamped at LowLimit.
DeltaT
REAL
Elapsed time between updates. This is the elapsed time in seconds used by the control algorithm to calculate the process output.
Status
DINT
Status of the function block.
InstructFault (Status.0)
BOOL
The instruction detected one of the following execution errors. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
KpInv (Status.1)
BOOL
Kp < minimum or Kp > maximum.
WldInv (Status.2)
BOOL
Wld < minimum or Wld > maximum.
HighLowLimsInv (Status.3)
BOOL
HighLimit Less than or equal to LowLimit.
ShapeKpPlusInv (Status.4)
BOOL
ShapeKpPlus < minimum or ShapeKpPlus > maximum.
ShapeKpMinusInv (Status.5)
BOOL
ShapeKpMinus < minimum or ShapeKpMinus > maximum.
KpInRangeInv (Status.6)
BOOL
KpInRange < minimum or KpInRange > maximum.
ShapeWldPlusInv (Status.7)
BOOL
ShapeWldPlus < minimum or ShapeWldPlus > maximum.
ShapeWldMinusInv (Status.8)
BOOL
ShapeWldMinus < minimum or ShapeWldMinus > maximum.
WldInRangeInv (Status.9)
BOOL
WldInRange < minimum or WldInRange > maximum.
TimingModeInv (Status.27)
BOOL
Invalid TimingMode.
For more information about timing modes, see Function Block Attributes.
RTSMissed (Status.28)
BOOL
Only used in real time sampling mode. Set when
ABS | DeltaT - RTSTime | > 1 (.001 second).
RTSTimeInv (Status.29)
BOOL
Invalid RTSTime value.
RTSTimeStampInv (Status.30)
BOOL
Invalid RTSTimeStamp value.
DeltaT (Status.31)
BOOL
Invalid DeltaT value.
Description
The PI instruction uses the position form of the PI algorithm. This means the gain terms are applied directly to the input signal, rather than to the change in the input signal. The PI instruction is designed to execute in a task where the scan rate remains constant.
In the non-linear algorithm, the proportional and integral gains vary as the magnitude of the input signal changes. The PI instruction supports two non-linear gain modes: linear and parabolic. In the linear algorithm, the gains vary linearly as the magnitude of input changes. In the parabolic algorithm, the gains vary according to a parabolic curve as the magnitude of input changes.
The PI instruction calculates Out using this equation:
PI_fbd_eq
Whenever the value computed for the output is invalid, NAN, or Plus or Minus sign INF, the instruction sets Out = the invalid value and sets the math overflow status flag. The internal parameters are not updated. In each subsequent scan, the output is computed using the internal parameters from the last scan when the output was valid.
Operating in Linear Mode
In linear mode, the non-linear gain mode is disabled. The Kp and Wld values are the proportional and integral gains used by the instruction. The instruction calculates the value for Out using these equations:
Value
Equation
ITerm
PI_fbd_ITerm_eq
where DeltaT is in seconds
PTerm
Kp x In
Out
ITerm + PTerm
with these limits on Wld:
  • Low Limit > 0.0
  • High Limit = 0.7
    p
    /DeltaT
  • WldInput = In
Operating in Non-Linear Mode
In non-linear mode, the instruction uses the non-linear gain mode selected by ParabolicLinear to compute the actual proportional and integral gains.
The gains specified by Kp and Wld are multiplied by 1.0 when In = 0. Separate proportional and integral algorithms increase or decrease the proportional or integral gain as the magnitude of error changes. These algorithms use the input range and shaping gain parameters to compute the actual proportional and integral gains. Input range defines the range of In (i.e. error) over which the gain is shaped. Input ranges are set by the two KpInRange and WldInRange. Shaping gain defines the gain multiplier for the quadrant controlled by the shaping gain parameter. Shaping gains are set by ShapeKpPlus, ShapeKpMinus, ShapeWldPlus and ShapeWldMinus.
The ParabolicLinear input selects the non-linear gain mode. If ParabolicLinear is cleared, linear mode is selected. If ParabolicLinear is set, parabolic mode is selected.
To configure a particular shaping gain curve, enter a shaping gain 0.0-10.0 for integral shaping, a shaping gain 0.1-10.0 for proportional shaping, and the input range over which shaping is to be applied. Kp and Wld are multiplied by the calculated ShapeMultiplier to obtain the actual proportional and integral gains. Entering a shaping gain of 1.0 disables the non-linear algorithm that calculates the proportional or integral gain for the quadrant.
When the magnitude of In (error) is greater then InRange then the ShapeMultiplier equals the value computed when | In | was equal to InRange.
The following diagram illustrates the maximum and minimum gain curves that represent the parabolic and linear gain equations.
PI_fbd_GainCurves
The instruction calculates the value for Out using these equations:
Value
Equation
Kp shaping gain multiplier
PI_fbd_KPShapeGainMult_eq
Kp input ratio
PI_fbd_KPInputRatio_eq
Kp ratio
PI_fbd_KPRatio_eq
Kps shaping gain
PI_fbd_KPSShapingGain_eq
Proportional output
PI_fbd_PropOutput_eq
Wld shaping gain
PI_fbd_WLDShapingGain_eq
Wld input
PI_fbd_WLDInput_eq
Wld input ratio
PI_fbd_WLDInputRatio_eq
Wld ratio
PI_fbd_WLDRatio_eq
Wlds shaping gain
PI_fbd_WLDSShapingGain_eq
Wlds limits
PI_fbd_WLDSLimits_eq
Integral output
PI_fbd_IntegralOutput_eq
Output
PI_fbd_Output_eq
Limiting
The instruction stops the ITerm windup based on the state of the hold inputs.
Condition
Action
PI_fbd_Condition1
PI_fbd_Action1
PI_fbd_Condition2
PI_fbd_Action1
The instruction also stops integrator windup based on the HighLimit and LowLimit values.
Condition
Action
Integrator > HighLimit
Integrator = HighLimit
Integrator > LowLimit
Integrator = LowLimit
The instructions limits the value of Out based on the HighLimit and LowLimit values.
Condition
Action
HighLimit Less than or equal to LowLimit
Out = LowLimit
ITerm = LowLimit
HighLowLimsInv is set
HighAlarm is set
LowAlarm is set
WldInput = 0
Out Greater than or equal to HighLimit
Out = HighLimit
ITerm = ITerm
n-1
HighAlarm is set
ITerm > HighLimit
ITerm = HighLimit
Out Less than or equal to LowLimit
Out = LowLimit
ITerm = ITerm
n-1
LowAlarm is set
ITerm < LowLimit
ITerm = LowLimit
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition
Action Taken
Prescan
EnableIn and EnableOut are cleared to false.
Tag.EnableIn is false
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is true
EnableIn and EnableOut bit is set to true.
The instruction executes.
Instruction first run
Out n-1 = 0
The algorithm used to calculate Out will not be executed.
Instruction first scan
Out n-1 = 0
The algorithm used to calculate Out will not be executed.
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal Execution
See Tag.EnableIn is true in the Function Block table.
Postscan
See Postscan in the Function Block table.
Example
The PI instruction is a regulating instruction with proportional and integral gain components. The integral gain component is set by the user in radians/sec; this sets the basic frequency response of the PI regulator. The proportional gain sets the overall gain of the block, including the proportional AND integral gain of the block.
Excluding initialization and holding/clamping functionality, the following diagram shows the PI block’s basic regulating loop while in the linear mode.
PI Instruction: Linear Mode
PI Instruction Linear Mode_v31
The following example shows the PI instruction used as a velocity regulator. In this example, velocity error is created by subtracting the velocity feedback signal (see the PMUL instruction example) from the system’s velocity reference (through the SCRV instruction). Velocity error is driven directly into the PI instruction, which acts on this signal according to the function shown in the diagram above.
Function Block
PI_FBD_example_v31
Structured Text
Reference_Select.In1 := Master_Machine_Ref;
Reference_Select.Select1 := Master_Machine_Select;
Reference_Select.In2 := Section_Jog;
Reference_Select.Select2 := Jog_Select;
SSUM(Reference_Select);
S_Curve.In := Reference_Select.Out;
S_Curve.AccelRate := accel_rate;
S_Curve.DecelRate := accel_rate;
SCRV(S_Curve);
PMUL_01.In := Resolver_Feedback;
PMUL_01.WordSize := 12;
PMUL_01.Multiplier := 100000;
PMUL(PMUL_01);
Speed_Feedback := PMUL_01.Out;
Velocity_Error := S_Curve.Out - Speed_Feedback;
PI_01.In := Velocity_Error;
PI_01.Initialize := Enable_Regulator;
PI_01.Kp := Velocity_Proportional_Gain;
PI_01.Wld := Velocity_Integral_Gain;
PI(PI_01);
Torque_Reference := PI_01.Out;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal