Integrator (INTG)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
CompactLogix
5380,
ControlLogix
5580, and ControlLogix 5590 controllers.
The INTG instruction implements an integral operation. This instruction is designed to execute in a task where the scan rate remains constant.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram logic.
Function Block
RSL5K_INTG Function Block_v31
Structured Text
INTG(INTG_tag);
Operands
Function Block
Operand
Type
Format
Description
INTG tag
INTEGRATOR
Structure
INTG structure
INTEGRATOR Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set.
In
REAL
The analog signal input to the instruction.
Valid = any float
Default = 0.0
Initialize
BOOL
Request to initialize control algorithm. Output = InitialValue as long as Initialize is set.
Valid = any float
Default = 0.0
InitialValue
REAL
The initial value for instruction. Output = InitialValue as long as Initialize is set.
Valid = any float
Default = 0.0
IGain
REAL
The integral gain multiplier. If IGain < 0; the instruction sets IGain = 0.0, sets the appropriate bit in Status, and leaves the Output unchanged.
Valid = 0.0 to maximum positive float
Default = 0.0
HighLimit
REAL
The high limit value for Out. If HighLimit Less than or equal to LowLimit, the instruction sets HighAlarm and LowAlarm, sets the appropriate bit in Status, and sets Out = LowLimit.
Valid = any float
Default = maximum positive float
LowLimit
REAL
The low limit value for Out. If HighLimit Less than or equal to LowLimit, the instruction sets HighAlarm and LowAlarm, sets the appropriate bit in Status, and sets Out = LowLimit.
Valid = any float
Default = maximum negative float
HoldHigh
BOOL
Hold output high request. When set, Out is not allowed to increase in value.
Default is cleared.
HoldLow
BOOL
Hold output low request. When set, Out is not allowed to decrease in value.
Default is cleared.
TimingMode
DINT
Selects timing execution mode.
0 = Periodic mode
1 = Oversample mode
2 = Real time sampling mode
For more information about timing modes, see Function Block Attributes.
Valid = 0 to 2
Default = 0
OversampleDT
REAL
Execution time for oversample mode.
Valid = 0 to 4194.303 seconds
Default = 0
RTSTime
DINT
Module update period for real time sampling mode
Valid = 1 to 32,767ms
Default = 1
RTSTimeStamp
DINT
Module time stamp value for real time sampling mode.
Valid = 0 to 32,767ms
Default = 0
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled. Cleared to false if Out overflows.
Out
REAL
The calculated output of the algorithm.
HighAlarm
BOOL
High limit alarm indicator. When Out Greater than or equal to HighLimit, HighAlarm is set and the output is limited to the value of HighLimit.
LowAlarm
BOOL
Low limit alarm indicator. When Out Less than or equal to LowLimit, LowAlarm is set and the output is limited to the value of LowLimit.
DeltaT
REAL
Elapsed time between updates. This is the elapsed time in seconds used by the control algorithm to calculate the process output.
Status
DINT
Status of the function block.
InstructFault (Status.0)
BOOL
The instruction detected one of the following execution errors. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
IGainInv (Status.1)
BOOL
IGain > maximum or IGain < minimum.
HighLowLimsInv (Status.2)
BOOL
HighLimit Less than or equal to LowLimit.
TimingModeInv (Status.27)
BOOL
Invalid TimingMode value.
For more information about timing modes, see Function Block Attributes.
RTSMissed (Status.28)
BOOL
Only used in real time sampling mode. Set when
ABS | DeltaT - RTSTime | > 1 (.001 second).
RTSTimeInv (Status.29)
BOOL
Invalid RTSTime value.
RTSTimeStampInv (Status.30)
BOOL
Invalid RTSTimeStamp value.
DeltaTInv (Status.31)
BOOL
Invalid DeltaT value.
Structured Text
Operand
Type
Format
Description
INTG tag
INTEGRATOR
Structure
INTG structure
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
The INTG instruction is designed to execute in a task where the scan rate remains constant.
The INTG instruction executes this control algorithm when Initialize is cleared and DeltaT > 0.
INTG Description
Whenever the value computed for the output is invalid, NAN, or Plus or Minus sign INF, the instruction sets Out = the invalid value. The internal parameters are not updated. In each subsequent scan, the output is computed using the internal parameters from the last scan when the output was valid.
Limiting
The INTG instruction performs windup limiting to stop Out from changing based on the state of the HoldHigh and HoldLow inputs. If HoldHigh is set and Out > Out
n-1
, then Out = Out
n-1
. If HoldLow is set and Out < Out
n-1
, then Out = Out
n-1
.
The INTG instruction also performs output limiting using HighLimit and LowLimit. If Out ≥ HighLimit, the Out = HighLimit and HighAlarm is set. If Out ≤ LowLimit, then Out = LowLimit and LowAlarm is set.
Affects Math Status Flags
No
Major/Minor Faults
Minor fault occurs when
Fault type
Fault code
Feature is enabled and overflow is detected.
4
4
See Common Attributes for operand-related faults.
Execution
NOTE: In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic, it will execute. For more details including definitions and general behavior for all Function Block instructions, refer to Publication 1756-RM006G-EN-P, Advanced Process Control and Drives Instructions.
Condition/State
Action Taken
Prescan
No action taken.
Postscan
No action taken.
Conditions that occur only during Normal Scan mode
Condition/State
Action Taken
Instruction first run
The internal parameters and Out are set to 0. The primary algorithm is not executed but will validate input parameters.
Instruction first scan
The internal parameters and Out are set to 0. The primary algorithm is not executed but will validate input parameters.
EnableIn is false
.EnableOut bit is cleared to false.
EnableIn is true
.EnableOut bit is set to true.
The instruction’s main algorithm will be executed and outputs will be updated.
Examples
In many applications an integral gain component is included in the closed loop regulator design in order to eliminate or minimize error in the system being regulated. A straight proportional-only regulator will not tend to drive error in the system to zero. A regulator that uses proportional and integral gain, however, tends to drive the error signal to zero over a period of time. The INTG instruction uses the following equation to calculate its output.
INTG Description
In the chart below, the input to the block moves from 0 to +200 units. During this period, the output of the block integrates to 2800 units. As In changes from +200 units to 0 units, Out maintains at 2800 units. When In transitions from 0 to -300 units, Out slowly integrates down to -1400 units until In transitions back to 0. Finally, as In moves from 0 to +100, Out integrates back to 0 where In is set to 0 coincidentally with Out reaching 0.
This characteristic of the integrator - continually driving in a specific direction while any input to the function is present or holding at any level during the point where the input is at zero - is what causes a regulator using integral gain to drive toward zero error over a period of time.
INTG Graph
The following example shows how the INTG instruction can be used. In many instances, the HighLimit and LowLimit inputs limit the total percentage of control that the integral gain element might have as a function of the regulator’s total output. The HoldHigh and HoldLow inputs, on the other hand, can be used to prevent the output from moving further in either the positive or negative direction. The HoldHigh and HoldLow inputs prevent the INTG instruction from "winding-up" in a direction which is already beyond the limits of the controlled variable.
Function Block
This example is the minimal legal programming of the INTG function block and is only used to show the neutral text and generated code for this instruction. This is for internal purposes only and is not a testable case.
RSL5K_INTG Function Block example_v31
Structured Text
INTG_01.In := Input_Value;
INTG_01.Initialize := Initialize_flag;
INTG_01.InitialValue := Int_Init_Val;
INTG_01.IGain := I_Gain;
INTG_01.HighLimit := Int_saturate_high;
INTG_01.LowLimit := Int_saturate_low;
INTG_01.HoldHigh :=HAlarm_Status;
INTG_01.HoldLow := LAlarm_Status;
INTG(INTG_01);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal