COORDINATE_SYSTEM Structure

Listed below are attributes of a coordinate system.
How to Access Attributes
The following table describes how to access attributes. The Access column shows how to access the attribute. The Description column explains the access method that is used.
Example
Attribute
Axis Type
Data Type
Access
Description
Actual Position Tolerance
GSV
Use a Get System Value (GSV) instruction to get the value.
SSV
Config Fault
Tag
Use the tag for the axis to get the value.
Coordinate Motion Status
Tag
Use the tag for the axis to get the value.
Coordinate System Attributes
This table describes each attribute of an axis.
Attribute
Data Type
Access
Description
Accel Status
BOOL
Tag
Use the Accel Status bit to determine if the coordinated (vectored) motion is currently being commanded to accelerate.
The acceleration bit is set when a coordinated move is in the accelerating phase due to the current coordinated move. It is cleared when the coordinated move has been stopped or the coordinated move is in the decelerating phase.
Active Tool Frame ID
DINT
GSV
Tag
Active Tool identifier specified by the user in the MCTO instruction.
Active Tool Frame Offset
DINT
GSV
Value of the active tool offset being used in the MCTO instruction.
First three entries are coordination units. Second three entries are degrees.
Actual Pos Tolerance
BOOL
Tag
Use the Actual Pos Tolerance Status bit to determine when a coordinate move is within the Actual Position Tolerance.
The Actual Position Tolerance Status bit is set for AT term type only. The bit is set when interpolation is complete and the actual distance to programmed endpoint is less than the configured AT value.
The bit remains set after an instruction completes. The bit is reset if either a new instruction is started or the axis moves such that the actual distance to programmed endpoint is greater than the configured AT value.
Actual Position
REAL[8]
Tag
Array of actual position of each axis associated to this motion coordinate system in Coordinate Units.
Actual Position Tolerance
REAL
GSV SSV
Coordination Units
The Actual Position Tolerance attribute value is a distance unit used when instructions such as MCLM, MCCM and so on specify a Termination Type of Actual Position.
Actual Position Tolerance Status
BOOL
Tag
The Actual Position Tolerance Status bit attribute can be used to determine when a coordinate move is within the Actual Position Tolerance.
Axes Configuration Faulted
DINT
Tag
Shows which axes in this coordinate system have a configuration fault.
If this bit is on
Then this axis has a configuration fault
0
0
1
1
2
2
Axes Inhibited Status
DINT
Tag
Shows which axes in this coordinate system are inhibited.
If this bit is on
Then this axis is inhibited
0
0
1
1
2
2
Axes Servo On Status
DINT
Tag
Shows which axes in this coordinate system are on (via MSO).
If this bit is on
Then this axis is on
0
0
1
1
2
2
Axes Shutdown Status
DINT
Tag
Shows which axes in this coordinate system are shutdown.
If this bit is on
Then this axis is shutdown
0
0
1
1
2
2
Axis Fault
DINT
Tag
The Axis Fault Bits attribute is a roll-up of all of the axes associated to this motion coordinate system. A bit being set indicates that one of the associated axes has that fault.
Type
Bit
Physical Axis Fault
0
Module Fault
1
Config Fault
2
Group Fault
3
Axis Inhibit Status
BOOL
Tag
If this bit is the following.
ON - An axis in the coordinate system is inhibited.
OFF - None of the axis in the coordinate system are inhibited.
Command Pos Tolerance Status
BOOL
Tag
Use the Command Position Tolerance Status bit to determine when a coordinate move is within the Command Position Tolerance.
The Command Position Tolerance Status bit is set for all term types whenever the distance to programmed endpoint is less than the configured CT value. The bit remains set after an instruction completes. The bit is reset when a new instruction is started.
Command Position Tolerance
REAL
GSV SSV
Coordination Units
The Command Position Tolerance attribute value is a distance unit used when instructions such as MCLM, MCCM and so on specify a Termination Type of Command Position.
Config Fault
BOOL
Tag
The Configuration Fault bit is set when an update operation targeting an axis configuration attribute of an associated motion module has failed. Specific information concerning the Configuration Fault may be found in the Attribute Error Code and Attribute Error ID attributes associated with the motion module.
CoordinateSystemLockStatus
BOOL
Tag
The CoordinateSystemLockStatus is set when linear (MCLM) or circular (MCCM) move is position locked whereby the master axis has moved past the lock position in the specified lock direction.
Coordinated Motion Status
DINT
Tag
Lets you access the motion status bits for the coordinate system in one 32-bit word.
Status
Bit
Accel Status
0
Decel Status
1
Actual Pos Tolerance Status
2
Command Pos Tolerance Status
3
Stopping Status
4
Reserved
5
Move Status
6
Move Transition Status
7
Move Pending Status
8
Move Pending Queue Full Status
9
Reserved
10
Reserved
11
Tool Change Allowed Status
12
Transform Source
13
Transform Target
14
CoordinateSystemLockStatus
15
Coordinated System Auto Tag Update
SINT
GSV SSV
The Coordinate System Auto Tag Update attribute configures whether the Actual Position attribute is automatically updated each motion task scan. This is similar to, but separate from the Motion Group’s "Auto Tag Update" attribute.
0 - auto update disabled
1 - auto update enabled (default)
Coordinated System Status
DINT
Tag
Lets you access the status bits for the coordinate system in one 32-bit word.
Status
Bit
Shutdown Status
0
Ready Status
1
Motion Status
2
Axis Inhibit Status
3
Decel Status
BOOL
Tag
Use the Decel Status bit to determine if the coordinated (vectored) motion is currently being commanded to decelerate.
The deceleration bit is set when a coordinated move is in the decelerating phase due to the current coordinated move. It is cleared when the coordinated move has been stopped or the coordinated move is complete.
Dynamics Configuration Bits
DINT
GSV SSV
Revision 16 improved how the controller handles changes to an S-curve profile.
Do you want to return to revision 15 or earlier behavior for S-curves?
NO - Leave these bits ON (default).
YES - Turn OFF one or more of these bits.
To turn off this change
Turn off this bit
Reduced S-curve Stop Delay
This change applies to the Motion Coordinated Stop (MCS) instruction. It lets you use a higher deceleration jerk to stop an accelerating coordinate system more quickly.
The controller uses the deceleration jerk of the stopping instruction if it is more than the current acceleration jerk.
0
Reduced S-curve Velocity Reversals
Before revision 16, you could cause a coordinate system to momentarily reverse direction if you decreased the deceleration jerk while the coordinate system was decelerating. This typically happened if you tried to restart a move with a lower deceleration rate while the coordinate system was stopping. This change prevents the coordinate system from reversing in those situations.
1
Reduced S-curve Velocity Overshoots
You can cause a coordinate system to overshoot its programmed speed if you decrease the acceleration jerk while the coordinate.
2
Group Fault
BOOL
Tag
The Group Fault bit attribute is set when one or more faults have occurred related to the motion group associated with the selected axis. The specific fault conditions can then be determined through access to the Group Fault attribute of the associated motion group. Usually, a group fault affects all axes associated with the motion group. A group fault generally results in the shutdown of all associated axes. Reconfiguration of the entire motion subsystem is required to recover from a group fault condition.
Maximum Acceleration
REAL
GSV SSV
Coordination Units / Sec2
The Maximum Acceleration attribute value is used by motion instructions such as MCLM, MCCM and so on, to determine the acceleration rate to apply to the coordinate system vector when the acceleration is specified as a percent of the Maximum.
Maximum Deceleration
REAL
GSV SSV
Coordination Units / Sec2
The Maximum Deceleration attribute value is used by motion instructions such as MCLM, MCCM and so on, to determine the deceleration rate to apply to the coordinate system vector when the deceleration is specified as a percent of the Maximum.
Maximum Pending Moves
DINT
GSV
The Maximum Pending Moves attribute is used to determine how many Move Pending queue slots should be created as part of the Coordinate System’s create service.
Limited to a queue of one.
Maximum Speed
REAL
GSV SSV
Coordination Units / Sec
The value of the Maximum Speed attribute is used by various motion instructions (for example, MCLM, MCCM and so on) to determine the steady-state speed of the coordinate system vector when the speed is specified as a percent of the Maximum.
Module Fault
BOOL
Tag
The Module Fault bit attribute is set when a serious fault has occurred with the motion module associated with the selected axis. Usually a module fault affects all axes associated with the motion module. A module fault generally results in the shutdown of all associated axes. Reconfiguration of the motion module is required to recover from a module fault condition.
Modules Faulted
DINT
Tag
Shows which axes in this coordinate system have a module fault.
If this bit is on
Then this axis has a module fault
0
0
1
1
2
2
Motion Status
BOOL
Tag
The Motion Status bit attribute is set indicating that at least one Coordinate Motion instruction is active and the Coordinate System is connected to its associated axes.
Move Pending Queue Full Status
BOOL
Tag
The move pending queue full bit is set there is no room in the instruction queue for the next coordinated move instruction. Once there is room in the queue, the bit is cleared.
Move Pending Status
BOOL
Tag
The move pending bit is set once a coordinated motion instruction is queued. Once the instruction has begun executing, the bit will be cleared, provided no subsequent coordinated motion instructions have been queued in the mean time. In the case of a single coordinated motion instruction, the status bit may not be detected by the user in the Logix Designer application since the transition from queued to executing is faster than the coarse update. The real value of the bit comes in the case of multiple instructions. As long as an instruction is in the instruction queue, the pending bit will be set. This provides the Logix Designer application programmer a means of stream-lining the execution of multiple coordinated motion instructions. Ladder logic containing coordinated motion instructions can be made to execute faster when the programmer allows instructions to be queued while a preceding instruction is executing. When the MovePendingStatus bit is clear, the next coordinated motion instruction can be executed (that is, setup in the queue).
Move Status
BOOL
Tag
The move bit is set when coordinated motion is generating motion for any associated axes. Once coordinated motion is no longer being commanded, the move bit is cleared.
Move Transition Status
BOOL
Tag
The move transition bit is set once the blend point between two successive coordinated moves has been reach. The bit remains set while the blend of the two moves into one is in process. Once the blend is complete, the move transition bit is cleared.
Physical Axes Faulted
DINT
Tag
Shows which axes in this coordinate system have a servo axis fault.
If this bit is on
Then this axis has a servo axis fault
0
0
1
1
2
2
Physical Axis Fault
BOOL
Tag
If the Physical Axis Fault bit is set, it indicates that there is one or more fault conditions have been reported by the physical axis. The specific fault conditions can then be determined through access to the fault attributes of the associated physical axis.
Ready Status
BOOL
Tag
The Ready bit is set when all associated axes are enabled. It is cleared after an MCSD, MGSD or a fault on any of the associated axes.
Robot Configuration
DWORD
GSV
Tag
The robot configuration parameter will reflect the current pose of the Robot in space. It will be represented by one or more of these parameters depending on the geometry:
  1. Lefty/Righty
  2. Above/Below
  3. Flip/No-Flip
Bit Field:
0: Change(1) / Same(0)
1:Lefty(1) / Righty(0)
2:Above(1) / Below(0)
3: Flip(1) / No Flip(0)
4: Transforms Not Active(1) / Transforms Active(0)
This attribute only applies to the Robot coordinate system.
Shutdown Status
BOOL
Tag
The Coordinate System bit will be set after an MCSD or MGSD is executed and all associated axes have stopped. A MCSR or a MGSR will reset the coordinate system and clear the bit. Coordinated moves cannot be initiated while this bit is set.
Stopping Status
BOOL
Tag
The stopping bit is set when a MCS instruction is executed. The bit will remain set until all coordinated motion is stopped. The bit is cleared when all coordinated motion has stopped.
Tool Change Allowed Status
BOOL
Tag
The Tool Change Allowed Status bit attribute is set to indicate when the user is allowed to change a tool via a transform instruction.
Transform Source Status
BOOL
Tag
If the bit is the following.
ON - The coordinate system is the source of an active transform.
OFF - The coordinate system isn’t the source of an active transform.
Transform Target Status
BOOL
Tag
If the bit is the following.
ON - The coordinate system is the target of an active transform.
OFF - The coordinate system isn’t the target of an active transform.
Turns Counters
INT[4]
GSV
Tag
A counter indicating the number of times the 180 degree point has been crossed in the +/- direction for the axis when turned. Three integers specifying the turns counts for J1, J4 and J6 axis.
Turns counters range is +/-127 value.
Default 128 value is selected as initial values value when Transforms are not active on the coordinate system.
1 – Turns counters on J1 axis
2 – Turns counters on J4 axis
3 – Turns counters on J6 axis
4 – Reserved for future use
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal