Negate (NEG)

This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers. Controller differences are noted where applicable.
When enabled, the NEG instruction and operator subtract the Source value from zero.
Available Languages
Ladder Diagram
NEG_LD_avail_v31
Function Block Diagram
Function Block Diagram supports these elements:
FBD Block
NEG_FBD_avail_v31
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
NEG FBD Function
Structured Text
This instruction is not available in structured text.
TIP: Use operator '-' in an expression to compute the same result. Refer to Structured Text Syntax for more information on the syntax of expressions and assignments within structured text.
Operands
IMPORTANT: Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data Conversions.
Ladder Diagram
Operand
Data Type
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Data Type
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Format
Description
Source
SINT
INT
DINT
REAL
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
immediate
tag
Value to negate
Dest
SINT
INT
DINT
REAL
SINT
INT
DINT
LINT
USINT
UINT
UDINT
ULINT
REAL
LREAL
tag
Tag to store result of the instruction.
Function Block Diagram
FBD Block
Operand
Data Type
Format
Description
NEG
FBD_MATH_ADVANCED
tag
NEG structure
FBD_MATH_ADVANCED Structure
Input Members
Data Type
Description
EnableIn
BOOL
Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true.
Source
REAL
Value to negate.
Output Members
Data Type
Description
EnableOut
BOOL
Indicates if the instruction executed without fault when it was enabled.
Dest
REAL
Result of the instruction
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
Input Operand (Left Pin)
Data Type
Description
Source
SINT
USINT
INT
UINT
DINT
UDINT
LINT
ULINT
REAL
LREAL
Value to negate.
Output Operand (Right Pin)
Data Type
Description
Dest
DINT
UDINT
LINT
ULINT
REAL
LREAL
Result of the function.
Affects Math Status Flags
Controllers
Affects Math Status Flags
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers
Conditional
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers
Yes
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-in is false
Set Rung-condition-out to Rung-condition-in.
Rung-condition-in is true
Set Rung-condition-out to Rung-condition-in.
Dest = 0 - Source.
Postscan
N/A
Function Block Diagram
FBD Block
Condition/State
Action Taken
Prescan
N/A
EnableIn is false
Set EnableOut to EnableIn.
EnableIn is true
Dest = 0 - Source.
If overflow occurs
Clear EnableOut to false
else
Set EnableOut to true
Instruction first run
N/A
Instruction first scan
N/A
Postscan
N/A
FBD Function
TIP: FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
Condition/State
Action Taken
Prescan
N/A
Normal Scan
Dest = 0 - Source.
Instruction first run
N/A
Instruction first scan
N/A
Postscan
N/A
Examples
Ladder Diagram
NEG_LD_ex_v31
Function Block Diagram
FBD Block
NEG_FBD_ex_v31
FBD Function
NEG_FBD Function_v32
Structured Text
DINT_dest := -DINT_src;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal