Modulo (MOD)
This information applies to the CompactLogix 5370, ControlLogix 5570, Compact GuardLogix
5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580,
GuardLogix 5580, and ControlLogix 5590 controllers. Controller differences are noted where
applicable.
When enabled, the MOD instruction and the operator divides Source A by Source B and places the remainder in Dest. This is done using the algorithm:
Dest = Source A – (truncate ( Source A / Source B) * Source B)
Available Languages
Ladder Diagram

Function Block Diagram
Function Block Diagram supports these elements:
FBD Block

FBD Function
TIP:
FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.

Structured Text
This instruction is not available in structured text.
TIP:
Use MOD as an operator in an expression to compute the same result. Refer to
Structured Text Syntax for more information on the syntax of
expressions and assignments within structured text.
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data Conversions.
Ladder Diagram
These are the operands for Ladder Diagram.
Operand | Data Type CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Data Type CompactLogix 5380, ControlLogix 5580, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers | Format | Description |
---|---|---|---|---|
Source A | SINT INT DINT REAL | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value of the dividend. |
Source B | SINT INT DINT REAL | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value of the divisor. |
Dest | SINT INT DINT REAL | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | tag | Tag to store result of the instruction. |
Function Block Diagram
FBD Block
Operand | Data Type | Format | Description |
---|---|---|---|
MOD | FBD_MATH | tag | MOD structure |
FBD_MATH Structure
Input Members | Data Type | Description |
---|---|---|
EnableIn | BOOL | Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true. |
SourceA | REAL | Value of the dividend. |
SourceB | REAL | Value of the divisor. |
Output Members | Data Type | Description |
---|---|---|
EnableOut | BOOL | Indicates if the instruction executed without fault when it was enabled. |
Dest | REAL | Result of the instruction. |
FBD Function
TIP:
FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
Input Operands (Left Pins) | Data Type CompactLogix 5380, ControlLogix 5580, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only | Description |
---|---|---|
SourceA (top) | SINT USINT INT UINT DINT UDINT LINT ULINT REAL LREAL | Value of the dividend. |
SourceB (bottom) | SINT USINT INT UINT DINT UDINT LINT ULINT REAL LREAL | Value of the divisor |
Output Operand (Right Pin) | Data Type CompactLogix 5380, ControlLogix 5580, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only | Description |
---|---|---|
Dest | DINT UDINT LINT ULINT REAL LREAL | Result of the function. |
See FBD Functions.
Affects Math Status Flags
Controllers | Affects Math Status Flags |
---|---|
CompactLogix 5380, ControlLogix 5580, Compact GuardLogix 5380, GuardLogix 5580,
and ControlLogix 5590 controllers | Conditional |
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes |
See Math Status Flags.
Major/Minor Faults
A minor fault will occur if: | Fault Type | Fault Code |
---|---|---|
Source B = 0 | 4 | 4 |
See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | N/A |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in |
Rung-condition-in is true | Set Rung-condition-out to Rung-condition-in Dest is set (to the remainder) as described in the Description section. |
Postscan | N/A |
Function Block Diagram
FBD Block
Condition/State | Action Taken |
---|---|
Prescan | N/A |
EnableIn is false | Set EnableOut to EnableIn |
EnableIn is true | Dest is set (to the remainder) as described in the Description section. If an overflow occurs Clear EnableOut to false else Set EnableOut to true |
Instruction first run | N/A |
Instruction first scan | N/A |
Postscan | N/A |
FBD Function
TIP:
FBD Function is applicable to CompactLogix 5380, ControlLogix 5580, Compact
GuardLogix 5380, GuardLogix 5580, and ControlLogix 5590 controllers only.
Condition/State | Action Taken |
---|---|
Prescan | N/A |
Normal Scan | Dest is set (to the remainder) as described in the Description section. |
Instruction first run | N/A |
Instruction first scan | N/A |
Postscan | N/A |
TIP:
If Source B is 0, the result is 0 and a minor fault is generated.
Examples
Ladder Diagram

Divide dividend by divisor and place the remainder in remainder. In this example, 3 goes into 10, three times, with a remainder of 1.
Function Block Diagram
FBD Block

FBD Function

Structured Text
remainder := dividend MOD divisor;
Provide Feedback