Proving Operational Sequences

Proving tests are performed when enabling or disabling the drive axis. During these state transitions a series of operations are performed by the drive to ensure the proper function of the motor (Torque Proving) and the brake (Brake Proving).
The following flow charts define these operational sequences in the context of a drive enable transition and a drive disable or abort transition.
Drive Enable Sequence with Proving Tests
Drive Disable Sequence with Proving Test
Drive Disable Sequence with Proving
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal