Motion Database Storage Attributes
The following are the Motion Database Storage attributes associated with a Motion Control
Axis.
System Acceleration Base
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - C | Set | REAL | 0 DB | 0 | ![]() | Motor Units/sec 2 @ 100 % Rated |
This floating point value represents the acceleration of the selected unloaded motor based
on 100% Rated current and used to compute System Inertia. This attribute is used to store
the original System Acceleration value for subsequent upload.
Drive Model Time Constant Base
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - C | Set | REAL | .0015 DB | 0 | ![]() | Sec |
This floating point value represents the lumped model time constant associated with the
drive device for the purposes of computing loop gains. This attribute is used to store the
original Drive Model Time Constant value for subsequent upload. The Drive Model Time
Constant Base (DMTC_Base) is computed based on the current loop bandwidth, the velocity loop
update time and the feedback sample period according to the following formula:
DMTC_Base = 2 * 1/(2*PI*Current Loop Bandwidth(Hz)) + Velocity Loop Update Period +
Feedback Sample Period/2
Drive Rated Peak Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | Amps |
This floating point value represents the peak current rating associated with the drive
device and used to compute peak torque and acceleration limits. This attribute is used to
store the original Drive Rated Peak Current value for subsequent upload.
Bus Overvoltage Operational Limit
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Optional - C (PM) | Set | REAL | 0 DB | 0 | ![]() | Volts |
This floating point value represents the maximum DC Bus voltage level that can be sustained
during drive operation, which is used to calculate the factory default value for PM Motor
Rotary Bus Overvoltage Speed or the PM Motor Linear Bus Overvoltage Speed associated with PM
motor types. This attribute is used to store the Bus Overvoltage Operational Limit value
used in this calculation for subsequent upload.
Converter Model Time Constant Base
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0.001 DB | 0 | ![]() | Seconds |
This floating point value represents the lumped model time constant associated with the
regenerative converter device for the purposes of computing loop gains. This attribute is
used to store the original Converter Model Time Constant value for subsequent upload. The
Converter Model Time Constant Base is computed based on the converter current loop
bandwidth, the bus voltage loop update time and the bus voltage feedback sample period
according to the following formula:
CMTC_Base = 2 * 1/(2*PI*Current Loop Bandwidth(Hz)) + Bus Voltage Loop Update Period
Converter Current Loop Bandwidth Base
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0 DB | 0 | ![]() | Hz |
This floating point value represents the default bandwidth for the active and reactive
current loops for the regenerative converter. This attribute is used to store the original
default Converter Current Loop Bandwidth value that was used to compute the Converter Model
Time Constant that is the basis for tuning the converter.
Converter Rated Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0 DB | 0 | ![]() | Amps |
This floating point value represents the continuous output current rating associated with
the regenerative converter and used to compute the System Capacitance scaling attribute
value from the Total Capacitance of the DC Bus. This attribute is used to store the original
Converter Rated Current value for subsequent upload.
Converter Rated Peak Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0 DB | 0 | ![]() | Amps |
This floating point value represents the peak output current rating associated with the
regenerative converter and used together with the Converter Rated Current to compute the
default Converter Current Vector Limit attribute value. This attribute is used to store the
original Converter Rated Peak Current value for subsequent upload.
Converter Rated Voltage
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0 DB | 0 | ![]() | Volts (RMS) |
This floating point value represents the input voltage rating associated with the
regenerative converter and used to compute the Bus Voltage Set Point attribute value. This
attribute is used to store the original Converter Rated Voltage value for subsequent
upload.
Converter DC Bus Capacitance
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0 DB | 0 | ![]() | ![]() |
This floating point value represents the internal bus capacitance of the regenerative
converter and is used to compute the System Capacitance scaling attribute. This attribute is
used to store the original Converter DC Bus Capacitance value for subsequent upload.
Converter Rated Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - G | Set | REAL | 0 DB | 0 | ![]() | kVA |
This floating point value represents the power rating of the converter. This attribute is
used to estimate the default AC Line Source Power value.
Current Loop Bandwidth
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - C | Set | REAL | 0 DB | 0 | ![]() | Hz |
This floating point value represents the bandwidth of the current loop that is used to set
the factory default value for of the Torque Loop Bandwidth and the Flux Loop Bandwidth. This
attribute is used to store the Current Loop Bandwidth value for subsequent upload.
Current Loop Bandwidth Scaling Factor
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - C | Set | REAL | 0 DB | 0 | ![]() |
This floating point value represents the scaling factor, based on motor type, which is used
to set the factory default value for of the Torque Loop Bandwidth and the Flux Loop
Bandwidth. This attribute is used to store the original Current Loop Bandwidth Scaling
Factor value for subsequent upload.
Drive Rated Voltage
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | V rms |
This floating point value represents the RMS voltage rating of the drive that is used to
set the factory default value for the Break Voltage associated with V/Hz drives. This
attribute is used to store the original Drive Rated Voltage value for subsequent upload.
Max Output Frequency
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | Hz |
This floating point value represents the maximum frequency rating of the drive that is used
to set the factory default values for Velocity Limits. This attribute is used to store the
original Max Output Frequency value for subsequent upload.
Inverter Type
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | USINT | 0 DB | 0 | 3 | Enumeration: 0 = Voltage Source PWM Output 1 = Voltage Source Sine Output 2 = Current Source PWM Output 3 = Current Source Sine Output 4 - 255 = reserved |
This enumerated value indicates the inverter type.
Motor Rated Output Power Sine
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - C | Set | REAL | 0 DB | 0 | ![]() | Power Units |
Reference attribute 1321, Motor Rated Output Power.
This is one of two possible values that may be copied to attribute 1321, Motor Rated Output
Power.
When this attribute value exceeds the attribute 1254 value, then the motor has been
characterized for operation with a Voltage Source Sine Output inverter. When this attribute
value equals the attribute 1254 value, then the motor has not been characterized for
operation with a Voltage Source Sine Output inverter.
If the Inverter Type = Voltage Source Sine Output and the motor has been characterized for
operation with a Voltage Source Sine Output inverter, then this attribute value is copied to
attribute 1321.
Motor Rated Output Power PWM
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - C | Set | REAL | 0 DB | 0 | ![]() | Power Units |
Reference attribute 1253, Motor Rated Output Power Sine.
If the Inverter Type != Voltage Source Sine Output or the motor has not been characterized
for operation with a Voltage Source Sine Output inverter, then this attribute value is
copied to attribute 1321, Motor Rated Output Power.
Rotary Motor Rated Speed Sine
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | RPM |
Reference attribute 1253, Motor Rated Output Power Sine.
If the Inverter Type = Voltage Source Sine Output and the motor has been characterized for
operation with a Voltage Source Sine Output inverter, then this attribute value is copied to
attribute 1331, Rotary Motor Rated Speed.
Rotary Motor Rated Speed PWM
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | RPM |
Reference attribute 1253, Motor Rated Output Power Sine.
If the Inverter Type != Voltage Source Sine Output or the motor has not been characterized
for operation with a Voltage Source Sine Output inverter, then this attribute value is
copied to attribute 1331, Rotary Motor Rated Speed.
Linear Motor Rated Speed Sine
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | m/s |
Reference attribute 1253, Motor Rated Output Power Sine.
If the Inverter Type = Voltage Source Sine Output and the motor has been characterized for
operation with a Voltage Source Sine Output inverter, then this attribute value is copied to
attribute 1335, Linear Motor Rated Speed.
Linear Motor Rated Speed PWM
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - D | Set | REAL | 0 DB | 0 | ![]() | m/s |
Reference attribute 1253, Motor Rated Output Power Sine.
If the Inverter Type != Voltage Source Sine Output or the motor has not been characterized
for operation with a Voltage Source Sine Output inverter, then this attribute value is
copied to attribute 1335, Linear Motor Rated Speed.
Provide Feedback