Motion Control Interface Attributes
The Motion Control Interface attributes are used by the
Logix Designer
application to support the interface to an axis. Interface attributes are used to customize what choices appear on the properties pages and help you structure a motion axis.
TIP:
Remember that the attributes that appear in the
Logix Designer
application are dependent on the current Control
Mode.Axis Address
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get | DINT | - | - | - | Absolute Address when the attribute is supported. Zero (0) when the attribute is deprecated. |
Absolute Address of Motion Control Axis Object data structure. The Axis Address attribute
is used to return the actual physical address in memory where the axis instance is located.
Newer controllers return a value of 0 (zero) for this attribute. The Axis Instance attribute
should be used instead of the Axis Address.
Axis Instance
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get/
GSV | DINT | - | - | - | Instance Number |
Instance Number assigned to this instance of the Motion Control Axis Object. The Axis Instance attribute is used to return the instance number of an axis. An example of using this attribute is responding to an axis major fault. Major fault records contain the axis instance of the offending axis. Use this attribute to query an axis instance and determine if the instance number matches the fault record.
The Axis Instance attribute is required when accessing an attribute using a MSG instruction.
Group Instance
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get/
GSV | DINT | - | - | - | Instance Number |
Instance Number of the Motion Group or Motion Control Group assigned to this instance of the Motion Control Axis Object. Use the Group Instance attribute to determine what motion group this axis is assigned to.
Map Instance
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | DINT | - | - | - | Instance Number |
I/O Map Instance Number assigned to this instance of the Motion Control Axis Object. The Map Instance attribute associates an axis to a specific motion compatible module by specifying the I/O map entry representing the module. This value is set to 0 for virtual and consumed data types.
Module Channel
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | USINT | 255 | - | - | Channel Number (0, 1, 2, …)
A value of 255 indicates the axis is unassigned. |
Channel number of the module assigned to this instance of the Motion Control Axis Object. The Module Channel attribute associates an axis to a specific channel on a motion compatible module by specifying the Module Channel attribute.
Module Class Code
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | DINT | - | - | - | Object Class Code |
Object class code of the motion engine in the module. The Module Class Code attribute is the class code of the object in the motion module which is supporting motion; for example 0xAF is the object ID of the Servo Module Axis residing in the 1756-M02AE module.
C2C Map Instance
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | DINT | - | - | - | Producer/Consumed axis's associated C2C map instance |
Producer/Consumed axis's associated C2C map instance. When the Axis Data Type attribute is specified to be 'Consumed' then this axis is associated to the consumed data by specifying both the C2C Map Instance and the C2C Connection Instance. For all other Axis Data Types if this axis is to be produced then this attribute is set to 1 (one) to indicate that the connection is off of the local controller's map instance.
C2C Connection Instance
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | DINT | - | - | - | Producer/Consumed axis's associated C2C connection in reference to the C2C
map instance |
Producer/Consumed axis's associated C2C connection in reference to the C2C map instance. If this axis is to be produced, then this attribute is set to the connection instance under the local controller's map instance (1) that will be used to send the remote axis data through the C2C connection.
Memory Use
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get/
GSV | UINT | - | - | - | 105 (0x69) = I/O space 106 (0x6a) = Data Table space |
Controller memory space where this instance of the Motion Control Axis Object exists. This attribute is initialized as part of the create service when you create the axis.
The
Logix Designer
programming application uses this attribute to create axis instances in I/O memory for axes that are either to be produced or consumed.The Memory Use attribute can only be set as part of an axis create service and is used to control which controller memory the object instance is created in.
Memory Usage
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get | DINT | - | - | - | Bytes |
Amount of memory consumed for this instance of the Motion Control Axis Object. The Memory Use attribute can be used to determine the amount of memory the created instance consumes in bytes.
Axis Data Type
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get | USINT | - | - | - | Enumeration: 0 = Feedback 1 = Consumed 2 = Virtual 3 = Generic 4 = Servo 5 = Servo Drive 6 = Generic Drive 7 = CIP Drive |
Associated tag data type for this instance of the Motion Control Axis Object. This attribute is initialized as part of the create service when you create the axis.
The Axis Data Type attribute and is used to determine which data template, memory format, and set of attributes are created and applicable for this axis instance. This attribute can only be set as part of an axis create service.
Axis Configuration State
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get/
GSV | USINT | - | - | - | Enumeration 0 = Axis Instance Created 1 = Connection Created 126 = Axis Inhibited 128 = Axis Configured |
State of the configuration state machine for this instance of the Motion Control Axis Object. The Axis Configuration State attribute is used for troubleshooting purposes to indicate where in the axis configuration state-machine this axis presently is. Even consumed and virtual axes will utilize this attribute. This attribute is valid for all physical and non-physical data types.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Axis Configuration State semantics of values.
Semantics of Values | Axis Test Mode Support (Test Mode Configuration) |
---|---|
Enumeration 0 = Axis Instance Created 1 = Connection Created 126 = Axis Inhibited 128 = Axis Configured | Controller Loop Back: v35 |
Axis State
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Get | USINT | - | - | - | Enumeration 0 = Ready 1 = Drive Enable, (direct drive control) 2 = Servo Control 3 = Faulted 4 = Shutdown 5 = Inhibited 6 = Ungrouped 7 = No Module 8 = Configuring (FW default) |
State of this instance of the Motion Control Axis. Indicates the operating state of the axis. Examples of possible states include: axis-ready, drive enable, servo control, axis faulted, axis shutdown, axis inhibited, and axis unassigned.
Watch Event Task
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - E | Get | DINT | - | - | - | - |
User Event Task that will be triggered to execute when a Watch event occurs.
This attribute is set through internal communication from the user Task object to the Axis object when the Task trigger attribute is set to select this attributes of an Axis. It cannot be set directly by an external device. It is available to be read externally for diagnostic information.
The Watch Event Task attribute indicates which user Task will be triggered when a watch event occurs. An instance value of 0 indicates that no event task has been configured to be triggered by the Watch Event.
The user Task is triggered at the same time that the Process Complete bit is set for the instruction that armed the watch event.
Registration 1 Event Task
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - E | Get | DINT | - | - | - | - |
User Event Task that will be triggered to execute when a Registration 1 event occurs.
This attribute is set through internal communication from the user Task object to the Axis object when the Task trigger attribute is set to select this attributes of an Axis. It cannot be set directly by an external device. It is available to be read externally for diagnostic information.
The Registration 1 Event Task attribute indicates which user Task will be triggered when a Registration 1 event occurs. An instance value of 0 indicates that no event task has been configured to be triggered by the Registration 1 Event.
The user Task is triggered at the same time that the Process Complete bit is set for the instruction that armed the registration event.
Registration 2 Event Task
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - E | Get | DINT | - | - | - | - |
User Event Task that will be triggered to execute when a Registration 2 event occurs.
This attribute is set through internal communication from the user Task object to the Axis object when the Task trigger attribute is set to select this attributes of an Axis. It cannot be set directly by an external device. It is available to be read externally for diagnostic information.
The Registration 2 Event Task attribute indicates which user Task will be triggered when a Registration 2 event occurs.An instance value of 0 indicates that no event task has been configured to be triggered by the Registration 2 Event.
The user Task is triggered at the same time that the Process Complete bit is set for the instruction that armed the registration event.
Home Event Task
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - E | Get | DINT | - | - | - | - |
User Event Task that will be triggered to execute when a Home event occurs.
This attribute is set through internal communication from the user Task object to the Axis object when the Task trigger attribute is set to select this attributes of an Axis. It cannot be set directly by an external device. It is available to be read externally for diagnostic information.
The Home Event Task attribute indicates which user Task will be triggered when a home event occurs. An instance value of 0 indicates that no event task has been configured to be triggered by the Home Event.
The user Task is triggered at the same time that the Process Complete bit is set for the instruction that armed the home event.
Inhibit Axis
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
SSV | SINT | 0 | - | - | 0 triggers an uninhibit. 1 triggers an inhibit. Setting to any non-zero value is treated the same as a value of 1, and results in the attribute being set to a 1. |
Used to initiate putting an axis into the inhibit state.
This feature is designed for the following situations:
- To park an unused or faulted axis so that the application program can continue to run without the unused or faulted axis.
- To allow a 'generic' application program to be developed for a family of similar machines that may vary in axis count such that it can be configured during runtime to match the configuration of the specific machine.
The on-line inhibit process is an intrusive operation in that it impacts all axes associated to the same motion module as the one being inhibited. As such it is expected that the users will trigger this operation with the machine in a safe, non-operating, state. The inhibit process includes breaking connection to the associated motion module and then allowing the module to be reconfigured with or without (depending if you are inhibiting or un-inhibiting) this axis.
The inhibit/un-inhibit operation will also stop all motion on all axes associated to the same motion module including breaking all gearing relationships. This stop operation follows that of the shutdown fault action; servo action is immediately disabled as is the drives power structure. Unless some external form of braking capability is applied the axis will generally coast to a stop.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back support inhibiting and un-inhibiting individual axes.
Axis ID
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | DINT | - | - | - | ID |
Unique number assigned to axis on creation by configuration software.
The Axis ID is used by the Absolute Position Recovery feature during a configuration software download to determine if a given axis is a new axis or pre-existing axis. If the axis existed prior to the download, the controller saves critical absolute position data associated with the axis before continuing the download. Using the Axis ID, the controller is able to match the saved absolute position data with the pre-existing axis and recover absolute position. Using the saved data, absolute position will be recomputed to account for any motion that occurred while the download was in process or while power was off.
Axis Update Schedule
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | Set/
GSV | USINT | - | - | - | Enumeration: 0 = Base 1 = Alternate 1 2 = Alternate 2 3-255 = Reserved |
Determines the update schedule for the associated axis instance.
The default schedule setting of Base results in the axis being updated with every Base Update Period of the Motion Task, or the Base Update Period of the Motion Group. Alternate 1 and Alternate 2 schedule selections result in the axis being updated at multiples of the Base Update Period given by the Alternate 1 and Alternate 2 Update Multiplier attribute values of the Motion Group, or Motion Task or Alternate 1 Update Period and Alternate 2 Update Period, respectively.
Axis Data Type
Usage | Access | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|
Required - All | GSV | USINT | - | - | - | Enumeration: 0 = Feedback 1 = Consumed 2 = Virtual 3 = Generic 4 = Servo 5 = Servo Drive 6 = Generic Drive 7 = CIP Drive |
Associated tag data type for this instance of the Motion Control Axis Object.
The Axis Data Type attribute and is used to determine which data template, memory format, and set of attributes are created and applicable for this axis instance.
Provide Feedback