Motion Control Config Attributes
These are the basic motion control configuration attributes associated with a motion control axis. These attributes govern the overall behavior of the motion control axis.
Axis features
Usage | Access | Data Type | Default | Min | Max | Value Description |
---|---|---|---|---|---|---|
Required - All | Set/ GSV | DWORD | 0 | - | - | Bitmap 0 = Fine Interpolation (O) 1 = Registration Auto-rearm (O) 2 = Alarm Log (O) 3 = Marker (O) 4 = Home Switch (O) 5 = Hookup Test (O) 6 = Commutation Test (O) 7 = Motor Test (O) 8 = Inertia Test (O) 9 = Sensorless Control (O) 10 = Drive Scaling (O) 11 = Extended Event Block (O) 12 = Integer Command Position (O) 13 = Ext. Motor Test (O) 14 = Control Mode Change (O) 15 = Feedback Model Change (O) 16 = Pass Bus Status (O) 17 = Pass Bus Unload (O) 18 = Ext. Speed for SPM (O) 19 = Ext. Speed for IPM (O) 20 = Ext. Pos. Feedback (O) 21 = Ext. Sub Code Format (O) 22: Ext. Dynamic Motor Test (O) 23: Hookup Test Speed(O) 24: Device Test Mode 25-31: (reserved) |
The following table provides descriptions of the bit specified Axis feature attribute values.
Bit | Motion Status | Description |
---|---|---|
0 | Fine Interpolation (O) | Indicates that the axis supports fine interpolation of command data based on command target time. Fine interpolation is used to provide smoother command reference signals when the drive update period is smaller than the controller update period. |
1 | Registration Auto-rearm (O) | Indicates that the axis supports the automatic re-arming mechanism for registration inputs. This feature is required for windowed registration support. |
2 | Alarm Log (O) | Indicates that this axis supports the Alarm Log feature. Alarm Log data is received from the drive using the Alarm bit of the Status Data Set and updates the Alarm Log of the controller. |
3 | Marker (O) | Indicates that the axis position feedback device supports a marker function. This functionality is required for Homing Sequences that employ the marker signal and for the marker Hookup Test. |
4 | Home Switch (O) | Indicates that the axis supports a home switch input. This functionality is required for Homing Sequences that employ the home switch input signal. |
5 | Hookup Test (O) | The axis supports a Hookup Test service. This service is required to perform a Hookup Test (MRHD) to check wiring to the motor and feedback components. |
6 | Commutation Test (O) | The axis supports a Commutation Test as part of the Hookup Test service. This service is required to perform a Hookup Test (MRHD) to check commutation wiring and determine the Commutation Offset. |
7 | Motor Test (O) | The axis supports a Motor Test service. This service is required to perform a Motor Test (MRMT) to measure motor model parameters. |
8 | Inertia Test (O) | The axis supports an Inertia Test service. This service is used as part of the Auto Tune (MRAT) that measures inertia. |
9 | Sensorless Control (O) | The axis supports sensorless control operation letting the drive run in velocity loop mode without an external feedback device. |
10 | Drive Scaling (O) | The device supports Drive Scaling functionality where the device is able to scale feedback counts to planner counts and manage absolute position. |
11 | Extended Event Block (O) | The device supports the extended Event Data Block format. This format supports additional features generally associated with Drive Scaling functionality, such as Watch Position events and Windowed Registration. |
12 | Integer Command Position (O) | The device requires Command Position Format to be a DINT (32-bit signed integer) data type. If not set, the device supports the standard LREAL (64-bit floating point) Command Position data type. |
13 | Ext. Motor Text (O) | The device supports the extended motor data format for the Motor Test service. This format supports transfer of vendor specific motor parameters and is required for the Motor Test service to support IPM motors. |
14 | Control Mode Change (O) | The device supports changes to the Control Mode while in the Running state without generating large motion disturbances (bumpless). An example of such a mode change would be to switch from Position Control to Torque Control using an SSV instruction. If a particular Control Mode change is not supported by the device, a Configuration Fault will be generated. |
15 | Feedback Mode Change (O) | The device supports the ability to change the Feedback Mode while in the Running state without generating large motion disturbances (bumpless). An example of such a mode change would be to switch from Load Feedback to Motor Feedback using an SSV instruction. If a particular Feedback Mode change is not supported by the device, a Configuration Fault will be generated. |
16 | Pass Bus Status (O) | The device supports passing Converter Status bits, Bus Up and AC Power Loss, in the Control Status element of the C2D Connection's Axis Instance header when configured for DC Bus Sharing. The states of these Bus Status bits are determined by the controller based on the Bus Up and AC Power Loss bits passed in the Axis Status element of the D2C Connection's Cyclic Data of Converters or Drives (Bus Masters) that also support the Pass Bus Status feature. If clear, the associated device does not support Bus Up and AC Power Loss bits in the C2D Connection. Furthermore, if clear, the Bus Up and AC Power Loss status bits received by the controller in the device's D2C connection are not passed on to any other devices. |
17 | Pass Bus Unload (O) | The associated device is capable of generating a Bus Sharing exception based on Bus Unload request bit passed in the Control Status element of the C2D Connection's Axis Instance header. In this case, the controller passes a Bus Unload request to the device if any Converter or Drive (Bus Masters) in its Bus Sharing Group requests a Bus Unload. If clear, the controller is responsible for generating a Bus Sharing exception for this device axis in response to a Bus Unload request from any Converter or Drive (Bus Masters) in its Bus Sharing group. |
18 | Ext. Speed for SPM (O) | The device supports extending the speed range of an SPM motor through field weakening to speeds that require methods to protect drives from destructive DC Bus Overvoltage conditions. To manage that risk, the Extended Speed feature provides additional PM motor attributes including a PM Motor Extended Speed Permissive attribute. |
19 | Ext. Speed for IPM (O) | The device supports extending the speed range of an IPM motor through field weakening to speeds that require methods to protect drives from destructive DC Bus Overvoltage conditions. To manage that risk, the Extended Speed feature provides additional PM motor attributes including a PM Motor Extended Speed Permissive attribute. |
20 | Ext. Position Feedback (O) | The device supports passing Actual Position as a 64-bit LINT element in the Cyclic Data Block of the D2C Connection. If this bit is clear, the device only supports passing Actual Position as a 32-bit DINT. |
21 | Ext. Sub Code Format (O) | The device supports the Extended Sub Code Format as defined in the Motion Device Axis Object. The extended format uses the most significant bit of the Sub Code to select one of two bit field formats for the remaining 7-bits. |
24 | Device Test Mode | If set, the associated device supports operation in one or more device test modes. |
Axis configuration
Usage | Access | Data Type | Default | Min | Max | Value Description |
---|---|---|---|---|---|---|
Required - All | Set/GSV | USINT | AOP* | 0 | 5 | Enumeration 0 = Feedback Only (O) 1 = Frequency Control (O) 2 = Position Loop (O) 3 = Velocity Loop (O) 4 = Torque Loop (O) 5 = Non-Regenerative AC/DC Converter (O) 6 = Regenerative AC/DC Converter (O) 7 = Low Harmonic AC/DC Converter (O) 8 = DC/DC Converter (O) 9 = Non-Regenerative AC/DC/DC Converter (O) 10-127 = Reserved 128-255 Vendor Specific |
* The default value can be specified by the specific drive profile (AOP).
The axis configuration attribute determines the general dynamic control behavior of the motion device axis instance.
This attribute is used to set both the Control Mode and Control Method attributes according to the following table:
Axis Config | Control Mode | Control Method |
---|---|---|
Regenerative AC/DC Converter | No Control | No Control |
Non-Regenerative AC/DC Converter | No Control | No Control |
Low Harmonic AC/DC Converter | No Control | No Control |
DC/DC Converter | No Control | No Control |
Non-Regenerative AC/DC/DC Converter | No Control | No Control |
Feedback Only | No Control | No Control |
Frequency Control | Velocity Control | Frequency Control |
Position Loop | Position Control | PI Vector Control |
Velocity Loop | Velocity Control | PI Vector Control |
Torque Loop | Torque Control | PI Vector Control |
The axis configuration attribute is an enumerated value that determines the general dynamic control behavior of the motion device axis instance. This attribute is used by the controller to set the Control Mode attribute that is sent to the drive as part of the cycle connection, and also determines Control Method attribute configuration. So, when axis configuration is set by configuration software, control mode and control method are also updated.
The following table provides descriptions of the Axis configuration attribute values:
Enumeration | Usage | Name | Description |
---|---|---|---|
0 | R/E O/C | Feedback Only | Provides an axis interface to a specific feedback device as a master feedback source. The Control Mode and Control Method are set to No Control in this configuration, indicating that there is no dynamic control capability associated with this axis. |
1 | R/F | Frequency Control | Selects the Frequency Control Method that applies voltage to the motor, generally in proportion to the commanded frequency or speed. Accordingly, the Control Mode attribute is set to Velocity Control. |
2 | R/P | Position Loop | Selects the PI Vector Control Method that applies feedback to provide closed loop cascaded PI control of motor position, velocity, and torque, and includes closed loop control of Iq and Id components of the motor current vector. Accordingly, the Control Mode attribute is set to Position Control. |
3 | R/V O/P | Velocity Loop | Selects the PI Vector Control Method that applies feedback to provide closed loop cascaded PI control of motor velocity, and torque, and includes closed loop control of Iq and Id components of the motor current vector. Accordingly, the Control Mode attribute is set to Velocity Control. |
4 | R/T O/PV | Torque Loop | Selects the PI Vector Control Method that applies feedback to provide closed loop PI control of motor torque through control of Iq and Id components of the motor current vector. Accordingly, the Control Mode attribute is set to Torque Control. |
5 | O/N D | Non-Regenerative AC/DC Converter | Provides an axis interface to a standalone non-regenerative power converter device. Both the Control Mode and Control Method are set to No Control in this configuration, indicating that there is no dynamic control capability associated with this axis. |
6 | O/G | Regenerative AC/DC Converter | Provides an axis interface to a standalone regenerative power converter device or the regenerative converter function of an integrated regenerative drive device. Both the Control Mode and Control Method are set to No Control in the configuration, indicating that there is no dynamic control capability associated with this axis. |
7 | O/G | Low Harmonic AC/DC Converter | Provides an axis interface to a standalone AC/DC low harmonic converter device, or the AC/DC converter function of an integrated low harmonic drive device that utilizes active electronics to that regulate power flow from the AC source to the DC bus. Both the Control Mode and Control Method are set to No Control in this configuration, indicating that there is no dynamic motor control capability associated with this axis. |
8 | O/N | DC/DC Converter | Provides an axis interface to a class of devices that convert power between two
DC sources using active electronics, or simply distribute in-cabinet (primary) DC
input power to on-machine (secondary) DC buses. DC/DC converters with active
electronics are capable of transferring energy between an in-cabinet (primary) DC
bus and one or more on-machine (secondary) DC buses, each with different voltage
levels. Both the Control Mode and Control Method are set to No Control in this
configuration, indicating that there is no motor control capability associated
with this axis. |
9 | O/N | Non-Regenerative AC/DC/DC Converter | Provides an axis interface to a standalone AC/DC/DC non-regenerative power
converter device. This device is capable of providing either one or two DC Bus
outputs within one axis instance. Both the Control Mode and Control Method are set
to No Control in this configuration, indicating that there is no dynamic converter
control capability associated with this axis. |
10-127 | (Reserved) | ||
128-255 | (Vendor Specific) | ||
128 | R/X | Track Section | Track Section provides an axis interface to the Track Section function of a Track Section device that applies force to one or more Track Movers local to the Track Section. Both the Control Mode and Control Method are set to No Control in this configuration, indicating that there is no dynamic motor control associated with this axis commanded by the controller. |
Axis Test Mode
Axes with Test Mode Configuration set to Controller read the axis configuration to simulate the supported drive model behavior.
Enumeration | Name | Axis Test Mode Support (Test Mode Configuration) |
---|---|---|
0 | Feedback Only | * Controller Loop Back: v35 |
1 | Frequency Control | * Controller Loop Back: v35 |
2 | Position Loop | Controller Loop Back: v35 |
3 | Velocity Loop | * Controller Loop Back: v35 |
4 | Torque Loop | * Controller Loop Back: v35 |
5 | Non-Regenerative AC/DC Converter | Controller Loop Back: v35 |
6 | Regenerative AC/DC Converter | Controller Loop Back: v35 |
7 | Low Harmonic AC/DC Converter | Controller Loop Back: v35 |
8 | DC/DC Converter | Controller Loop Back: v35 |
128 | Track Section | Controller Loop Back: v36 |
* Limited support: Actual position does not track commanded position. Axis state and status are supported.
Control Mode
Usage | Access | Data Type | Default | Min | Max | Value Description |
---|---|---|---|---|---|---|
Required - All Derived from Axis Configuration | Get/ SSV (1) | BYTE | 0 | 0 | 4 | Enumeration 0 = No Control 1 = Position Control 2 = Velocity Control 3 = Acceleration Control 4 = Torque Control 5-15 = Reserved Bits 4-7 Reserved |
(1)
SSV -
These configuration attributes cannot be changed online or
using an SSV instruction if the axis is in the Running state, for example the Tracking
Command bit of the CIP Axis Status attribute.The Control Mode attribute determines the general dynamic control behavior of the drive device axis instance and consists of a 4-bit enumeration. This value is derived from the axis configuration attribute value during initialization. This attribute is transferred to the device as part of the Cyclic data block.
When modified programmatically, using SSV, the Control Mode value cannot be set to an enumeration that the current Axis Configuration cannot support. For example if the axis configuration is set for Velocity Loop, the Control Mode cannot be changed to Position Loop since position loop attributes have not been configured. This table provides a list of valid Control Modes for a given axis configuration:
Axis Configuration | Valid Control Modes |
---|---|
Track Section | No Control |
Non-Regenerative AC/DC Converter | No Control |
Regenerative AC/DC Converter | No Control |
Low Harmonic AC/DC Converter | No Control |
DC/DC Converter | No Control |
Feedback Only | No Control |
Frequency Control | Velocity Control |
Position Loop | Position Control Velocity Control Torque Control |
Velocity Loop | Velocity Control Torque Control |
Torque Loop | Torque Control |
The Control Mode attribute is a 4-bit enumeration that determines the specific dynamic behavior of the motor that the device is to control for this axis instance. Converters that use active control use the No Control attribute value. The operating mode of these converters is configured with the Converter Control Mode attribute. The following table provides descriptions of valid Control Modes.
Enumeration | Usage | Name | Description |
---|---|---|---|
0 | R/XBE | No Control | No control is provided in this mode. |
1 | R/P | Position Control | Controls the position, or orientation, of the motor. |
2 | R/PV | Velocity Control | Controls the velocity of the motor. |
3 | O/PVT | Acceleration Control | Controls the acceleration of the motor. |
4 | R/C | Torque Control | Controls the torque output of the motor. |
5-15 | Reserved | - |
Control Method
The Control Method (derived from axis configuration) attribute is an 8-bit enumerated code that determines the basic control algorithm applied by the device to control the dynamic behavior of the motor.
Usage | Access | Data Type | Default | Min | Max | Value Description |
---|---|---|---|---|---|---|
Required - All Derived from Axis Configuration | Get/ GSV | USINT | 0 | 0 | 2 | Enumeration 0 = No Control 1 = Frequency Control 2 = PI Vector Control 3-255 = Reserved |
This value is sent to the drive during initialization and cannot be changed during operation.
Enumeration | Usage | Name | Description |
---|---|---|---|
0 | R/XBE | No Control | Associated with a Control Mode of No Control where there is no explicit motor control provided by the device for this axis instance. |
1 | R/F | Frequency Control | An open loop control method that applies voltage to the motor, generally in proportion to the commanded frequency or speed. This control method is associated with Variable Frequency Drives (VFDs) or so called Volts/Hertz drives. |
2 | R/C | PI Vector Control | A closed loop control method that uses actual or estimated feedback for closed loop cascaded PI control of motor dynamics, for example, position, velocity, acceleration, and torque, and always includes independent closed loop PI control of Iq and Id components of the motor current vector. |
3-127 | Reserved | - | |
128-255 | Vendor Specific | - |
Provide Feedback