Axis Safety Status Attributes

The following attribute tables contains axis attributes used with the integrated Safety functionality associated with a Motion Device Axis Object instance included in a CIP Motion Safety Drive. These attributes reflect the current state of an embedded Safety Core within for a CIP Motion Safety Drive device that is designed to interoperate with an external Safety Controller using a CIP Safety connection.
In the Logix Integrated Architecture, many of the safety functions can be executed either in the drive or in the associated safety controller. A unique feature of the architecture is that regardless of where the safety function is executed, the Axis Safety Status and Axis Safety Fault information reported by these safety functions is the same. This is achieved by the Safety Status Pass Thru feature where safety functions executing in the safety controller transmit their fault and status information to the drive via the Safety Output Assembly where this information is combined with the fault and status information of safety function executing in the Safety Core of the drive. The combined safety function fault and status data is then "Passed Thru" to the associated Motion Device Axis Object instance attributes.
The following table identifies the supported safety functions:
Short Name
Full Name
Safety Controller
Drive
Description
Axis Test Mode Support
(Test Mode Configuration)
STO
Safe Torque Off
No
Yes
Disables associated drive power structure.
Controller Loop Back: V36
SBC
Safe Brake Control
Yes
Yes
Engages safety brake.
Controller Loop Back: V36
SS1
Safe Stop 1
Yes
Yes
Monitors Category 1 Stop followed by STO.
Controller Loop Back: V36
SS2
Safe Stop 2
Yes
No
Monitors Category 2 Stop followed by SOS.
Controller Loop Back: V36
SOS
Safe Operating Stop
Yes
No
Monitor standstill condition for movement.
Controller Loop Back: V36
SMT
Safe Motor Temperature
No
Yes
Monitor motor temperature for overtemperature.
SLT
Safely-limited Torque
No
No
Prevents the motor from exceeding the specified torque limit.
SLA
Safely-limited Acceleration
No
No
Monitor acceleration exceeding configured limit.
SLS
Safely-limited Speed
Yes
No
Prevents the motor from exceeding the specified speed limit.
Controller Loop Back: V36
SDI
Safe Direction
Yes
No
Monitor for change in direction of travel.
Controller Loop Back: V36
SSM
Safe Speed Monitor
Yes
No
Monitor speed exceeding configured limit.
SLP
Safely-limited position
Yes
No
Prevents the motor shaft from exceeding the specified position limit(s).
Controller Loop Back: V36
SCA
Safe CAM
Yes
No
Monitors whether the motor shaft position is within a specified range.
SFX
Safe Feedback Interface
Yes
No
Scales and references safety feedback data.
Controller Loop Back: V36
SLR
Safe Load Retention
No
Yes
Monitors for Brake Slip when stopped and requests Cat2 stop when Brake Slip exceeds safety limit.
SBT
Safe Brake Test
No
Yes
Tests that a brake can hold a specific load without excess brake slip.
The Axis Safety State, Axis Safety Status, and Axis Safety Fault attributes defined below are based on the values read from attributes resident in objects associated with the Safety Core and are used by the motion control system to monitor the behavior of the Safety Core via the CIP Motion connection.
Axis Safety State
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
UINT
-
-
-
Enumeration:
0 = Unknown (No Motion Connection)
1 = Self-Testing
2 = Configured (No Safety Connection)
3 = Self-Test Exception
4 = Running
5 = Recoverable Fault
6 = Unrecoverable Fault
7 = Configuring
8 = Not Configured
9-50 = Reserved by CIP
51 = Not Configured (Torque Permitted)
52 = Running (Torque Permitted)
53-99 = Device Specific
100-255 = Vendor Specific
The Axis Safety State attribute is an 8-bit enumerated value that indicates the state of the associated Safety Supervisor object of the device as it applies to this axis instance. There is only one Safety Supervisor object servicing the CIP Motion device so its state generally applies to all applicable Axis instances of the device. This means that all instances of this object generally have the same state for this attribute.
The two exceptions to this general state behavior are the Waiting for TUNID with Torque Permitted (state=51) and Executing with Torque Permitted (state=8) states that have axis specific qualification. When the Safety Supervisor State is Waiting for TUNID with Torque Permitted, if the Axis Safety Status bit, Safe Torque Disabled, is set, the Axis Safety State is set to Waiting for TUNID. When the Safety Supervisor State is Executing with Torque Permitted, if the Axis Safety Status bit, Safe Torque Disabled, is set, the Axis Safety State is Executing.
Axis Safety State Bit Descriptions
Bit
Safety Supervisor State
Description
0 = Undefined/Unknown (No MotionConnection)
Undefined
No motion connection has been opened to the drive. Actual safety state is unknown.
1 = Self-Testing
Self-Testing
The safety function of drive has been initialized; all attributes given appropriate defaults and safety faults have been reset.
Device is performing tests to determine if it is qualified to execute its safety function.
2 = Configured (No Safety Connection)
Idle
The safety function of drive has been initialized, successfully completed self-testing, and has a valid safety configuration. However, the device is not executing the operational components of its safety functions. Configuring and Configured are persistent states that are preserved through power cycles.
3 = Self-Test Exception
Self-Test Exception
The safety function of drive has detected an exception condition during self-testing. The details of the exception are stored in the appropriate attribute values of the Safety Supervisor object.
4 = Running
Executing
The safety function of drive is fully configured with an open safety output connection and executing.
In this state, the drive is operational and free to apply torque to the motor as long as there are no safety demands.
5 = Recoverable Fault
Abort
The safety function of drive is in a faulted state that can be recovered by cycling the power or reconnecting the drive.
6 = Unrecoverable Fault
Critical Fault
The safety function of drive is in a faulted state for which there is no recovery other than replacing the module.
7 = Configuring
Configuring
The safety function of drive has been initialized, successfully completed self-testing, and is in the process of receiving a valid configuration from a safety controller.
Configuring and Idle are persistent states that are preserved through power cycles.
8 = Not Configured
Waiting for TUNID
The safety function of drive has exited Self-testing and recognizes that it has the out-of-box default configuration values, for example it has not been configured by a safety controller. The drive remains in this state until a safety controller initiates the configuration process. Application of torque to the motor is NOT permitted in this state.
9-50 = Reserved
-
-
51 = Not Configured (Torque Permitted)
Waiting for TUNID with Torque Permitted
Same behavior as Not Configured state with the exception that the drive axis is operational and the safety function will permit application of torque to the motor.
52 = Running (Torque Permitted)
Executing with Torque Permitted
Same behavior as Running state with the exception that the drive axis is operational and the safety function will permit application of torque to the motor.
Entering this state from the Running state requires a successful STO Mode change service applied while the safety controller is in Program Mode.
53-99 = Device Specific
-
-
100-255 = Vendor Specific
-
-
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Axis Safety State values.
Value
Safety Supervisor State
Axis Test Mode Support
(Test Mode Configuration)
0 = Undefined/Unknown (No MotionConnection)
Undefined/Unknown (No Motion Connection)
Controller Loop Back: V36
4 = Running
Executing
Controller Loop Back: V36
8 = Not Configured
Not Configured / Waiting for TUNID
Controller Loop Back: V36
52 = Running (Torque Permitted)
Executing with Torque Permitted
Controller Loop Back: V36
Axis Safety Status
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0 = Safety Fault
1 = Safety Reset Request
2 = Safety Reset Required
3 = Safe Torque Off Active
4 = Safe Torque Disabled
5 = Safe Brake Control (SBC) Active
6 = Safe Brake Control (SBC) Engaged
7 = Safe Stop 1 (SS1) Active
8 = Safe Stop 2 (SS2) Active
9 = Safe Operating Stop (SOS) Active
10 = Safe Operating Stop (SOS) Standstill
11 = Safe Motor Temperature (SMT) Active
12 = Safe Motor (SMT) Overtemperature
13-15 = (reserved)
16 = Safe Speed Monitoring (SSM) Active
17 = Safe Speed Monitoring (SSM) Status
18 = Safe Limited Speed (SLS) Active
19 = Safe Limited Speed (SLS) Limit
20 = Safe Limited Accel (SLA) Active
21 = Safe Limited Accel (SLA) Limit
22 = Safe Direction (SDI) Active
23 = Safe Direction (SDI) Limit
24 = Safe Positive Motion
25 = Safe Negative Motion
26 = Safe CAM (SCA) Active
27 = Safe CAM (SAC) Status
28 = Safe Limited Position (SLP) Active
29 = Safe Limited Position (SLP) Limit
30 = Safety Output Connection Closed
31 = Safety Output Connection Idle
The Axis Safety Status attribute is a collection of bits indicating the status of the standard safety functions for the axis as reported by the embedded Safety Core of the device. The Axis Safety Status word is a concatenation of two 16-bit safety status attributes. The lower 16-bits are the current Safety Stop Status attribute value of the Safety Stop Functions object associated with this axis instance. The upper 16-bits are the current Safety Limit Status attribute value of the Safety Limit Functions object associated with this axis instance with the exception of the two most significant bits that are masked off to accommodate two Safety Output Connection status bits. Specifically, the Safety Output Connection Closed bit, when set, indicates that the Safety Output Connection has either not been opened or has been closed. The Safety Output Connection Idle bit, when set, indicates that the Safety Output Connection's Run/Idle bit has been set to Idle.
For Rockwell Automation safety drive devices, the safety status data from the drive's Safety Core may include safety status from the Safety Controller through the Pass Thru data included in the Safety Output assembly. This allows the Axis Safety Status attribute to reflect safety function status conditions regardless of where the safety function is executed, be it in the Safety Controller, or the drive's Safety Core.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Axis Safety Status bits.
Bit
Name
Axis Test Mode Support
(Test Mode Configuration)
0
Safety Fault
Controller Loop Back: V36
1
Safety Reset Request
Controller Loop Back: V36
2
Safety Reset Required
Controller Loop Back: V36
3
Safe Torque Off Active
Controller Loop Back: V36
4
Safe Torque Disabled
Controller Loop Back: V36
5
Safe Brake Control (SBC) Active
Controller Loop Back: V36
6
Safe Brake Control (SBC) Engaged
Controller Loop Back: V36
7
Safe Stop 1 (SS1) Active
Controller Loop Back: V36
8
Safe Stop 2 (SS2) Active
Controller Loop Back: V36
9
Safe Operating Stop (SOS) Active
Controller Loop Back: V36
10
Safe Operating Stop (SOS) Standstill
Controller Loop Back: V36
18
Safe Limited Speed (SLS) Active
Controller Loop Back: V36
19
Safe Limited Speed (SLS) Limit
Controller Loop Back: V36
22
Safe Direction (SDI) Active
Controller Loop Back: V36
23
Safe Direction (SDI) Limit
Controller Loop Back: V36
28
Safe Limited Position (SLP) Active
Controller Loop Back: V36
29
Safe Limited Position (SLP) Limit
Controller Loop Back: V36
Axis Safety Status - Mfg
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0-31: Reserved
The Axis Safety Status - Mfg attribute is a collection of bits indicating the status of the manufacturer specific safety functions for the axis as reported by the embedded Safety Core of the device.
Axis Safety Status - RA
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0 = Safe Brake Integrity
1 = Safe Feedback Homed
2 = SBT Active
3 = SBT Brake Failure
4 = SBT Passed
5 = SLR Mode
6 = SLR Active
7 = SLR Limit
8 = SLR Brake Slip Limit
9-31 = (reserved)
The Axis Safety Status - RA attribute is a collection of bits indicating the status of the Rockwell Automation specific safety functions for the axis as reported by the embedded Safety Core of the device. For Rockwell Automation safety drive devices, the safety status data from the drive's Safety Core may be combined with safety status from the Safety Controller through the Pass Thru data included in the Safety Output assembly. This allows the Axis Safety Status RA attribute to reflect safety function status conditions regardless of where the safety function is executed, be it in the Safety Controller, or the drive's Safety Core.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Safety Status Ra bits.
Bit
Name
Axis Test Mode Support
(Test Mode Configuration)
0
Safe Brake Integrity
Controller Loop Back: V36
1
Safe Feedback Homed
Controller Loop Back: V36
Axis Safety Faults
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0 = (reserved)
1 = Safety Core Fault
2 = Safety Feedback Fault
3 = Safe Torque Off Fault
4 = Safe Stop 1 (SS1) Fault
5 = Safe Stop 2 (SS2) Fault
6 = Safe Operating Stop (SOS) Fault
7= Safe Brake (SBC) Fault
8 = Safe Motor Temperature Fault (SMT)
9-15 = (reserved)
16 = Safe Speed Monitor (SSM) Fault
17 = Safe Limited Speed (SLS) Fault
18 = Safe Limited Accel (SLA) Fault
19 = Safe Direction (SDI) Fault
20 = Safe CAM (SCA) Fault
21 = Safe Limited Protection (SLP) Fault
22-29 = (reserved)
30 = Safety Validator Fault
31 = Safety Abort Fault
The Axis Safety Faults attribute is a collection of bits indicating the safety fault status of the axis associated with standard safety functionality as reported by the embedded Safety Core of the device. When a safety fault condition occurs, the Safety Core forces the axis into a Safe State and if the Safety Fault Action is set to Major Fault or Minor Fault, the corresponding bit is set in the Axis Safety Faults attribute. An active axis safety fault bit remains latched even if the underlying safety fault condition is cleared by the Safety Core. A Fault Reset Request to the associated axis clears the axis safety fault bits, but the bits immediately set again if the underlying safety fault conditions are still present. The Axis Safety Faults bitmap is a concatenation of two 16-bit safety fault attributes. The lower 16-bits is the current Safety Stop Faults attribute value of the Safety Stop Functions object associated with this axis instance. The upper 16-bits is the current Safety Limit Faults attribute value of the Safety Limit Functions object associated with this axis instance. Bits 30 and 31 are used to indicate two safety faults conditions that are not tied to the drive safety functions. Bit 30 indicates that the Safety Validator object (0x3A) has detected a safety connection fault. Bit 31 indicates that the Safety Supervisor object (0x39) has detected a recoverable fault and transitioned to the Abort state.
For Rockwell Automation safety drive devices, the safety fault status data from the drive's Safety Core may include safety faults from the Safety Controller through the Pass Thru data included in the Safety Output assembly. This allows the Axis Safety Faults attribute to reflect safety function fault conditions regardless of where the safety function is executed, be it in the Safety Controller, or the drive's Safety Core.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Axis Safety Fault bits.
Bit
Name
Axis Test Mode Support
(Test Mode Configuration)
4
Safe Stop 1 (SS1) Fault
Controller Loop Back: V36
5
Safe Stop 2 (SS2) Fault
Controller Loop Back: V36
6
Safe Operating Stop (SOS) Fault
Controller Loop Back: V36
7
Safe Brake (SBC) Fault
Controller Loop Back: V36
17
Safe Limited Speed (SLS) Fault
Controller Loop Back: V36
19
Safe Direction (SDI) Fault
Controller Loop Back: V36
21
Safe Limited Protection (SLP) Fault
Controller Loop Back: V36
Axis Safety Faults - Mfg
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0-31: Reserved
The Axis Safety Faults - Mfg attribute is a collection of bits indicating the safety fault status of the axis associated with manufacturer specific safety functionality as reported by the embedded Safety Core of the device. When a safety fault condition occurs, the Safety Core forces the axis into a Safe State and, if the Safety Fault Action is set to Major Fault or Minor Fault, the corresponding bit is set in the Axis Safety Faults Mfg attribute. An active axis safety fault bit remains latched even if the underlying safety fault condition is cleared by the Safety Core. A Fault Reset Request to the associated axis clears the axis safety fault bits, but the bits immediately set again if the underlying safety fault conditions are still present.
Axis Safety Faults - RA
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0 = (reserved)
1 = Safety Feedback Interface (SFX) Fault
2 = Safe Brake Test (SBT) Fault
3 = Safe Load Retention (SLR) Fault
4-31 = Reserved
The Axis Safety Faults - RA attribute is a collection of bits indicating the safety fault status of the axis associated with Rockwell Automation specific safety functionality as reported by the embedded Safety Core of the device. When a safety fault condition occurs, the Safety Core forces the axis into a Safe State and if the Safety Fault Action is set to Major Fault or Minor Fault, the corresponding bit is set in the Axis Safety Faults RA attribute. An active axis safety fault bit remains latched even if the underlying safety fault condition is cleared by the Safety Core. A Fault Reset Request to the associated axis clears the axis safety fault bits, but the bits immediately set again if the underlying safety fault conditions are still present.
For Rockwell Automation safety drive devices, the safety fault status data from the drive's Safety Core may be combined with safety faults from the Safety Controller through the Pass Thru data included in the Safety Output assembly. This allows the Axis Safety Faults RA attribute to reflect safety function fault conditions regardless of where the safety function is executed, be it in the Safety Controller, or the drive's Safety Core.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Axis Safety Faults RA bits.
Bit
Name
Axis Test Mode Support
(Test Mode Configuration)
1
Safety Feedback Interface (SFX) Fault
Controller Loop Back: V36
Axis Safety Alarms
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0 = (reserved)
1 = Safety Core Alarm
2 = Safety Feedback Alarm
3 = Safe Torque Off Alarm
4 = SS1 Alarm
5 = SS2 Alarm
6 = SOS Alarm
7 = SBC Alarm
8 = SMT Alarm
9-15 = (reserved)
16 = SSM Alarm
17 = SLS Alarm
18 = SLA Alarm
19 = SDI Alarm
20 = SCA Alarm
21 = SLP Alarm
22-29 = (reserved_
30 = Safety Validator Alarm
31 = Safety Abort Alarm
The Axis Safety Alarms attribute is a collection of bits indicating the safety alarm status of the axis associated with standard safety functionality as reported by the embedded Safety Core of the device. When a safety fault condition occurs, the Safety Core forces the axis into a Safe State and, if the Safety Fault Action is set to Alarm, the corresponding bit is set in the Axis Safety Alarms attribute. An active axis safety alarm bit shall remain set as long as the underlying safety fault condition is present in the Safety Core.
The Axis Safety Alarm bitmap is a concatenation of two 16-bit safety fault attributes. The lower 16-bits is the current Safety Stop Faults attribute value (Attribute 41) of the Safety Stop Functions object associated with this axis instance. The upper 16-bits is the current Safety Limit Faults attribute value (Attribute 41) of the Safety Limit Functions object associated with this axis instance. Bit 30 indicates that the Safety Validator object (0x3A) has detected a safety connection fault. Bit 31 indicates that the Safety Supervisor object (0x39) has detected a recoverable fault and transitioned to the Abort state.
For Rockwell Automation safety drive devices, the safety fault status data from the drive’s Safety Core may be combined with safety faults from the Safety Controller via the Pass Thru data included in the Safety Output assembly. This allows the Axis Safety Alarms attribute to reflect safety function fault conditions regardless of where the safety function is executed, be it in the Safety Controller, or the drive’s Safety Core.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these Axis Safety Alarm bits.
Bit
Name
Axis Test Mode Support
(Test Mode Configuration)
3
Safe Torque Off Alarm
Controller Loop Back: V36
Axis Safety Alarms - Mfg
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0-31: Reserved
The Axis Safety Alarms - Mfg attribute is a collection of bits indicating the safety alarm status of the axis associated with manufacturer specific safety functionality as reported by the embedded Safety Core of the device. When a safety fault condition occurs, the Safety Core forces the axis into a Safe State and, if the Safety Fault Action is set to Alarm, the corresponding bit is set in the Axis Safety Alarm Mfg attribute. An active safety alarm bit remains set as long as the underlying safety fault condition is present in the Safety Core.
Axis Safety Alarms - RA
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Get/GSV
T
DWORD
-
-
-
Bitmap:
0 = (reserved)
1 = Safety Feedback Interface (SFX) Alarm
2 = Safe Brake Test (SBT) Alarm
3 = Safe Load Retention (SLR) Alarm
4-31 = Reserved
The Axis Safety Alarms - RA attribute is a collection of bits indicating the safety alarm status of the axis associated with RA specific safety functionality as reported by the embedded Safety Core of the device. When a safety fault condition occurs, the Safety Core forces the axis into a Safe State and, if the Safety Fault Action is set to Alarm, the corresponding bit is set in the Axis Safety Alarm RA attribute. An active safety alarm bit remains set as long as the underlying safety fault condition is present in the Safety Core.
For Rockwell Automation safety drive devices, the safety fault status data from the drive’s Safety Core may be combined with safety faults from the Safety Controller via the Pass Thru data included in the Safety Output assembly. This allows the Axis Safety Alarms RA attribute to reflect safety function fault conditions regardless of where the safety function is executed, be it in the Safety Controller, or the drive’s Safety Core.
Safety Fault Action
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Safety only
Set/SSV
USINT
4 (D)
2 (E)
4 (X)
-
-
Enumeration: (D)
0 = Ignore (O)
1 = Alarm (O)
2 = Fault Status Only (O)
3 = Stop Planner (O)
4 = Disable (R)
5 = Shutdown (R)
Enumeration: (E)
0 = Ignore (O)
1 = Alarm (O)
2 = Fault Status Only (R)
3 = N/A
4 = N/A
5 = Shutdown (R)
Enumeration: (X)
0 = Ignore (O)
1 = Alarm (O)
2 = Fault Status Only (O)
3 = n/a
4 = Disable (R)
5 = Shutdown (R)
6-254 = Reserved
The Safety Fault Action attribute is an enumerated value that specifies the action taken in the event of a safety fault condition reported by the Safety Core.
Safe Torque Off Action
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XD
Safety Only
Set/
SSV#
USINT
Eq 23
1 for C
0 for F
0 for X
-
-
Enumeration:
0 = Disable and Coast
1 = Current Decel and Disable
2 = Ramped Decel and Disable
3-127 = (reserved)
128-255 = (vendor specific)
128 = DC Injection Brake
129 = AC Injection Brake
#
Indicates the attribute cannot be set while the tracking command (Tracking Command bit in CIP Axis Status is true).
When the drive detects a Safe Torque Off (STO) Active condition that was not initiated by a Safe Stop 1 (SS1) Active condition, as reported by the embedded Safety Core through the Axis Safety Status attribute, and the Safe Torque Off Action Source is set to Connected Drive, this value determines the stopping method to apply to the motor. Each Safe Torque Off Action enumeration initiates one of two defined Stopping Sequences, Category 0 Stop, or Category 1 Stop. The definition for each enumeration will follow the same enumerations defined for the Stopping Action attribute.
Category 1 Stop enumerations of Current Decel & Disable or Ramped Decel & Disable are often used in conjunction with a configured delay (for example, STO to Safe Brake Control (SBC) Delay or STO Delay) between the STO Active condition and Safe Torque Disabled to allow the drive to bring the motor to a controlled stop and engage a brake prior to disabling the power structure. This capability is particularly important for vertical load applications.
The final state after the Stopping Sequence is applied is the Start Inhibited state or, in the case of a Safety Fault initiated STO activation, the Major Faulted state. In either final state the device's inverter power structure will be disabled, ultimately with safety integrity as enforced by the Safety Core's STO safety function.
Safe Torque Off Action Source
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XD
Safety Only
Set/
SSV#
USINT
0
-
-
Enumeration:
0 = Connected Drive (R)
1 = Running Controller (O)
2-127 = (reserved)
128-255 = (vendor specific)
#
Indicates the attribute cannot be set while the tracking command (Tracking Command bit in CIP Axis Status is true).
The Safe Torque Off Action Source attribute determines whether the drive or the controller initiates the stopping sequence in response a STO Active condition in the Axis Safety Status attribute that was not initiated by an SS1 or Safe Stop 2 (SS2) Active condition.
When configured for Connected Drive (default), the drive will initiate the stopping sequence according to the selected Safe Torque Off Action. However, the drive must have an open connection to the controller for the configured stopping action to occur. If the drive is not connected, the drive would have already initiated the configured Connection Loss Stopping Action.
When configured for Running Controller, the stopping sequence is initiated by the connected controller as long as the controller connection's "Run/Idle" bit in the Real Time (RT) Header is indicating Run Mode. This allows the controller to provide a programmed stopping action. If the controller is in Idle Mode, i.e. not actively running the application program, the connected drive will initiate the stopping sequence according to the configured Safe Torque Off Action. This selection is only valid if the connected controller is supplying the "Run/Idle" Real Time header.
Axis Test Mode
Axes with the Test Mode Enable attribute set to Enabled and that are configured for Controller Loop Back use the Safe Torque Off Action Source attribute to ensure that the axis simulates a stop in response to a STO active condition that was not initiated by an SS1 or a SS2 Active condition in the Axis Safety Status attribute. The drive model simulates any required Device Safety input parameters, Axis Safety Status, and Axis Safety faults at the appropriate time.
Safe Stopping Action
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XD
Safety Only
Set/
SSV#
USINT
0
-
-
Enumeration:
0 = Current Decel
1 = Ramped Decel
2-127 = (reserved)
128-255 = (vendor specific)
#
Indicates the attribute cannot be set while the tracking command (Tracking Command bit in CIP Axis Status is true).
The Safe Stopping Action attribute determines the stopping method that the drive applies to the motor when:
  • An SS1 or SS2 condition occurs. The Axis Safety Status attribute indicates an SS1 or SS2 condition.
  • The Axis Safety Stopping Source is set to the Connected Drive.
The selected stopping method is applied while in the Stopping state and the final state after the stopping method completes is the Stopped state. In this final state the device's inverter power structure will either be Disabled and free of torque, if initiated by an SS1 Active status bit, or actively held (Hold selection) in a static condition if initiated by an SS2 Active status bit.
Safe Stopping Action Bit Descriptions
Bit
Required/Optional
Name
Description
0
R/C
O/F
Current Decel
Current Decel leaves the power structure and any active control loops enabled while stopping. If configured for position control mode, the drive forces the position reference to hold its current value until the axis reaches zero speed. Once at zero speed the position reference is immediately set equal to the actual position to hold the axis at standstill. If in velocity control mode, the drive forces the velocity reference to zero. In either case, forcing the position or velocity reference signals to a fixed value results in a rapid increase in control loop error of the moving axis that saturates the output current of the drive to the configured Stopping Torque that brings the motor to a stop. In torque control mode, the drive directly applies the configured Stopping Torque to the torque command signal to decelerate the motor. When the velocity feedback value reaches zero speed, the torque command is set to zero. In frequency control mode the Current Vector Limit attribute, rather than the Stopping Torque attribute, is used to regulate the stopping current. Once stopped, or the configured Stopping Time, or factory limit expires, the Current Decel stopping action is complete.
1
O/FV
Ramped Decel
Current Decel & Disable also leaves the power structure and any active control loops enabled while stopping but uses the Ramp Generator associated with the Velocity Fine Command Generator block to decelerate the motor to a stop. When initiating a Current Decel & Disable Stop, the Ramp Generator is immediately activated and the drive no longer follows command from the controller. The Ramp Generator input is initialized to zero and the output is initialized to the current speed of the motor, thus causing the Ramp Generator output to ramp the motor from its current speed down to zero according to the ramp control parameters. Once stopped, or the configured Stopping Time or factory timeout limit expires, the Ramped Decel stopping action is complete.
2-127
Reserved
128-255
Vendor Specific
Safe Stopping Action Source
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XD
Set/
SSV#
USINT
0
-
-
Enumeration:
0 = Connected Drive (R)
1 = Running Controller (O)
2-127 = (reserved)
128-255 = (vendor specific)
#
Indicates the attribute cannot be set while the tracking command (Tracking Command bit in CIP Axis Status is true).
This attribute determines whether the drive or the controller initiates the stopping sequence in response to an SS1 or SS2 Active bit transition in the Axis Safety Status attribute.
When configured for Connected Drive (default), the drive will initiate the stopping sequence according to the selected Safe Stopping Action. However, the drive must have an open connection to the controller for the configured stopping action to occur. If the drive is not connected, the drive would have already initiated the configured Connection Loss Stopping Action.
When configured for Running Controller, the stopping sequence is initiated by the connected controller as long as the controller connection's "Run/Idle" bit in the Real Time (RT) Header is indicating Run Mode. This allows the controller to provide a programmed stopping action. If the controller is in Idle Mode, i.e. not actively running the application program, the connected drive will initiate the stopping sequence according to the configured Safe Stopping Action. This selection is only valid if the connected controller is supplying the "Run/Idle" Real Time header.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back read the Safe Stopping Action Source attribute and depending on the action source, the drive model simulates any required Device Safety input parameters, Axis Safety Status, and Axis Safety faults.
Axis Safety Data A
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Get/GSV
DWORD
-
-
-
General Purpose Data Container
A 32-bit container holding general purpose Safety Data passed from the Safety Controller thru the Safety Pass Thru object attribute, Safety Pass Thru Data A.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back read the Safety Pass Thru Data A object attribute from the simulated device and make the content available in the Axis Safety Data A attribute.
Axis Safety Data B
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - XDE
Get/GSV
DWORD
-
-
-
General Purpose Data Container
A 32-bit container holding general purpose Safety Data passed from the Safety Controller thru the Safety Pass Thru object attribute, Safety Pass Thru Data B.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back read the Safety Pass Thru Data B object attribute from the simulated device and make it available in the Axis Safety Data B attribute.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal