CAM_PROFILE_EXTENDED Structure
The CAM_PROFILE_EXTENDED data type is an array of coefficients representing a calculated
cam profile that can be used as input to a time cam or position cam instruction.
CAM_PROFILE_EXTENDED is supported by
Compact GuardLogix
5580, and CompactLogix
5380 controllers only.This table describes the format of the array elements.
Mnemonic | Data Type | Description |
Status | DINT | The status parameter indicates that the Cam Profile Extended array element has been calculated. If you attempt the execution of a camming instruction by using an uncalculated element in a cam profile, the instruction produces an error. 0 = cam profile element was not calculated 1 = cam profile element is being calculated 2 = cam profile element has been calculated n = cam profile element has been calculated and is being used by (n-2) MAPC and MATC instructions. |
Segment Type | DINT | The type of interpolation: 0 = linear 1 = cubic |
Master | LREAL | The x value of the point. |
Slave | LREAL | The y value of the point. |
C0 | LREAL | Coefficients of the polynomial equation that determines slave position as a function of master position or time. See Motion Calculate Cam Profile (MCCP) for additional information. |
C1 | LREAL |
IMPORTANT:
Modification of these coefficients can
cause unintended motion.
Coefficients of the polynomial equation that determines slave position as a function of master position or time. |
C2 | LREAL | |
C3 | LREAL |
IMPORTANT:
Do not attempt to copy data between CAM_PROFILE and
CAM_PROFILE_EXTENDED data types. Copying the data between these data types will result in
data corruption.
TIP:
You cannot convert the CAM_PROFILE data type to CAM_PROFILE_EXTENDED, and you
cannot convert the CAM_EXTENDED data type to CAM.
Provide Feedback