Lower Case (LOWER)
This information applies to the CompactLogix 5370, ControlLogix 5570, Compact
GuardLogix 5370, GuardLogix 5570, Compact GuardLogix 5380, CompactLogix 5380,
ControlLogix 5580, GuardLogix 5580, and ControlLogix 5590 controllers.
The LOWER instruction converts the alphabetical characters in a string to lower case characters.
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
LOWER(Source,Dest);
Operands
Ladder Diagram and Structured Text
Operand | Type | Format | Description |
---|---|---|---|
Source | String | Tag | The tag that contains the characters you want to convert to lower case |
Destination | String | Tag | The tag to store the characters in lower case |
See Structured Text Syntax for
more information on the syntax of expressions within structured text.
Description
The LOWER instruction converts all the letters in the Source to lower case, and places the result in the Destination.
- ASCII characters are case-sensitive. Upper case A ($41) is not equal to lower case a ($61).
- If operators directly enter ASCII characters, convert the characters to all upper case or lower case before you compare them.
Any characters in the Source string that are not letters remain unchanged.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | N/A |
Rung-condition-in is false | N/A |
Rung-condition-in is true | The instruction executes. |
Postscan | N/A |
Structured Text
Condition | Action |
---|---|
Prescan | See Prescan in the preceding Ladder Diagram table |
Normal execution | See rung-condition-in is true in the preceding Ladder Diagram table. |
Postscan | See Postscan in the preceding Ladder Diagram table |
Examples
To find information about a specific item, an operator enters the item number into an ASCII terminal. After the controller reads the input from a terminal (terminal_read is set), the LOWER instruction converts the characters in item_number to all upper case characters and stores the result in item_number_lower_case. A subsequent rung then searches an array for characters that match those in item_number_lower_case.
Ladder Diagram

Structured Text
IF terminal_read THEN
LOWER(item_number,item_number_lower_case);
terminal_read := 0;
END_IF;
Provide Feedback